/****************************************************************************** @file cc13x2_cc26x2.cmd @brief Linker configuration file for sensor/collector on cc13x2/cc26x2 devices Group: WCS LPC Target Device: cc13x2_26x2 ****************************************************************************** Copyright (c) 2016-2021, Texas Instruments Incorporated All rights reserved. Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met: * Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer. * Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution. * Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission. THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. ****************************************************************************** *****************************************************************************/ /* Retain interrupt vector table variable */ --retain=g_pfnVectors /* Override default entry point. */ --entry_point ResetISR /* Allow main() to take args */ --args 0x8 /* Suppress warnings and errors: */ /* - 10063: Warning about entry point not being _c_int00 */ /* - 16011, 16012: 8-byte alignment errors. Observed when linking in object */ /* files compiled using Keil (ARM compiler) */ --diag_suppress=10063,16011,16012 /* The following command line options are set as part of the CCS project. */ /* If you are building using the command line, or for some reason want to */ /* define them here, you can uncomment and modify these lines as needed. */ /* If you are using CCS for building, it is probably better to make any such */ /* modifications in your CCS project and leave this file alone. */ /* */ /* --heap_size=0 */ /* --stack_size=256 */ /* --library=rtsv7M3_T_le_eabi.lib */ /****************************************************************************** Memory Sizes *****************************************************************************/ /* The starting address of the application. Normally the interrupt vectors */ /* must be located at the beginning of the application. */ #define FLASH_BASE 0x00000000 #define FLASH_LAST_BASE 0x56000 #define RAM_BASE 0x20000000 #define FLASH_SIZE 0x56000 #define FLASH_LAST_SIZE 0x2000 #define RAM_SIZE 0x14000 /****************************************************************************** System memory map *****************************************************************************/ MEMORY { /* Application stored in and executes from internal flash */ FLASH (RX) : origin = FLASH_BASE, length = FLASH_SIZE /* Last flash page */ FLASH_LAST (RX) : origin = FLASH_LAST_BASE, length = FLASH_LAST_SIZE /* Application uses internal RAM for data */ SRAM (RWX) : origin = RAM_BASE, length = RAM_SIZE } /****************************************************************************** Section allocation in memory *****************************************************************************/ SECTIONS { .intvecs : > FLASH_BASE /* flash_last_text { mac_user_config.obj(.text) macTask.obj(.text) hmac_rom_init.obj (.const) osal_port.obj (.text) } > FLASH_LAST */ .text : >> FLASH_LAST | FLASH .const : > FLASH .constdata : > FLASH .rodata : > FLASH .cinit : > FLASH .pinit : > FLASH .init_array : > FLASH .emb_text : > FLASH .ccfg : > FLASH_LAST (HIGH) GROUP > SRAM { .data .bss .vtable .vtable_ram vtable_ram .sysmem .nonretenvar } LOAD_END(heapStart) .stack : > SRAM (HIGH) LOAD_START(heapEnd) } /* Create global constant that points to top of stack */ /* CCS: Change stack size under Project Properties */ __STACK_TOP = __stack + __STACK_SIZE;