/******************************************************************************

 @file  bim_main.c

 @brief This module contains the definitions for the main functionality of a
        Boot  Image Manager for on chip OAD.

 Group: CMCU
 $Target Device: DEVICES $

 ******************************************************************************
 $License: BSD3 2018 $
 ******************************************************************************
 $Release Name: PACKAGE NAME $
 $Release Date: PACKAGE RELEASE DATE $
 *****************************************************************************/

/*******************************************************************************
 *                                          Includes
 */
#include <stdint.h>
#include <string.h>
#include <ti/devices/DeviceFamily.h>
#include DeviceFamily_constructPath(driverlib/flash.h)
#include DeviceFamily_constructPath(driverlib/watchdog.h)
#include DeviceFamily_constructPath(inc/hw_prcm.h)

#include "ti/common/cc26xx/crc/crc32.h"
#include "ti/common/cc26xx/flash_interface/flash_interface.h"
#include "ti/common/cc26xx/bim/bim_util.h"
#include "ti/common/cc26xx/oad/oad_image_header.h"

#ifdef __IAR_SYSTEMS_ICC__
#include <intrinsics.h>
#endif

#if defined(DEBUG_BIM) || defined(BIM_BLINK_LED_NO_VALID_IMAGE)
#include DeviceFamily_constructPath(driverlib/gpio.h)
#include "ti/common/flash/no_rtos/extFlash/bsp.h"
#include "ti/common/cc26xx/debug/led_debug.h"
#endif

#if defined(SECURITY)
#include "sign_util.h"
#if defined(DeviceFamily_CC26X2) || defined(DeviceFamily_CC13X2) || defined(DeviceFamily_CC13X2X7) || defined(DeviceFamily_CC26X2X7)
#include "sha2_driverlib.h"
#else
#include DeviceFamily_constructPath(driverlib/rom_sha256.h)
#endif /* DeviceFamily_CC26X2 || DeviceFamily_CC13X2 || DeviceFamily_CC13X2X7 || DeviceFamily_CC26X2X7 */
#endif

#if defined(BIM_DUAL_ONCHIP_IMAGE)
#if defined(DEBUG_BIM) || !defined(SECURITY)
    // DUAL Image BIM is considered a strictly production ready variant. DEBUG_BIM cannot be used as
    // it would skip key security steps.
    #error "Error: DUAL ON CHIP BIM needs the macro SECURITY to be enabled & DEBUG_BIM to be disabled!"
#endif
#endif
/*******************************************************************************
 *                                          Constants
 */

/* Customer to update these as per their images */
#ifdef BIM_DUAL_ONCHIP_IMAGE
#define IMAGE_1_HDR_START_PAGE_NUM (0)
#define IMAGE_2_HDR_START_PAGE_NUM (42)
#if(IMAGE_2_HDR_START_PAGE_NUM <= IMAGE_1_HDR_START_PAGE_NUM)
    #error "Error: Ensure Image 2 Header starts at a higher flash page as compared to Image 1 Header!"
#endif

/* Customer to update these as per their images */
/* In the current example:*/
/* Flash pages 0 to 20 is slot 1 */
/* Flash pages 21 & 22 are being used as shared NV between both the images */
/* Flash pages 23 to 42 is slot 2 */
/* Flash page 43 is BIM + CCFG */
/* Total flash pages on CC26x2, CC13x2 is 44 pages */
#define IMAGE_1_START_FLASH_PAGE_NUM (IMAGE_1_HDR_START_PAGE_NUM)
#define IMAGE_1_END_FLASH_PAGE_NUM   (41)
#define IMAGE_2_START_FLASH_PAGE_NUM (IMAGE_2_HDR_START_PAGE_NUM)
#define IMAGE_2_END_FLASH_PAGE_NUM   (83)

#if(IMAGE_2_START_FLASH_PAGE_NUM <= IMAGE_1_START_FLASH_PAGE_NUM)
    #error "Error: Ensure Image 2 starts at a higher flash page as compared to Image 1!"
#endif
#if(IMAGE_1_END_FLASH_PAGE_NUM <= IMAGE_1_START_FLASH_PAGE_NUM)
    #error "Error: Incorrect image 1: end flash page number is less than start flash page number!"
#endif
#if(IMAGE_2_END_FLASH_PAGE_NUM <= IMAGE_2_START_FLASH_PAGE_NUM)
    #error "Error: Incorrect image 2: end flash page number is less than start flash page number!"
#endif
#if(IMAGE_2_END_FLASH_PAGE_NUM <= IMAGE_1_END_FLASH_PAGE_NUM)
    #error "Error: Ensure Image 2 ends at a higher flash page as compared to Image 1!"
#endif
#if(IMAGE_2_END_FLASH_PAGE_NUM > 86)
    #error "Error: CC13x2/26x2 devices have only 44 flash pages & 43th flash page is reserved for BIM + CCFG !"
#endif

#define IMG_TYPE_NO_IMAGE_PRESENT           (uint8_t)(0x00)
#define IMG_TYPE_IMAGE_PRESENT              (uint8_t)(0x01)
#define IMG_TYPE_INVALID_APPSTACKLIB_IMG    (uint8_t)(0x00)
#define IMG_TYPE_VALID_APPSTACKLIB_IMG      (uint8_t)(0x02)

#define IMG_PRESENT_MASK  (uint8_t)(0x01)
#define IMG_VALIDITY_MASK (uint8_t)(0x02)

#define BIM_ONCHIP_MAX_NUM_SEARCHES (2)
#endif //BIM_DUAL_ONCHIP_IMAGE


#if defined (SECURITY)
#define SHA_BUF_SZ                      EFL_PAGE_SIZE
#endif

#define SUCCESS                         0
#define FAIL                           -1

/*******************************************************************************
 * LOCAL VARIABLES
 */

#ifndef DEBUG_BIM
static uint32_t intFlashPageSize;       /* Size of internal flash page */
#endif

#ifdef BIM_DUAL_ONCHIP_IMAGE
uint8_t img1_status = IMG_TYPE_NO_IMAGE_PRESENT;
uint8_t img2_status = IMG_TYPE_NO_IMAGE_PRESENT;
#endif

#if (defined(SECURITY))

#if defined(__IAR_SYSTEMS_ICC__)
__no_init uint8_t shaBuf[SHA_BUF_SZ];
#elif defined(__TI_COMPILER_VERSION__) || defined(__clang__)
uint8_t shaBuf[SHA_BUF_SZ];
#endif

/* Cert element stored in flash where public keys in Little Endian format*/
#ifdef __TI_COMPILER_VERSION__
#pragma DATA_SECTION(_secureCertElement, ".cert_element")
#pragma RETAIN(_secureCertElement)
const certElement_t _secureCertElement =
#elif __clang__
const certElement_t _secureCertElement __attribute__((section(".cert_element"))) =
#elif  defined(__IAR_SYSTEMS_ICC__)
#pragma location=".cert_element"
const certElement_t _secureCertElement @ ".cert_element" =
#endif
{
  .version    = SECURE_SIGN_TYPE,
  .len        = SECURE_CERT_LENGTH,
  .options    = SECURE_CERT_OPTIONS,
  .signerInfo = {0xb0,0x17,0x7d,0x51,0x1d,0xec,0x10,0x8b},
  .certPayload.eccKey.pubKeyX = {0xd8,0x51,0xbc,0xa2,0xed,0x3d,0x9e,0x19,0xb7,0x33,0xa5,0x2f,0x33,0xda,0x05,0x40,0x4d,0x13,0x76,0x50,0x3d,0x88,0xdf,0x5c,0xd0,0xe2,0xf2,0x58,0x30,0x53,0xc4,0x2a},
  .certPayload.eccKey.pubKeyY = {0xb9,0x2a,0xbe,0xef,0x66,0x5f,0xec,0xcf,0x56,0x16,0xcc,0x36,0xef,0x2d,0xc9,0x5e,0x46,0x2b,0x7c,0x3b,0x09,0xc1,0x99,0x56,0xd9,0xaf,0x95,0x81,0x63,0x23,0x7b,0xe7}
 };

uint32_t eccWorkzone[SECURE_FW_ECC_NIST_P256_WORKZONE_LEN_IN_BYTES + SECURE_FW_ECC_BUF_TOTAL_LEN(SECURE_FW_ECC_NIST_P256_KEY_LEN_IN_BYTES)*5] = {0};
uint8_t headerBuf[HDR_LEN_WITH_SECURITY_INFO];

#endif

/*******************************************************************************
 * EXTERN FUNCTIONS
 */


/*******************************************************************************
 * LOCAL FUNCTIONS
 */
static void Bim_findImage(uint8_t flashPageNum, uint8_t imgType);

#ifdef BIM_DUAL_ONCHIP_IMAGE
inline static void BIM_updateImgStatus(uint8_t flashPageNum, uint8_t status);
static void Bim_UpdateExecValidImg();
#ifdef BIM_ERASE_INVALID_IMAGE
static uint8_t Bim_EraseOnchipFlashPages(uint8_t startPage, uint8_t endPage);
#else
inline static void Bim_updateVerifStatus(uint8_t flashPageNum, uint8_t secStatus);
#endif //BIM_ERASE_INVALID_IMAGE
#endif //BIM_DUAL_ONCHIP_IMAGE

#if defined(SECURITY)

#ifndef DEBUG_BIM

static bool    Bim_checkForSecSegmnt(uint32_t iflStartAddr, uint32_t imgLen);
static uint8_t Bim_verifyImage(uint32_t iflStartAddr);

#endif

// Function which is used to verify the authenticity of the OAD commands
int8_t Bim_payloadVerify(uint8_t ver, uint32_t cntr, uint32_t payloadlen,
                          uint8_t  *dataPayload, uint8_t *signPayload,
                          ecdsaSigVerifyBuf_t *ecdsaSigVerifyBuf);

// Creating a section for the function pointer, so that it can be easily accessed by OAD application(s)
#ifdef __TI_COMPILER_VERSION__
#pragma DATA_SECTION(_fnPtr, ".fnPtr")
#pragma RETAIN(_fnPtr)
const uint32_t _fnPtr = (uint32_t)&Bim_payloadVerify;
#elif  defined(__IAR_SYSTEMS_ICC__)
#pragma location=".fnPtr"
const uint32_t _fnPtr @ ".fnPtr" = (uint32_t)&Bim_payloadVerify;
#endif // #ifdef __TI_COMPILER_VERSION__

#endif //#if defined (SECURITY)


#if defined(SECURITY)
#ifndef DEBUG_BIM
/*******************************************************************************
 * @fn         Bim_checkForSecSegmnt
*
*  @brief      Check for Security Segment. Reads through the headers in the .bin
*              file. If a security header is found the function checks to see if
*              the header has a populated segment.
*
*  @param       iFlStrAddr - The start address in internal flash of the binary image
*  @param       imgLen - Length of the image over which presence of security segment
*               is searched
*  @return      0  - valid security segment not found
*  @return      1  - valid security segment found
*
*/
static bool Bim_checkForSecSegmnt(uint32_t iFlStrAddr, uint32_t imgLen)
{
    bool securityFound = false;
    uint8_t endOfSegment = 0;
    uint8_t segmentType = DEFAULT_STATE;
    uint32_t segmentLength = 0;
    uint32_t searchAddr =  iFlStrAddr+OAD_IMG_HDR_LEN;

    while(!endOfSegment)
    {
        //extFlashRead(searchAddr, 1, &segmentType);
        readFlash(searchAddr, &segmentType, 1);

        if(segmentType == IMG_SECURITY_SEG_ID)
        {
            /* In this version of BIM, the security header will ALWAYS be present
               But the payload will sometimes not be there. If this finds the
               header, the payload is also checked for existence. */
            searchAddr += SIG_OFFSET;
            uint32_t sigVal = 0;
            readFlash(searchAddr, (uint8_t *)&sigVal, sizeof(uint32_t));

            if(sigVal != 0) //Indicates the presence of a signature
            {
                endOfSegment = 1;
                securityFound = true;
            }
            else
            {
                break;
            }
        }
        else
        {
            searchAddr += SEG_LEN_OFFSET;
            if((searchAddr + sizeof(uint32_t)) > (iFlStrAddr + imgLen))
            {
                break;
            }
            //extFlashRead(searchAddr, sizeof(uint32_t), (uint8_t *)&segmentLength);
            readFlash(searchAddr, (uint8_t *)&segmentLength, sizeof(uint32_t));

            searchAddr += (segmentLength - SEG_LEN_OFFSET);
            if((searchAddr) > (iFlStrAddr + imgLen))
            {
                break;
            }
        }
    }

    return securityFound;
}//end of function

/*******************************************************************************
 * @fn      Bim_verifyImage
 *
 * @brief   Verifies the image stored on internal flash using ECDSA-SHA256
 *
 * @param   iflStartAddr - internal flash address of the image to be verified.
 *
 * @return  Zero when successful. Non-zero, otherwise..
 */
static uint8_t Bim_verifyImage(uint32_t iflStartAddr)
{
    uint8_t verifyStatus = (uint8_t)FAIL;

    /* clear the ECC work zone Buffer */
    uint32_t *eccPayloadWorkzone = eccWorkzone;
    memset(eccPayloadWorkzone, 0, sizeof(eccWorkzone));

    /* Read in the header to get the image signature */
    readFlash(iflStartAddr, headerBuf, HDR_LEN_WITH_SECURITY_INFO);

    // First verify signerInfo
    verifyStatus = verifyCertElement(&headerBuf[SEG_SIGERINFO_OFFSET]);
    if(verifyStatus != SUCCESS)
    {
        return verifyStatus;
    }

    // Get the hash of the image
    uint8_t *finalHash;

    finalHash = computeSha2Hash(iflStartAddr, shaBuf, SHA_BUF_SZ, false);

    if(NULL == finalHash)
    {
        verifyStatus = (uint8_t)FAIL;
        return verifyStatus;
    }

    // Verify the hash
    // Create temp buffer used for ECDSA sign verify, it should 6*ECDSA_KEY_LEN
    uint8_t tempWorkzone[ECDSA_SHA_TEMPWORKZONE_LEN];
    memset(tempWorkzone, 0, ECDSA_SHA_TEMPWORKZONE_LEN);

    verifyStatus = bimVerifyImage_ecc(_secureCertElement.certPayload.eccKey.pubKeyX,
                                      _secureCertElement.certPayload.eccKey.pubKeyY,
                                       finalHash,
                                       &headerBuf[SEG_SIGNR_OFFSET],
                                       &headerBuf[SEG_SIGNS_OFFSET],
                                       eccWorkzone,
                                       tempWorkzone);

    if(verifyStatus == SECURE_FW_ECC_STATUS_VALID_SIGNATURE)
    {
        verifyStatus = SUCCESS;
    }
    else
    {
        verifyStatus = (uint8_t)FAIL;
    }
    return verifyStatus;

}//end of function

#endif // DEBUG_BIM

/*******************************************************************************
 * @fn      Bim_payloadVerify
 *
 * @brief   Function in BIM to verify the payload of an OTA command.
 *
 * @param   ver - version of the security algorithm
 *          cntr - time-stamp /counter value use to verify the payload
 *          payloadlen - payload length in bytes
 *          dataPayload - pointer to data payload to be verified
 *          signPayload - pointer to sign payload
 *          eccPayloadWorkzone - pointer to the workzone used to verify the command
 *          shaPayloadWorkzone - pointer to the workzone used to generate a hash of the command
 *
 *
 * @return  Zero when successful. Non-zero, otherwise..
 */
int8_t Bim_payloadVerify(uint8_t ver, uint32_t cntr, uint32_t payloadlen,
                         uint8_t  *dataPayload, uint8_t *signPayload,
                         ecdsaSigVerifyBuf_t *ecdsaSigVerifyBuf)
{
    signPld_ECDSA_P256_t *signPld = (signPld_ECDSA_P256_t*)signPayload;

    uint8_t *sig1 = signPld->signature;
    uint8_t *sig2 = &signPld->signature[32];
    int8_t status = FAIL;
    int8_t verifyStatus = FAIL;
    uint8_t *finalHash = ecdsaSigVerifyBuf->tempWorkzone;

    memset(ecdsaSigVerifyBuf->tempWorkzone, 0, sizeof(ECDSA_SHA_TEMPWORKZONE_LEN));

    if (ver == 1)
    {
#if defined(DeviceFamily_CC26X2) || defined(DeviceFamily_CC13X2) || defined(DeviceFamily_CC13X2X7) || defined(DeviceFamily_CC26X2X7)
        SHA2_open();
        SHA2_addData(dataPayload, payloadlen);
        SHA2_finalize(finalHash);
        SHA2_close();
#else
        SHA256_Workzone sha256_workzone;
        SHA256_init(&sha256_workzone);
        SHA256_full(&sha256_workzone, finalHash, dataPayload, payloadlen);
#endif /* DeviceFamily_CC26X2 || DeviceFamily_CC13X2 || DeviceFamily_CC13X2X7 || DeviceFamily_CC26X2X7 */

        // First verify signerInfo
        verifyStatus = verifyCertElement(signPld->signerInfo);
        if(verifyStatus != SUCCESS)
        {
            return FAIL;
        }

        verifyStatus = bimVerifyImage_ecc(_secureCertElement.certPayload.eccKey.pubKeyX,
                                          _secureCertElement.certPayload.eccKey.pubKeyY,
                                           finalHash, sig1, sig2,
                                           ecdsaSigVerifyBuf->eccWorkzone,
                                           (ecdsaSigVerifyBuf->tempWorkzone + ECDSA_KEY_LEN));
        if(verifyStatus == (int8_t)SECURE_FW_ECC_STATUS_VALID_SIGNATURE)
        {
            status = SUCCESS;
        }
    }
    return status;
}//end of function

#endif /* if defined(SECURITY) */


/*******************************************************************************
 * @fn     Bim_findImage
 *
 * @brief  Performs various checks on the image, if present at
 *         flash page number. In case on non-dual onchip case,
 *         it jumps to a certain image if all checks pass. In
 *         dual image on-chip case, the image status variables
 *         are updated based on checks performed.
 *
 * @param  flashPageNum - flash page number
 *         imgType      - image type to be searched
 *
 * @return None.
 */
static void Bim_findImage(uint8_t flashPageNum, uint8_t imgType)
{
    imgHdr_t imgHdr;
#ifndef BIM_DUAL_ONCHIP_IMAGE
    uint8_t securityStatus = VERIFY_FAIL;
#else
    uint8_t imgStatus;
#endif //BIM_DUAL_ONCHIP_IMAGE

    /* Read flash to find OAD image identification value */
    readFlashPg(flashPageNum, 0, &imgHdr.fixedHdr.imgID[0], OAD_IMG_ID_LEN);

    /* Check imageID bytes */
    if ((imgIDCheck(&(imgHdr.fixedHdr)) != true))
    {
#ifdef BIM_DUAL_ONCHIP_IMAGE
       imgStatus = IMG_TYPE_NO_IMAGE_PRESENT;
       BIM_updateImgStatus(flashPageNum, imgStatus);
#endif
        /* return so that same process can be repeated*/
        return;
    }
    else //valid OAD image ID value is found
    {
        /* Read whole of fixed header in the image header */
        readFlashPg(flashPageNum, 0, (uint8_t *)&imgHdr, OAD_IMG_HDR_LEN);

        if(imgType != imgHdr.fixedHdr.imgType || (evenBitCount(imgHdr.fixedHdr.imgVld) == false))
        {
#ifdef BIM_DUAL_ONCHIP_IMAGE
            imgStatus = (IMG_TYPE_IMAGE_PRESENT | IMG_TYPE_INVALID_APPSTACKLIB_IMG);
            BIM_updateImgStatus(flashPageNum, imgStatus);
#endif
            /* didn't find the image type we are looking for */
            /* Or the image we found is considered 'invalid' */
            /* return so that same process can be repeated */
            return;
        }

        /* Image type matched: proceed with further checks */

        /* check BIM and Metadata version and CRC status (if need be). If DEBUG_BIM is enabled
         * skip the crc checking and updating the crc status- as crc wouldn't have been
         * calculated at the first place */

        if( (imgHdr.fixedHdr.bimVer != BIM_VER  || imgHdr.fixedHdr.metaVer != META_VER) /* Invalid metadata version */
#ifndef DEBUG_BIM
              ||
           (imgHdr.fixedHdr.crcStat == 0xFC)  /* Invalid CRC */
#endif
          )
        {
#ifdef BIM_DUAL_ONCHIP_IMAGE
            imgStatus = (IMG_TYPE_IMAGE_PRESENT | IMG_TYPE_INVALID_APPSTACKLIB_IMG);
            BIM_updateImgStatus(flashPageNum, imgStatus);
#endif
            /* return so that same process can be repeated*/
            return;
        }
#ifdef AUTHENTICATE_PERSISTENT_IMG
        else if((imgHdr.fixedHdr.imgType == OAD_IMG_TYPE_APPSTACKLIB || imgHdr.fixedHdr.imgType == OAD_IMG_TYPE_PERSISTENT_APP)
                && imgHdr.fixedHdr.crcStat == 0xFF) /* CRC not calculated yet */
#else
        else if(imgHdr.fixedHdr.imgType == OAD_IMG_TYPE_APPSTACKLIB
                && imgHdr.fixedHdr.crcStat == 0xFF) /* CRC not calculated yet */
#endif

        {
#ifndef DEBUG_BIM

            /* Calculate the CRC over the data buffer and update status */
            uint32_t crc32 = 0;
            uint8_t  crcstat = CRC_VALID;
            crc32 = CRC32_calc(flashPageNum, intFlashPageSize, 0, imgHdr.fixedHdr.len, false);

            /* Check if calculated CRC matched with the image header */
            if (crc32 != imgHdr.fixedHdr.crc32)
            {
                /* Update CRC status */
                crcstat = CRC_INVALID;
                writeFlashPg(flashPageNum, CRC_STAT_OFFSET, (uint8_t *)&crcstat, 1);

#ifdef BIM_DUAL_ONCHIP_IMAGE
                imgStatus = (IMG_TYPE_IMAGE_PRESENT | IMG_TYPE_INVALID_APPSTACKLIB_IMG);
                BIM_updateImgStatus(flashPageNum, imgStatus);
#endif
                /* return so that same process can be repeated */
                return;

            } /* if (crc32 != imgHdr.crc32) */

            /* if we have come here: CRC check has passed */
            /* Update CRC status */
            writeFlashPg(flashPageNum, CRC_STAT_OFFSET, (uint8_t *)&crcstat, 1);
#endif
        } /* else if(imgHdr.crcStat == 0xFF) */


#if defined(SECURITY)
        /* populate the start address of the image in the internal flash */
        uint32_t iFlStrAddr = FLASH_ADDRESS(flashPageNum, 0);

        /* Verify the start address and the img is within internal flash bounds */
#ifndef BIM_DUAL_ONCHIP_IMAGE
        if ((iFlStrAddr + imgHdr.fixedHdr.len) > (MAX_ONCHIP_FLASH_PAGES * INTFLASH_PAGE_SIZE))
        {
            /* return so that same process can be repeated */
            return;
        }
#else

        /* verify that start address + length of image is less than the slot boundary */
        if (((iFlStrAddr == IMAGE_1_START_FLASH_PAGE_NUM * INTFLASH_PAGE_SIZE) && /* if slot 1 image */
             ((iFlStrAddr + imgHdr.fixedHdr.len) > IMAGE_2_START_FLASH_PAGE_NUM * INTFLASH_PAGE_SIZE)) ||
            ((iFlStrAddr != IMAGE_1_START_FLASH_PAGE_NUM * INTFLASH_PAGE_SIZE) && /* if slot 2 image */
             ((iFlStrAddr + imgHdr.fixedHdr.len) > MAX_ONCHIP_FLASH_PAGES * INTFLASH_PAGE_SIZE)))
        {
            imgStatus = (IMG_TYPE_IMAGE_PRESENT | IMG_TYPE_INVALID_APPSTACKLIB_IMG);
            BIM_updateImgStatus(flashPageNum, imgStatus);
            /* return so that same process can be repeated */
            return;
        }
#endif //BIM_DUAL_ONCHIP_IMAGE


#ifndef DEBUG_BIM //during debug: the sign is not populated to even verify
        int8_t signVrfyStatus = FAIL;

#ifdef AUTHENTICATE_PERSISTENT_IMG
        if(imgHdr.fixedHdr.imgType == OAD_IMG_TYPE_APPSTACKLIB ||
                imgHdr.fixedHdr.imgType == OAD_IMG_TYPE_PERSISTENT_APP)
#else
        if(imgHdr.fixedHdr.imgType == OAD_IMG_TYPE_APPSTACKLIB)
#endif
        {
            uint8_t securityPresence = false;

            /* check if security segment is present or not in the image */
            securityPresence = Bim_checkForSecSegmnt(iFlStrAddr, imgHdr.fixedHdr.len);

            if(securityPresence)
            {
                /* Calculate the SHA256 of the image */
                uint8_t readSecurityByte[SEC_VERIF_STAT_OFFSET + 1];

                /* Read in the header to check if the signature has already been denied */
                readFlashPg(flashPageNum, 0, &readSecurityByte[0], (SEC_VERIF_STAT_OFFSET + 1));

#ifndef BIM_DUAL_ONCHIP_IMAGE
                if(readSecurityByte[SEC_VERIF_STAT_OFFSET] == DEFAULT_STATE)
#else
                if(readSecurityByte[SEC_VERIF_STAT_OFFSET] != VERIFY_FAIL)
#endif
                {
                    signVrfyStatus = Bim_verifyImage(iFlStrAddr);

                    /* If the signature is invalid, update the sign verification status */
                    if((uint8_t)signVrfyStatus != SUCCESS)
                    {
                        readSecurityByte[SEC_VERIF_STAT_OFFSET] = VERIFY_FAIL;
                        writeFlashPg(flashPageNum, SEC_VERIF_STAT_OFFSET,  &readSecurityByte[SEC_VERIF_STAT_OFFSET], 1);
                    }
#ifndef BIM_DUAL_ONCHIP_IMAGE
                    else
                    {
                        readSecurityByte[SEC_VERIF_STAT_OFFSET] = VERIFY_PASS;
                        writeFlashPg(flashPageNum, SEC_VERIF_STAT_OFFSET,  &readSecurityByte[SEC_VERIF_STAT_OFFSET], 1);
                    }
                }
                else if (readSecurityByte[SEC_VERIF_STAT_OFFSET] == VERIFY_PASS)
                {
                    signVrfyStatus = SUCCESS;
#endif
                }
            } /* if(securityPresence) */
        }
#ifndef AUTHENTICATE_PERSISTENT_IMG
        else
        {
            signVrfyStatus = SUCCESS;
        }
#endif

        /*
         * sign verification has failed or
         * didn't find the security segment in the first place or
         * iFlStrAddr is outside of the authenticated flash space
         */
#ifdef AUTHENTICATE_PERSISTENT_IMG
        /*
         * In the case that  AUTHENTICATE_PERSISTENT_IMG is defined,
         * all image types should be authenticated and therefore no
         * logic for imgType is necessary.
         */
        if((uint8_t)signVrfyStatus != SUCCESS ||
                (imgHdr.fixedHdr.prgEntry < iFlStrAddr) ||
                (imgHdr.fixedHdr.prgEntry > (iFlStrAddr + imgHdr.fixedHdr.len)))
#else
        /*
         *  In the case that AUTHENTICATE_PERSISTENT_IMG is NOT defined,
         *  only imgType == OAD_IMG_TYPE_APPSTACKLIB should be authenticated.
         */
        if((uint8_t)signVrfyStatus != SUCCESS ||
                ((imgHdr.fixedHdr.imgType == OAD_IMG_TYPE_APPSTACKLIB) &&
                ((imgHdr.fixedHdr.prgEntry < iFlStrAddr) ||
                (imgHdr.fixedHdr.prgEntry > (iFlStrAddr + imgHdr.fixedHdr.len)))))
#endif
        {
#ifdef BIM_DUAL_ONCHIP_IMAGE
            imgStatus = (IMG_TYPE_IMAGE_PRESENT | IMG_TYPE_INVALID_APPSTACKLIB_IMG);
            BIM_updateImgStatus(flashPageNum, imgStatus);
#endif
            /* return so that same process can be repeated */
            return;
        }
        else
        {
#ifndef BIM_DUAL_ONCHIP_IMAGE
            securityStatus = VERIFY_PASS;
#endif
        }

#else //DEBUG_BIM is defined
#ifndef BIM_DUAL_ONCHIP_IMAGE
        securityStatus = VERIFY_PASS;
#endif
#endif

#else //SECURITY not defined
#ifndef BIM_DUAL_ONCHIP_IMAGE
        securityStatus = VERIFY_PASS;
#endif
#endif

#ifndef BIM_DUAL_ONCHIP_IMAGE
        /*if we get here, its highly likely we found a valid image to boot to */
        if (VERIFY_PASS == securityStatus)
        {

            jumpToPrgEntry((uint32_t*)imgHdr.fixedHdr.prgEntry);

        }
        else
        {
            /* return so that same process can be repeated */
            return;
        }
#else
        /*if we get here, its highly likely we found a valid image */
        imgStatus = (IMG_TYPE_IMAGE_PRESENT | IMG_TYPE_VALID_APPSTACKLIB_IMG);
        BIM_updateImgStatus(flashPageNum, imgStatus);
#endif //BIM_DUAL_ONCHIP_IMAGE
    }//valid imageID found

    return;
}

#ifdef BIM_DUAL_ONCHIP_IMAGE
/*******************************************************************************
 * @fn     BIM_updateImgStatus
 *
 * @brief  Updates the imgX_status variable based on if
 *         the image being checked is in slot 1 or slot 2.
 *         These global variables will be later consumed in
 *         Bim_UpdateExecValidImg() function.
 *
 * @param  flashPageNum - flash page number
 *
 * @return None.
 */
inline static void BIM_updateImgStatus(uint8_t flashPageNum, uint8_t status)
{
    if( IMAGE_1_HDR_START_PAGE_NUM == flashPageNum ) /* 1st slot */
    {
        img1_status = status;
    }
    else /* 2nd slot */
    {
        img2_status = status;
    }
}

/*******************************************************************************
 * @fn     Bim_updateVerifStatus
 *
 * @brief  Based on the img_status fields populated by Bim_findImage
 *         & anti-roll back check, decide which image to boot to &
 *         update the verifStatus fields in the security header
 *         of the images appropriately.
 *         Also, Jump into the decided upon image.
 *
 * @param  flashPageNum - flash page where the image header starts.
 * @param  secStatus - value to be written into verifStatus field.
 *
 * @return None.
 */
inline static void Bim_updateVerifStatus(uint8_t flashPageNum, uint8_t secStatus)
{
    writeFlashPg(flashPageNum, SEC_VERIF_STAT_OFFSET,  (uint8_t *)&secStatus, 1);
}

#ifdef BIM_ERASE_INVALID_IMAGE
/*******************************************************************************
 * @fn     Bim_EraseOnchipFlashPages
 *
 * @brief  It Erases the onchip flash pages.
 *
 * @param  startPage - Starting page on on-chip flash to be erased
 * @param  endPage  - End page on on-chip flash to be erased
 * @param  pageSize  - flash page size
 *
 * @return - SUCCESS on successful erasure else
 *           FAIL
 */
static uint8_t Bim_EraseOnchipFlashPages(uint8_t startPage, uint8_t endPage)
{
    int8_t status = SUCCESS;

    // Erase the correct amount of pages
    for(uint8_t page = startPage; page <= endPage; ++page)
    {
        uint8_t flashStat = eraseFlashPg(page);
        if(flashStat == FLASH_FAILURE)
        {
            // If we fail to pre-erase, then halt the process
            status = FAIL;
            break;
        }
    }
    return status;
}
#endif // BIM_ERASE_INVALID_IMAGE

/*******************************************************************************
 * @fn     Bim_UpdateExecValidImg
 *
 * @brief  Based on the img_status fields populated by Bim_findImage
 *         & anti-roll back check, decide which image to boot to &
 *         update the verifStatus fields in the security header
 *         of the images appropriately.
 *         Also, Jump into the decided upon image.
 *
 * @param  None.
 *
 * @return None.
 */
static void Bim_UpdateExecValidImg()
{
    /* Declare local variables used in the main function */
    imgHdr_t imgHdr_1, imgHdr_2;
    uint8_t secVer_1 = 0, secVer_2 = 0, verifStat_1 = 0, verifStat_2 = 0;
    uint8_t isPresImg_1 = img1_status & IMG_PRESENT_MASK;
    uint8_t isPresImg_2 = img2_status & IMG_PRESENT_MASK;
    uint8_t isValidImg_1 = img1_status & IMG_VALIDITY_MASK;
    uint8_t isValidImg_2 = img2_status & IMG_VALIDITY_MASK;

    if((isValidImg_1) && !(isValidImg_2)) /* first image is valid & 2nd image is not valid */
    {
        /* mark the verifStatus fields accordingly */
        if(isPresImg_2)
        {
#ifdef BIM_ERASE_INVALID_IMAGE
            Bim_EraseOnchipFlashPages(IMAGE_2_START_FLASH_PAGE_NUM, IMAGE_2_END_FLASH_PAGE_NUM);
#else
            Bim_updateVerifStatus(IMAGE_2_HDR_START_PAGE_NUM, VERIFY_FAIL);
#endif
        }
        Bim_updateVerifStatus(IMAGE_1_HDR_START_PAGE_NUM, VERIFY_PASS_CURRENT);
        readFlashPg(IMAGE_1_HDR_START_PAGE_NUM, 0, (uint8_t *)&imgHdr_1, OAD_IMG_HDR_LEN);
        /* jump to the image */
        jumpToPrgEntry((uint32_t*)imgHdr_1.fixedHdr.prgEntry);
    }
    else if(!(isValidImg_1) && (isValidImg_2))
    {
        /* mark the verifStatus fields accordingly */
        if(isPresImg_1)
        {
#ifdef BIM_ERASE_INVALID_IMAGE
            Bim_EraseOnchipFlashPages(IMAGE_1_START_FLASH_PAGE_NUM, IMAGE_1_END_FLASH_PAGE_NUM);
#else
            Bim_updateVerifStatus(IMAGE_1_HDR_START_PAGE_NUM, VERIFY_FAIL);
#endif
        }
        Bim_updateVerifStatus(IMAGE_2_HDR_START_PAGE_NUM, VERIFY_PASS_CURRENT);
        /* jump to the image */
        readFlashPg(IMAGE_2_HDR_START_PAGE_NUM, 0, (uint8_t *)&imgHdr_2, OAD_IMG_HDR_LEN);
        jumpToPrgEntry((uint32_t*)imgHdr_2.fixedHdr.prgEntry);
    }
    else if((isValidImg_1) && (isValidImg_2)) /* both the images are valid so far */
    {
        readFlashPg(IMAGE_1_HDR_START_PAGE_NUM, 0, (uint8_t *)&imgHdr_1, (OAD_IMG_HDR_LEN + sizeof(securityInfoSeg_t)));
        readFlashPg(IMAGE_2_HDR_START_PAGE_NUM, 0, (uint8_t *)&imgHdr_2, (OAD_IMG_HDR_LEN + sizeof(securityInfoSeg_t)));

        secVer_1 = imgHdr_1.secInfoSeg.secVer;
        secVer_2 = imgHdr_2.secInfoSeg.secVer;

        verifStat_1 = imgHdr_1.secInfoSeg.verifStat ;
        verifStat_2 = imgHdr_2.secInfoSeg.verifStat ;

        /* image 1 is new */
        if((DEFAULT_STATE == verifStat_1) && (DEFAULT_STATE != verifStat_2))
        {
            if(secVer_1 > secVer_2)
            {

#ifdef BIM_ERASE_INVALID_IMAGE
                Bim_EraseOnchipFlashPages(IMAGE_2_START_FLASH_PAGE_NUM, IMAGE_2_END_FLASH_PAGE_NUM);
#else
                Bim_updateVerifStatus(IMAGE_2_HDR_START_PAGE_NUM, VERIFY_FAIL);
#endif
                /* switch to new image */
                Bim_updateVerifStatus(IMAGE_1_HDR_START_PAGE_NUM, VERIFY_PASS_CURRENT);
                jumpToPrgEntry((uint32_t*)imgHdr_1.fixedHdr.prgEntry);
            }
            else if( secVer_1 < secVer_2)
            {
#ifdef BIM_ERASE_INVALID_IMAGE
                Bim_EraseOnchipFlashPages(IMAGE_1_START_FLASH_PAGE_NUM, IMAGE_1_END_FLASH_PAGE_NUM);
#else
                Bim_updateVerifStatus(IMAGE_1_HDR_START_PAGE_NUM, VERIFY_FAIL);
#endif
                /* Do not switch to new image */
                Bim_updateVerifStatus(IMAGE_2_HDR_START_PAGE_NUM, VERIFY_PASS_CURRENT);
                jumpToPrgEntry((uint32_t*)imgHdr_2.fixedHdr.prgEntry);
            }
            else /* same sec version */
            {
                /* switch to new image */
                Bim_updateVerifStatus(IMAGE_2_HDR_START_PAGE_NUM,  VERIFY_PASS_NOT_CURRENT);
                Bim_updateVerifStatus(IMAGE_1_HDR_START_PAGE_NUM, VERIFY_PASS_CURRENT);
                jumpToPrgEntry((uint32_t*)imgHdr_1.fixedHdr.prgEntry);
            }
        } /* end of if image 1 is new */
        /* image 2 is new */
        else if((DEFAULT_STATE != verifStat_1) && (DEFAULT_STATE == verifStat_2))
        {
            if(secVer_2 > secVer_1)
            {
#ifdef BIM_ERASE_INVALID_IMAGE
                Bim_EraseOnchipFlashPages(IMAGE_1_START_FLASH_PAGE_NUM, IMAGE_1_END_FLASH_PAGE_NUM);
#else
                Bim_updateVerifStatus(IMAGE_1_HDR_START_PAGE_NUM, VERIFY_FAIL);
#endif
                /* switch to new image */
                Bim_updateVerifStatus(IMAGE_2_HDR_START_PAGE_NUM, VERIFY_PASS_CURRENT);
                jumpToPrgEntry((uint32_t*)imgHdr_2.fixedHdr.prgEntry);
            }
            else if( secVer_2 < secVer_1)
            {
#ifdef BIM_ERASE_INVALID_IMAGE
                Bim_EraseOnchipFlashPages(IMAGE_2_START_FLASH_PAGE_NUM, IMAGE_2_END_FLASH_PAGE_NUM);
#else
                Bim_updateVerifStatus(IMAGE_2_HDR_START_PAGE_NUM, VERIFY_FAIL);
#endif
                /* Do not switch to new image */
                Bim_updateVerifStatus(IMAGE_1_HDR_START_PAGE_NUM, VERIFY_PASS_CURRENT);
                jumpToPrgEntry((uint32_t*)imgHdr_1.fixedHdr.prgEntry);
            }
            else /* same sec version */
            {
                /* switch to new image */
                Bim_updateVerifStatus(IMAGE_1_HDR_START_PAGE_NUM,  VERIFY_PASS_NOT_CURRENT);
                Bim_updateVerifStatus(IMAGE_2_HDR_START_PAGE_NUM, VERIFY_PASS_CURRENT);
                jumpToPrgEntry((uint32_t*)imgHdr_2.fixedHdr.prgEntry);
            }
        } /* end of if image 2 is new */
        /* neither of the images are new */
        else if((DEFAULT_STATE != verifStat_1) & (DEFAULT_STATE != verifStat_2))
        {
#ifdef FEATURE_SWITCH_VALID_IMAGES
            /* pick the one with higher number of bits in imgVld field */
            if(imgHdr_1.fixedHdr.imgVld > imgHdr_2.fixedHdr.imgVld )
            {
                /* no need to update the status fields */
                /* jump to the image */
                jumpToPrgEntry((uint32_t*)imgHdr_1.fixedHdr.prgEntry);
            }
            else if(imgHdr_1.fixedHdr.imgVld < imgHdr_2.fixedHdr.imgVld)
            {
                /* no need to update the status fields */
                /* jump to the image */
                jumpToPrgEntry((uint32_t*)imgHdr_2.fixedHdr.prgEntry);
            }
            else /*both are equal*/
#endif
            {
                /* boot into image that has been marked as the current image previously */
                if((VERIFY_PASS_CURRENT == imgHdr_1.secInfoSeg.verifStat) &&
                   (VERIFY_PASS_NOT_CURRENT == imgHdr_2.secInfoSeg.verifStat))
                {
                    jumpToPrgEntry((uint32_t*)imgHdr_1.fixedHdr.prgEntry);
                }
                else if((VERIFY_PASS_CURRENT == imgHdr_2.secInfoSeg.verifStat) &&
                        (VERIFY_PASS_NOT_CURRENT == imgHdr_1.secInfoSeg.verifStat))
                {
                    jumpToPrgEntry((uint32_t*)imgHdr_2.fixedHdr.prgEntry);
                }
                /* else: any other case: something is wrong */
            }

        } /* if neither of the images are new */

    } /* both the images are valid */

} /* end of function Bim_UpdateExecValidImg */


#endif // BIM_DUAL_ONCHIP_IMAGE



/*******************************************************************************
 * @fn          main
 *
 * @brief       C-code main function.
 *
 * input parameters
 *
 * None.
 *
 * output parameters
 *
 * None.
 *
 * @return      None.
 */
int main(void)
{
#ifdef __IAR_SYSTEMS_ICC__
  __set_CONTROL(0);
#endif

#ifndef DEBUG_BIM
    /* Read and populate the static variable intFlashPageSize */
    intFlashPageSize = FlashSectorSizeGet();
#endif
    uint8_t imgType;
    uint8_t flashPgNum;

#ifndef BIM_DUAL_ONCHIP_IMAGE
     /* First look for an application image*/
    imgType = OAD_IMG_TYPE_APPSTACKLIB;
#ifdef APP_HDR_LOC
    flashPgNum = APP_HDR_ADDR/ intFlashPageSize;
#else
    flashPgNum = 0x00;
#endif

    Bim_findImage(flashPgNum, imgType);

    /* If the application image isn't found, look for a persistent image */
    imgType = OAD_IMG_TYPE_PERSISTENT_APP;
#ifdef PERSIST_HDR_LOC
    flashPgNum = PERSIST_HDR_ADDR / intFlashPageSize;

    Bim_findImage(flashPgNum, imgType);
#else
    flashPgNum++;

    while(flashPgNum < MAX_ONCHIP_FLASH_PAGES)
    {
        Bim_findImage(flashPgNum, imgType);
        flashPgNum++;
    }
#endif
#else // BIM_DUAL_ONCHIP_IMAGE

    /* Check if image is present in slot 1, if yes, do checks on it */
    imgType = OAD_IMG_TYPE_APPSTACKLIB;
    flashPgNum = IMAGE_1_HDR_START_PAGE_NUM;
    Bim_findImage(flashPgNum, imgType);

    /* Check if image is present in slot 2, if yes, do checks on it */
    flashPgNum = IMAGE_2_HDR_START_PAGE_NUM;
    Bim_findImage(flashPgNum, imgType);

    /* once here, do checks on which image to boot to & boot into it */
    Bim_UpdateExecValidImg();
#endif

    /* If we get here, that means there is an Issue: No valid image found */
#if defined(DEBUG_BIM) || defined(BIM_BLINK_LED_NO_VALID_IMAGE)

    powerUpGpio();
    while(1)
    {
        lightRedLed();
    }

#else /* ifdef DEBUG_BIM */
    /* Set the device to the lowest power state. Does not return. */
    setLowPowerMode();

    return(0);
#endif

} /* end of main function */

/**************************************************************************************************
*/