MODE 5xx USB VERBOSE // to erase device, should fail RX_PASSWORD erase_pass.txt DELAY 1000 // delay for mass erase RX_PASSWORD ff_pass.txt RX_DATA_BLOCK_FAST RAM_BSL.00.05.04.34.txt SET_PC 0x2504 DELAY 3000 //------------------------------------------------------ // The USB BSL is now in RAM, and is started // We must now re-initialize communication //------------------------------------------------------ MODE 5xx USB //------------------------------------------------------ // Now we simply demo the use of the supported functions //------------------------------------------------------ RX_DATA_BLOCK_FAST 5529_LED_BLINK.txt TX_DATA_BLOCK 0x8000 0x100 Data_Read_1.txt CRC_CHECK 0x8000 0x10 0xCFB8 ERASE_SEGMENT 0x8000 TX_DATA_BLOCK 0x8000 0x100 Data_Read_2.txt CRC_CHECK 0x8000 0x100 0x5B2F TX_BSL_VERSION RX_DATA_BLOCK_FAST 5529_LED_BLINK.txt SET_PC 0x8000