#include "BSL_Device_File.h"
#include "BSL430_PI.h"
#include "BSL430_Command_Interpreter.h"
#include "BSL430_Command_Definitions.h"
/*******************************************************************************
Change Log:
--------------------------------------------------------------------------------
Version 0x52 
3.15.10  LCW   changed to DCORSEL_4
--------------------------------------------------------------------------------
Version 0x53 
5.18.10  LCW   made buffer size unsized to align with Interface
--------------------------------------------------------------------------------
*******************************************************************************/
//errors
#define HEADER_INCORRECT (PI_COMMAND_UPPER+0x01)
#define CHECKSUM_INCORRECT (PI_COMMAND_UPPER+0x02) 
#define PACKET_SIZE_ZERO (PI_COMMAND_UPPER+0x03)
#define PACKET_SIZE_TOO_BIG (PI_COMMAND_UPPER+0x04)
#define UNKNOWN_ERROR (PI_COMMAND_UPPER+0x05)
// errors for PI commands
#define UNKNOWN_BAUD_RATE (PI_COMMAND_UPPER+0x06)

// TA PI Commands
#define CHANGE_BAUD_RATE (PI_COMMAND_UPPER + 0x02)

// 4800 (unused)
#define BAUD_4800   0x01
#define BAUD_9600   0x02
#define BAUD_19200  0x03
#define BAUD_38400  0x04
#define BAUD_57600  0x05
#define BAUD_115200 0x06

#define MAX_BUFFER_SIZE 260

char verifyData( int checksum );
char receiveByte();
void sendByte( char data );
void interpretPI_Command();
void init_USCI( char baud_rate );

__no_init char *BSL430_ReceiveBuffer;
__no_init char *BSL430_SendBuffer;
__no_init unsigned int BSL430_BufferSize;
#pragma data_alignment=2
__no_init char RAM_Buf[MAX_BUFFER_SIZE];

#define USCIA_VERSION 0x03

#if 0
const unsigned char BSL430_PI_Version @ "BSL430_VERSION_PI" = (BSL430_USCIA_PI+USCIA_VERSION);
#pragma required=BSL430_PI_Version
#else
const unsigned char BSL430_PI_Version = (BSL430_USCIA_PI+USCIA_VERSION);
#endif
/*******************************************************************************
*Function:    init
*Description: Initialize the USCI and Ports
*Parameters: 
*******************************************************************************/
void PI_init()
{
  volatile int i;
  BSL430_ReceiveBuffer = RAM_Buf;
  BSL430_SendBuffer = RAM_Buf;

  UCSCTL4 = SELA__REFOCLK + SELM__DCOCLK + SELS__DCOCLK;  // to do check SELA
  
  UCSCTL0 = 0x000;                          // Set DCO to lowest Tap
  
  UCSCTL1 = DCORSEL_4;                      // 8MHz nominal DCO
  UCSCTL5 = DIVM_0 + DIVS_0;
  UCSCTL2 = FLLD_2 | (((DCO_SPEED/ACLK_SPEED)/4) - 1); // 8MHz

  // init led
  P8DIR |= BIT4; //Set LED0 as output
  P8OUT |= BIT4; //Set LED0 by default
                
  init_USCI( BAUD_9600 );
  
}//init


/*******************************************************************************
*Function:    receivePacket
*Description: Reads an entire packet, verifies it, and sends it to the core to be interpreted
*******************************************************************************/
char PI_receivePacket()
{
  char RX_StatusFlags = RX_PACKET_ONGOING;
  char dataByte = 0;
  int dataPointer = 0;
  volatile int checksum = 0;
  while( RX_StatusFlags == RX_PACKET_ONGOING )
  {
    dataByte = receiveByte();               // get another byte from host
    if( dataPointer == 0 )                  // first byte is the size of the Core packet
    {
      if ( dataByte != 0x80 )               // first byte in packet should be 0x80
      {
        sendByte( HEADER_INCORRECT );
        RX_StatusFlags = RX_ERROR_RECOVERABLE;
      }
      else
      {
        dataPointer++;
      }
    }
    else if( dataPointer == 1 )             // first byte is the size of the Core packet
    {
      BSL430_BufferSize = dataByte;
      dataPointer++;
    }
    else if( dataPointer == 2 )
    {
      BSL430_BufferSize |= (int)dataByte<<8;
      if( BSL430_BufferSize == 0 )
      {
        sendByte( PACKET_SIZE_ZERO );
        RX_StatusFlags = RX_ERROR_RECOVERABLE;
      }
      if( BSL430_BufferSize > MAX_BUFFER_SIZE )        // For future devices that might need smaller packets
      {
        sendByte( PACKET_SIZE_TOO_BIG );
        RX_StatusFlags = RX_ERROR_RECOVERABLE;
      } 
      dataPointer++;
    }
    else if( dataPointer == (BSL430_BufferSize + 3 ) )
    {
      // if the pointer is pointing to the Checksum low data byte which resides
      // after 0x80, rSize, Core Command.
      checksum = dataByte;
      dataPointer++;
    } 
    else if( dataPointer == (BSL430_BufferSize+4) ) 
    {  
      // if the pointer is pointing to the Checksum low data byte which resides
      // after 0x80, rSize, Core Command, CKL.
      checksum = checksum | dataByte<<8;
      if( verifyData(checksum) )
      {
        if( (RAM_Buf[0] & 0xF0) == PI_COMMAND_UPPER)
        {
          interpretPI_Command();
          RX_StatusFlags = RX_PACKET_ONGOING;
          dataByte = 0;
          dataPointer = 0;
          checksum = 0;
        }
        else
        {
          sendByte( ACK );
          RX_StatusFlags = DATA_RECEIVED;
        }
      }
      else
      {
        sendByte( CHECKSUM_INCORRECT );
        RX_StatusFlags = RX_ERROR_RECOVERABLE;
      }
    }
    else
    {
      RAM_Buf[dataPointer-3] = dataByte;
      dataPointer++;
    }
    
  }
  return RX_StatusFlags;
}
/*******************************************************************************
*Function:    sendData
*Description: Sends the data in the data buffer
*******************************************************************************/
void PI_sendData(int size)
{
  int i;
  sendByte( 0x80 );
  sendByte( size & 0xFF );
  sendByte( size>>8 & 0xFF );
  CRCINIRES = 0xFFFF;
  for( i = 0; i < size; i++){
    CRCDIRB_L = RAM_Buf[i];
    sendByte( RAM_Buf[i] );
  }
  i = CRCINIRES;
  sendByte( i & 0xFF );
  sendByte( i>>8 & 0xFF );
}

/*******************************************************************************
*Function:    sendByte
*Description: Sends a byte
*******************************************************************************/
void sendByte(char data)
{
  while (!(UCA0IFG&UCTXIFG));             // USCI_A0 TX buffer ready?
  while((UCA0STAT & UCBUSY) == UCBUSY);
  UCA0TXBUF = data;
}

void sendString( const char * string )
{
  int i=0;
  while(string[i] != 0)
  {
    sendByte(string[i]);
    i++;
  }
}
/*******************************************************************************
*Function:    receiveByte
*Description: receives a byte
*******************************************************************************/
char receiveByte()
{
  while( !(UCA0IFG & UCRXIFG));       // wait for RX flag
  return UCA0RXBUF;
}
/*******************************************************************************
*Function:    verifyData
*Description: verifies the data in the data buffer against a checksum
*Parameters: 
*           int checksum    the checksum to check against
*Returns:
*           1 checksum parameter is correct for data in the data buffer
*           0 checksum parameter is not correct for the data in the buffer
*******************************************************************************/
char verifyData( int checksum )
{
  int i;
  CRCINIRES = 0xFFFF;
  for( i = 0; i < BSL430_BufferSize; i++)
  {
    CRCDIRB_L = RAM_Buf[i];
  }
  return (CRCINIRES == checksum );
}

/*******************************************************************************
*Function:    getBufferSize
*Description: Returns the max Data Buffer Size for this PI
*Returns:     max buffer size
*******************************************************************************/
int PI_getBufferSize()
{
  return MAX_BUFFER_SIZE;
}


/*******************************************************************************
*Function:    interpretPI_Command
*Description: processes a PI command
*******************************************************************************/
void interpretPI_Command()
{
  char command = RAM_Buf[0];
  if( command == CHANGE_BAUD_RATE )
  {
    volatile int i;
    char rate = RAM_Buf[1];
    if( (rate < BAUD_9600 )||(rate > BAUD_115200) )
    {
        sendByte(UNKNOWN_BAUD_RATE);
    }
    else
    {
      sendByte(ACK);
      while(UCA0STAT&UCBUSY);
      init_USCI( rate );
    }
  }
}

/*******************************************************************************
*Function:    init_USCI
*Description: internal code size saving function used by init and change baud rate
*******************************************************************************/
void init_USCI( char baud_rate )
{
  UCA0CTL1 |= UCSWRST;                      // **Put state machine in reset**
  //UCA0CTL0 |= UCPEN+UCPAR;                  // even parity
  UCA0CTL0 = 0;
  UCA0CTL1 |= UCSSEL__SMCLK;                // SMCLK
  switch ( baud_rate )
  {
    case BAUD_9600:
      UCA0BRW = 833 ;                           // 8MHz 9600 (see User's Guide)
      UCA0MCTL = UCBRS_2 + UCBRF_0;             // Modulation   
    break;
    case BAUD_19200:
      UCA0BRW = 416;                            // 8MHz 19200 (see User's Guide)
      UCA0MCTL = UCBRS_6 + UCBRF_0;             // Modulation   
    break;
    case BAUD_38400:
      UCA0BRW = 208;                            // 8MHz 38400 (see User's Guide)
      UCA0MCTL = UCBRS_3 + UCBRF_0;             // Modulation   
    break;
    case BAUD_57600:
      UCA0BRW = 138;                            // 8MHz 57600 (see User's Guide)
      UCA0MCTL = UCBRS_7 + UCBRF_0;             // Modulation   
    break;
    case BAUD_115200:
      UCA0BRW = 69;                            // 8MHz 115200 (see User's Guide)
      UCA0MCTL = UCBRS_4 + UCBRF_0;            // Modulation   
    break; 
  }
  USCI_PORT_SEL = RXD+TXD;                        // P1.5.6 = USCI_A0 TXD/RXD
  UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
}