// // MSP430 LCD Code // #include "msp430g2553.h" // Defining ports for LCM #define LCM_DIR P1DIR #define LCM_OUT P1OUT // Defining ports for BUTTONS #define BUT_DIR P2DIR #define BUT_IN P2IN // // Define symbolic LCM - MCU pin mappings // We've set DATA PIN TO 4,5,6,7 for easy translation // #define LCM_PIN_RS BIT0 // P1.0 #define LCM_PIN_EN BIT1 // P1.1 #define LCM_PIN_D7 BIT7 // P1.7 #define LCM_PIN_D6 BIT6 // P1.6 #define LCM_PIN_D5 BIT5 // P1.5 #define LCM_PIN_D4 BIT4 // P1.4 // Define symbolic BUTTON - MCU mapping // we've set ports p2.0,p2.1,p2.2 as input ports #define BUT_PIN_T1 BIT0 // P2.0 #define BUT_PIN_T2 BIT1 // P2.1 #define ENROLL BIT2 // P2.2 #define LOGIN BIT3 // P2.3 #define LCM_PIN_MASK (LCM_PIN_RS | LCM_PIN_EN | LCM_PIN_D7 | LCM_PIN_D6 | LCM_PIN_D5 | LCM_PIN_D4) #define BUT_PIN_MASK (BUT_PIN_T1 | BUT_PIN_T2 | ENROLL | LOGIN) #define FALSE 0 #define TRUE 1 // // Routine Desc: // // This is the function that must be called // whenever the LCM needs to be told to // scan it's data bus. // // Parameters: // // void. // // Return // // void. // void PulseLcm() { // // pull EN bit low // LCM_OUT &= ~LCM_PIN_EN; __delay_cycles(200); // // pull EN bit high // LCM_OUT |= LCM_PIN_EN; __delay_cycles(200); // // pull EN bit low again // LCM_OUT &= (~LCM_PIN_EN); __delay_cycles(200); } // // Routine Desc: // // Send a byte on the data bus in the 4 bit mode // This requires sending the data in two chunks. // The high nibble first and then the low nible // // Parameters: // // ByteToSend - the single byte to send // // IsData - set to TRUE if the byte is character data // FALSE if its a command // // Return // // void. // void SendByte(char ByteToSend, int IsData) { // // clear out all pins // LCM_OUT &= (~LCM_PIN_MASK); // // set High Nibble (HN) - // usefulness of the identity mapping // apparent here. We can set the // DB7 - DB4 just by setting P1.7 - P1.4 // using a simple assignment // LCM_OUT |= (ByteToSend & 0xF0); if (IsData == TRUE) { LCM_OUT |= LCM_PIN_RS; } else { LCM_OUT &= ~LCM_PIN_RS; } // // we've set up the input voltages to the LCM. // Now tell it to read them. // PulseLcm(); // // set Low Nibble (LN) - // usefulness of the identity mapping // apparent here. We can set the // DB7 - DB4 just by setting P1.7 - P1.4 // using a simple assignment // LCM_OUT &= (~LCM_PIN_MASK); LCM_OUT |= ((ByteToSend & 0x0F) << 4); if (IsData == TRUE) { LCM_OUT |= LCM_PIN_RS; } else { LCM_OUT &= ~LCM_PIN_RS; } // // we've set up the input voltages to the LCM. // Now tell it to read them. // PulseLcm(); } // // Routine Desc: // // Set the position of the cursor on the screen // // Parameters: // // Row - zero based row number // // Col - zero based col number // // Return // // void. // void LcmSetCursorPosition(char Row, char Col) { char address; // // construct address from (Row, Col) pair // if (Row == 0) { address = 0; } else { address = 0x40; } address |= Col; SendByte(0x80 | address, FALSE); } // // Routine Desc: // // Clear the screen data and return the // cursor to home position // // Parameters: // // void. // // Return // // void. // void ClearLcmScreen() { // // Clear display, return home // __delay_cycles(20000); SendByte(0x01, FALSE); __delay_cycles(2000); SendByte(0x02, FALSE); __delay_cycles(20000); } // // Routine Desc: // // Initialize the LCM after power-up. // // Note: This routine must not be called twice on the // LCM. This is not so uncommon when the power // for the MCU and LCM are separate. // // Parameters: // // void. // // Return // // void. // void InitializeLcm(void) { // // set the MSP pin configurations // and bring them to low // LCM_DIR |= LCM_PIN_MASK; LCM_OUT &= ~(LCM_PIN_MASK); // // wait for the LCM to warm up and reach // active regions. Remember MSPs can power // up much faster than the LCM. // __delay_cycles(100000); // // initialize the LCM module // // 1. Set 4-bit input // LCM_OUT &= ~LCM_PIN_RS; LCM_OUT &= ~LCM_PIN_EN; LCM_OUT = 0x20; PulseLcm(); // // set 4-bit input - second time. // (as reqd by the spec.) // SendByte(0x28, FALSE); // // 2. Display on, cursor on, blink cursor // SendByte(0x0F, FALSE); // // 3. Cursor move auto-increment // SendByte(0x06, FALSE); __delay_cycles(500); SendByte(0x80,FALSE); } // // Routine Desc // // Initializes the Buttons so that input can be taken // // Parameters: // // void // // Returns // // void. // void InitializeBut() { BUT_DIR &= ~(BUT_PIN_MASK); BUT_IN &= BUT_PIN_MASK; P2IE |= LOGIN; // Interrupt Enable in P2.3 P2IES &= ~LOGIN; // P2.3 Interrupt flag low-to-high transition P2IFG &= ~LOGIN; // P2.3 IFG cleared } // // Routine Desc // // Print a string of characters to the screen // // Parameters: // // Text - null terminated string of chars // // Returns // // void. // void PrintStr(char *Text) { char *c; c = Text; unsigned short int n=0; while ((c != 0) && (*c != 0)) { if(n>15) { LcmSetCursorPosition(1,n-16); } SendByte(*c,TRUE); __delay_cycles(305000); c++; n++; } } // // Routine Desc // // Print a string of characters to the screen according to the value of buttons // // Parameters: // // void // // Returns // // void. // void Decision() { if ((BUT_IN & BUT_PIN_T1) == BUT_PIN_T1) { if ((BUT_IN & BUT_PIN_T2) == BUT_PIN_T2) { ClearLcmScreen(); PrintStr("Face recognized Access Granted"); __delay_cycles(1000000); } else { ClearLcmScreen(); PrintStr("unknown face like object"); __delay_cycles(1000000); } } else { if ((BUT_IN & BUT_PIN_T2) == BUT_PIN_T2) { ClearLcmScreen(); PrintStr("unknown face"); __delay_cycles(1005000); ClearLcmScreen(); PrintStr("You can be added to the database"); __delay_cycles(1005000); ClearLcmScreen(); PrintStr("Press ENROLL to start enrolling"); __delay_cycles(5005000); // put a button pressing routine here if ((BUT_IN & ENROLL) == ENROLL) { ClearLcmScreen(); PrintStr("u pressed ENROLL...enrolling...."); __delay_cycles(1000000); ClearLcmScreen(); PrintStr("image enrolled"); __delay_cycles(1000000); } else { ClearLcmScreen(); PrintStr("access denied"); __delay_cycles(1000000); } } else { ClearLcmScreen(); PrintStr("unknown object"); __delay_cycles(1000000); } } // ClearLcmScreen(); // PrintStr("Press LOGIN to login again"); // __delay_cycles(5000000); } // Port2 Interrupt Service Routine #pragma vector=PORT2_VECTOR __interrupt void Port_2(void) { _BIC_SR(LPM3_bits); //LPM3_EXIT; } // // Routine Desc // // main entry point to the sketch // // Parameters // // void. // // Returns // // void. // void main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer InitializeLcm(); // initializes the LCM InitializeBut(); // initializes the buttons for now // in fact it contains inputs from DSP ClearLcmScreen(); // clears the LCM screen PrintStr(" Welcome to Bio Recs"); __delay_cycles(1000000); while(1) { ClearLcmScreen(); PrintStr("Press LOGIN to start logging in"); // main program starts // __delay_cycles(1000000); _BIS_SR (LPM3_bits + GIE); Decision(); P2IFG &= ~LOGIN; // P2.3 IFG cleared } //if ((BUT_IN & LOGIN) == LOGIN) // put an interrupt here so that only // decision is called when interrupted // { __delay_cycles(1000000); // Decision(); // } }