// TI File $Revision: /main/2 $ // Checkin $Date: July 31, 2009 14:26:08 $ //########################################################################### // Filename: Example_28xEcan_A_to_B_Xmit.c // // Description: eCAN-A To eCAN-B TXLOOP - Transmit loop // // ASSUMPTIONS: // // This program requires the DSP280x header files. // // Both CAN ports of the 280x DSP need to be connected // to each other (via CAN transceivers) // // eCANA is on GPIO31 (CANTXA) and // GPIO30 (CANRXA) // // eCANB is on GPIO8 (CANTXB) and // GPIO10 (CANRXB) // // As supplied, this project is configured for "boot to SARAM" // operation. The 280x Boot Mode table is shown below. // For information on configuring the boot mode of an eZdsp, // please refer to the documentation included with the eZdsp, // // Boot GPIO18 GPIO29 GPIO34 // Mode SPICLKA SCITXDA // SCITXB // ------------------------------------- // Flash 1 1 1 // SCI-A 1 1 0 // SPI-A 1 0 1 // I2C-A 1 0 0 // ECAN-A 0 1 1 // SARAM 0 1 0 <- "boot to SARAM" // OTP 0 0 1 // I/0 0 0 0 // // // DESCRIPTION: // // This example TRANSMITS data to another CAN module using MAILBOX5 // This program could either loop forever or transmit "n" # of times, // where "n" is the TXCOUNT value. // // This example can be used to check CAN-A and CAN-B. Since CAN-B is // initialized in DSP280x_ECan.c, it will acknowledge all frames // transmitted by the node on which this code runs. Both CAN ports of // the 280x DSP need to be connected to each other (via CAN transceivers) // //########################################################################### // Original Author: HJ // // $TI Release: DSP280x C/C++ Header Files V1.70 $ // $Release Date: July 27, 2009 $ //########################################################################### #include "DSP280x_Device.h" // DSP280x Headerfile Include File #include "DSP280x_Examples.h" // DSP280x Examples Include File #define TXCOUNT 10 // Transmission will take place (TXCOUNT) times.. // Globals for this example long i; long loopcount = 0; void ReceiveCANMsg(int16, Uint32*, Uint32*); void SendCANMsg(int16, Uint32, Uint32); void main() { Uint32 datah; Uint32 datal; Uint32* raw_datah; Uint32* raw_datal; //Uint32 mdl; //Uint32 mdh; /* Create a shadow register structure for the CAN control registers. This is needed, since, only 32-bit access is allowed to these registers. 16-bit access to these registers could potentially corrupt the register contents. This is especially true while writing to a bit (or group of bits) among bits 16 - 31 */ struct ECAN_MBOXES MBoxesShadow; struct ECAN_REGS ECanaShadow; // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP280x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initalize GPIO: // This example function is found in the DSP280x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // Just initalize eCAN pins for this example // This function is in DSP280x_ECan.c InitECanGpio(); // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP280x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP280x_DefaultIsr.c. // This function is found in DSP280x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. // No interrupts used in this example. // Step 4. Initialize all the Device Peripherals: // This function is found in DSP280x_InitPeripherals.c // InitPeripherals(); // Not required for this example // In this case just initalize eCAN-A and eCAN-B // This function is in DSP280x_ECan.c InitECan(); // Step 5. User specific code: /* Write to the MSGID field */ // ECanaMboxes.MBOX15.MSGID.all = 0x95555555; // Extended Identifier ECanaMboxes.MBOX15.MSGID.all = 0x81800000; //Standard Identifier - Transmit MBOX 15 // ECanaMboxes.MBOX3.MSGID.all = 0xC2000000; // Standard Identifier - Rcv MBOX 3 MBoxesShadow.MBOX3.MSGID.bit.AAM = 0; MBoxesShadow.MBOX3.MSGID.bit.AME = 0; MBoxesShadow.MBOX3.MSGID.bit.IDE = 0; MBoxesShadow.MBOX3.MSGID.bit.STDMSGID = 0XFF; ECanaMboxes.MBOX3.MSGID.all = MBoxesShadow.MBOX3.MSGID.all; ECanaRegs.CANGAM.all = 0x8003FFFF; /* Configure Mailbox under test as a Transmit mailbox */ ECanaShadow.CANMD.all = ECanaRegs.CANMD.all; ECanaShadow.CANMD.bit.MD15 = 0; ECanaShadow.CANMD.bit.MD3 = 1; ECanaRegs.CANMD.all = ECanaShadow.CANMD.all; /* Enable Mailbox under test */ ECanaShadow.CANME.all = ECanaRegs.CANME.all; ECanaShadow.CANME.bit.ME15 = 1; ECanaShadow.CANME.bit.ME3 = 1; ECanaRegs.CANME.all = ECanaShadow.CANME.all; /* Write to DLC field in Master Control reg */ ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 4; /* Turn off RTR */ ECanaMboxes.MBOX15.MSGCTRL.bit.RTR = 0; ECanaMboxes.MBOX3.MSGCTRL.bit.RTR = 0; /* Set up/disable interrupts */ EALLOW; ECanaShadow.CANGIM.all = ECanaRegs.CANGIM.all; ECanaShadow.CANGIM.bit.MTOM = 0; ECanaShadow.CANGIM.bit.TCOM = 0; ECanaShadow.CANGIM.bit.AAIM = 0; ECanaShadow.CANGIM.bit.WDIM = 0; ECanaShadow.CANGIM.bit.WUIM = 0; ECanaShadow.CANGIM.bit.RMLIM = 0; ECanaShadow.CANGIM.bit.BOIM = 0; ECanaShadow.CANGIM.bit.EPIM = 0; ECanaShadow.CANGIM.bit.WLIM = 0; ECanaShadow.CANGIM.bit.GIL = 0; // Map global interrupts to ECAN0INT ECanaShadow.CANGIM.bit.I1EN = 0; ECanaShadow.CANGIM.bit.I0EN = 1; ECanaRegs.CANGIM.all = ECanaShadow.CANGIM.all; ECanaRegs.CANMIM.all = 0x00000006; ECanaShadow.CANMC.all = ECanaRegs.CANMC.all; ECanaShadow.CANMC.bit.DBO = 0; ECanaRegs.CANMC.all = ECanaShadow.CANMC.all; EDIS; ECanaRegs.CANMIL.all = 0xFFFFFFFF; // Mailbox Interrupt Level: All ECanaRegs.CANOPC.all = 0x00000000; datah = 0x55555555; datal = 0xAAAAAAAA; raw_datah = &datah; raw_datah = &datal; for(;;) { if (ECanaRegs.CANRMP.all > 0 && ECanaRegs.CANGIF0.bit.MIV0 == 3) { ReceiveCANMsg(3, raw_datah, raw_datal); SendCANMsg(15, datah, datal); } // SendCANMsg(15, datah, datal); } } void ReceiveCANMsg(int16 MBXnum, Uint32 *raw_datah, Uint32 *raw_datal) { volatile struct MBOX *srcMBox; if (0 <= MBXnum && MBXnum <= 32) { // Get pointer to mailbox struct and grab data srcMBox = &ECanaMboxes.MBOX0 + MBXnum; *raw_datah = srcMBox->MDH.all; *raw_datal = srcMBox->MDL.all; ECanaRegs.CANRMP.all = (0x00000001 << MBXnum); /* Process Data */ } } void SendCANMsg(int16 MBXnum, Uint32 MBXDL, Uint32 MBXDH) { volatile struct MBOX *srcMBox; if (0 <= MBXnum && MBXnum <= 32) { Uint32 MBXflag = (0x00000001 << MBXnum); srcMBox = &ECanaMboxes.MBOX0 + MBXnum; srcMBox->MDL.all = MBXDL; srcMBox->MDH.all = MBXDH; ECanaRegs.CANTRS.all = MBXflag; while(ECanaRegs.CANTA.all != MBXflag) {} ECanaRegs.CANTA.all = MBXflag; } } /* // Clear to the transmit mailbox RAM field ECanaMboxes.MBOX15.MDL.all = 0x00000000; ECanaMboxes.MBOX15.MDH.all = 0x00000000; // Begin reading from receive mailbox 3 ECanaShadow.CANRMP.bit.RMP3 = 0; ECanaRegs.CANRMP.all = ECanaShadow.CANRMP.all; mdl=0; mdh=0; do { ECanaShadow.CANRMP.all = ECanaRegs.CANRMP.all; } while(ECanaShadow.CANRMP.bit.RMP3 == 0); // Wait for CANRMP bit to be set.. ECanaRegs.CANRMP.bit.RMP3 = 1; mdl = ECanaMboxes.MBOX3.MDL.all; mdh = ECanaMboxes.MBOX3.MDH.all; // Copy received data to the transmit mailbox RAM field ECanaMboxes.MBOX15.MDL.all = mdl; ECanaMboxes.MBOX15.MDH.all = mdh; ECanaRegs.CANRMP.bit.RMP3 = 0; // Begin transmitting for(i=0; i < TXCOUNT; i++) { ECanaShadow.CANTRS.all = 0; ECanaShadow.CANTRS.bit.TRS15 = 1; // Set TRS for mailbox under test ECanaRegs.CANTRS.all = ECanaShadow.CANTRS.all; do { ECanaShadow.CANTA.all = ECanaRegs.CANTA.all; } while(ECanaShadow.CANTA.bit.TA15 == 0 ); ECanaShadow.CANTA.all = 0; ECanaShadow.CANTA.bit.TA15 = 1; // Clear TA5 ECanaRegs.CANTA.all = ECanaShadow.CANTA.all; loopcount ++; } asm(" ESTOP0"); // Stop here } */