Uint16 I2CA_ReadData(struct I2CMSG *msg) { // Wait until the STP bit is cleared from any previous master communication. // Clearing of this bit by the module is delayed until after the SCD bit is // set. If this bit is not checked prior to initiating a new message, the // I2C could get confused. if (I2caRegs.I2CMDR.bit.STP == 1) { return I2C_STP_NOT_READY_ERROR; } I2caRegs.I2CSAR = msg->SlaveAddress; if(msg->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP) { // Check if bus busy if (I2caRegs.I2CSTR.bit.BB == 1) { return I2C_BUS_BUSY_ERROR; } I2caRegs.I2CCNT = 2; I2caRegs.I2CDXR = msg->MemoryHighAddr; I2caRegs.I2CDXR = msg->MemoryLowAddr; I2caRegs.I2CMDR.all = 0x2620; // Send data to setup EEPROM address } else if(msg->MsgStatus == I2C_MSGSTAT_RESTART) { I2caRegs.I2CCNT = msg->NumOfBytes; // Setup how many bytes to expect I2caRegs.I2CMDR.all = 0x2C20; // Send restart as master receiver } return I2C_SUCCESS; }