#include "DSP280x_Device.h" #include "DSP280x_Examples.h" // Prototype statements for functions found within this file. void scia_loopback_init(void); void scia_fifo_init(void); void scia_xmit(int a); void error(int); interrupt void scia_rx_isr(void); interrupt void scia_tx_isr(void); #include // Global counts used in this example Uint16 LoopCount; Uint16 ErrorCount; void main(void) { Uint16 SendChar; Uint16 ReceivedChar; // Step 1. Initialize System Control registers, PLL, WatchDog, Clocks to default state: // This function is found in the DSP280x_SysCtrl.c file. InitSysCtrl(); // Step 2. Select GPIO for the device or for the specific application: // This function is found in the DSP280x_Gpio.c file. // InitGpio(); skip this as this is example selects the I/O // for SCI-A in this file itself InitSciGpio(); // Step 3. Initialize PIE vector table: // The PIE vector table is initialized with pointers to shell Interrupt // Service Routines (ISR). The shell routines are found in DSP280x_DefaultIsr.c. // Insert user specific ISR code in the appropriate shell ISR routine in // the DSP28_DefaultIsr.c file. // Disable and clear all CPU interrupts: DINT; IER = 0x0000; IFR = 0x0000; // Initialize Pie Control Registers To Default State: // This function is found in the DSP280x_PieCtrl.c file. // InitPieCtrl(); PIE is not used for this example // Initialize the PIE Vector Table To a Known State: // This function is found in DSP280x_PieVect.c. // This function populates the PIE vector table with pointers // to the shell ISR functions found in DSP280x_DefaultIsr.c. InitPieVectTable(); // Enable CPU and PIE interrupts // This example function is found in the DSP280x_PieCtrl.c file. EnableInterrupts(); // Step 4. Initialize all the Device Peripherals to a known state: // This function is found in DSP280x_InitPeripherals.c // InitPeripherals(); skip this for SCI tests // Step 5. User specific functions, Reassign vectors (optional), Enable Interrupts: LoopCount = 0; ErrorCount = 0; scia_fifo_init(); // Initialize the SCI FIFO scia_loopback_init(); // Initalize SCI for digital loop back // Note: Autobaud lock is not required for this example // Send a character starting with 0 SendChar = 0; // Step 6. Send Characters forever starting with 0x00 and going through // 0xFF. After sending each, check the recieve buffer for the correct value for(;;) { scia_xmit(SendChar); while(SciaRegs.SCIFFRX.bit.RXFFST !=1) { } // wait for XRDY =1 for empty state // Check received character ReceivedChar = SciaRegs.SCIRXBUF.all; if(ReceivedChar != SendChar) error(1); // Move to the next character and repeat the test SendChar++; // Limit the character to 8-bits SendChar &= 0x00FF; LoopCount++; } } // Step 7. Insert all local Interrupt Service Routines (ISRs) and functions here: void error(int ErrorFlag) { Uint16 Error = ErrorFlag; ErrorCount++; // asm(" ESTOP0"); // Uncomment to stop the test here // for (;;); } // Test 1,SCIA DLB, 8-bit word, baud rate 0x000F, default, 1 STOP bit, no parity void scia_loopback_init() { // Note: Clocks were turned on to the SCIA peripheral // in the InitSysCtrl() function SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback // No parity,8 char bits, // async mode, idle-line protocol SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK, // Disable RX ERR, SLEEP, TXWAKE SciaRegs.SCICTL2.all =0x0003; SciaRegs.SCICTL2.bit.TXINTENA =1; SciaRegs.SCICTL2.bit.RXBKINTENA =1; SciaRegs.SCIHBAUD =0x0000; SciaRegs.SCILBAUD =0x000F; SciaRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset } // Transmit a character from the SCI' void scia_xmit(int a) { SciaRegs.SCITXBUF=a; } // Initalize the SCI FIFO void scia_fifo_init() { SciaRegs.SCIFFTX.all=0xE040; SciaRegs.SCIFFRX.all=0x204f; SciaRegs.SCIFFCT.all=0x0; }