/* // NOTE: IMA copied most of this file from the flash programming example project // //########################################################################### // FILE: F28M36H63C2_m3.cmd // TITLE: Linker Command File for F28M36H63C2 projects that run from FLASH // Keep in mind that C0 and C1 are protected by the code security module. // What this means is in most cases you will want to move to // another memory map file which has more memory defined. //########################################################################### // $TI Release: F28M36x Support Library v201 $ // $Release Date: Fri Jun 7 10:37:02 CDT 2013 $ //########################################################################### */ //--retain=g_pfnVectors /* The following command line options are set as part of the CCS project. */ /* If you are building using the command line, or for some reason want to */ /* define them here, you can uncomment and modify these lines as needed. */ /* If you are using CCS for building, it is probably better to make any such */ /* modifications in your CCS project and leave this file alone. */ /* */ /* --heap_size=0 */ /* --stack_size=256 */ /* --library=rtsv7M3_T_le_eabi.lib */ /* The following options allow the user to program Z1 and Z2 DCSM security */ /* values, include CSM PSWD, ECSL PSWD, GRABSECT, GRABRAM, and FLASH EXEONLY */ /* The driverlib/dcsm_z1_secvalues.s and driverlib/dcsm_z2_secvalues.s files */ /* must be included in the Flash project for the below 2 lines to take */ /* effect. */ --retain=dcsm_z1_secvalues.obj(.z1secvalues,.z1_csm_rsvd) //--retain=dcsm_z2_secvalues.obj(.z2secvalues,.z2_csm_rsvd) --retain=BL_REVISION.obj(.blrev) /* System memory map */ MEMORY { /* Flash Block 0, Sector 0 Z1 CSM */ CSM_ECSL_Z1 : origin = 0x00200000, length = 0x0024 CSM_RSVD_Z1 : origin = 0x00200024, length = 0x000C //CSM_RSVD_OTHER : origin = 0x00200050, length = 0x01AF //Found at TRM pg. 550, but not verified /* Flash Block 0, Sector 0 */ RESETISR (RX) : origin = 0x00200030, length = 0x0008 /* Reset ISR is mapped to boot to Flash location */ BL_INTVECS (RX) : origin = 0x00200038, length = 0x0258 BL_FLASH (RX) : origin = 0x00200290, length = 0x7D60 // The Bootloader resides here - never touch this block (N) BL_REVISION : origin = 0x00207FF0, length = 0x0004 //4 bytes used for the bootloader revision number //8 empty bytes in the middle BL_RSVD : origin = 0x00207FFC, length = 0x0004 //4 bytes reserved for resolution reduction mode APP_RESETISR (RX) : origin = 0x00208000, length = 0x0008 // Entry point into the application APP_INTVECS (RX) : origin = 0x00208008, length = 0x0258 // Interrupt Vectors for the application APP_FLASH (RX) : origin = 0x00208260, length = 0xF7BA0 // The Application resides here /* Flash Block 0, Sector 13 Z2 CSM*/ CSM_RSVD_OTHER2 : origin = 0x002FFE00, length = 0x01D0 //Note found at TRM pg. 550 (set to 0x00) CSM_RSVD_Z2 : origin = 0x002FFFD0, length = 0x000C CSM_ECSL_Z2 : origin = 0x002FFFDC, length = 0x0024 /* ACTUAL FLASH PAGES (KEEP FOR REFERENCE): FLASH_N (RX) : origin = 0x00201258, length = 0x6DA8 // For storing code in Flash to copy to RAM at runtime FLASH_M (RX) : origin = 0x00208000, length = 0x8000 FLASH_L (RX) : origin = 0x00210000, length = 0x8000 FLASH_K (RX) : origin = 0x00218000, length = 0x8000 FLASH_J (RX) : origin = 0x00220000, length = 0x20000 FLASH_I (RX) : origin = 0x00240000, length = 0x20000 FLASH_H (RX) : origin = 0x00260000, length = 0x20000 FLASH_G (RX) : origin = 0x00280000, length = 0x20000 FLASH_F (RX) : origin = 0x002A0000, length = 0x20000 FLASH_E (RX) : origin = 0x002C0000, length = 0x20000 FLASH_D (RX) : origin = 0x002E0000, length = 0x8000 FLASH_C (RX) : origin = 0x002E8000, length = 0x8000 FLASH_B (RX) : origin = 0x002F0000, length = 0x8000 FLASH_A (RX) : origin = 0x002F8000, length = 0x7FD0 */ /* RAM */ C0 (RWX) : origin = 0x20000000, length = 0x2000 C1 (RWX) : origin = 0x20002000, length = 0x2000 BOOT_RSVD (RX) : origin = 0x20004000, length = 0x0FF8 C2 (RWX) : origin = 0x200051B0, length = 0x0E50 C3 (RWX) : origin = 0x20006000, length = 0x2000 // USED TO STORE NEW BINARY IMAGE FOR FLASHING C28 SHARED_RAM : origin = 0x20008000, length = 0x10000 /* SHARED RAM (KEEP FOR REFERENCE): S0 (RWX) : origin = 0x20008000, length = 0x2000 S1 (RWX) : origin = 0x2000A000, length = 0x2000 S2 (RWX) : origin = 0x2000C000, length = 0x2000 S3 (RWX) : origin = 0x2000E000, length = 0x2000 S4 (RWX) : origin = 0x20010000, length = 0x2000 S5 (RWX) : origin = 0x20012000, length = 0x2000 S6 (RWX) : origin = 0x20014000, length = 0x2000 S7 (RWX) : origin = 0x20016000, length = 0x2000 */ //USED TO STORE NEW BINARY IMAGE FOR FLASHING M3 RAM_HIGH (RWX) : origin = 0x20018000, length = 0x18000 /* ACTUAL RAM PAGES (KEEP FOR REFERENCE): C4 (RWX) : origin = 0x20018000, length = 0x2000 C5 (RWX) : origin = 0x2001A000, length = 0x2000 C6 (RWX) : origin = 0x2001C000, length = 0x2000 C7 (RWX) : origin = 0x2001E000, length = 0x2000 C8 (RWX) : origin = 0x20020000, length = 0x2000 C9 (RWX) : origin = 0x20022000, length = 0x2000 C10 (RWX) : origin = 0x20024000, length = 0x2000 C11 (RWX) : origin = 0x20026000, length = 0x2000 C12 (RWX) : origin = 0x20028000, length = 0x2000 C13 (RWX) : origin = 0x2002A000, length = 0x2000 C14 (RWX) : origin = 0x2002C000, length = 0x2000 C15 (RWX) : origin = 0x2002E000, length = 0x2000 */ CTOMRAM (RX) : origin = 0x2007F000, length = 0x0800 MTOCRAM (RWX) : origin = 0x2007F800, length = 0x0800 } /* Section allocation in memory */ SECTIONS { .resetisr: > RESETISR .intvecs: > BL_INTVECS .text : > BL_FLASH .const : > BL_FLASH .cinit : > BL_FLASH .pinit : > BL_FLASH .vtable : > C0 .data : > C0 .bss : > C1 .sysmem : > C0 .stack : > C0 .z1secvalues : > CSM_ECSL_Z1 .z1_csm_rsvd : > CSM_RSVD_Z1 // .z2secvalues : > CSM_ECSL_Z2 // .z2_csm_rsvd : > CSM_RSVD_Z2 .blrev : > BL_REVISION m3rambuffer : >> RAM_HIGH c28rambuffer : >> SHARED_RAM GROUP { ramfuncs { -l F021_API_CortexM3_LE.lib } } LOAD = BL_FLASH, RUN = C0, LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), PAGE = 0 GROUP : > MTOCRAM { PUTBUFFER PUTWRITEIDX GETREADIDX } GROUP : > CTOMRAM { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT } } __STACK_TOP = __stack + 256;