MEMORY { BEGIN : origin = 0x080000, length = 0x000002 // Update the codestart location as needed BOOT_RSVD : origin = 0x000002, length = 0x0001AF /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x0001B1, length = 0x00024F RAMM1 : origin = 0x000400, length = 0x000400 RAMD0 : origin = 0x00C000, length = 0x002000 RAMD1 : origin = 0x00E000, length = 0x002000 RAMD2 : origin = 0x01A000, length = 0x002000 // Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0x8000. User should comment/uncomment based on core selection RAMD3 : origin = 0x01C000, length = 0x002000 // Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0xA000. User should comment/uncomment based on core selection RAMD4 : origin = 0x01E000, length = 0x002000 // Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0xC000. User should comment/uncomment based on core selection // RAMD5 : origin = 0x020000, length = 0x002000 // Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0xE000. User should comment/uncomment based on core selection RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x000800 RAMLS6 : origin = 0x00B000, length = 0x000800 RAMLS7 : origin = 0x00B800, length = 0x000800 RAMLS8 : origin = 0x022000, length = 0x002000 // When configured as CLA program use the address 0x4000 RAMLS9 : origin = 0x024000, length = 0x002000 // When configured as CLA program use the address 0x6000 // RAMLS8_CLA : origin = 0x004000, length = 0x002000 // Use only if configured as CLA program memory // RAMLS9_CLA : origin = 0x006000, length = 0x002000 // Use only if configured as CLA program memory RAMGS0 : origin = 0x010000, length = 0x002000 RAMGS1 : origin = 0x012000, length = 0x002000 RAMGS2 : origin = 0x014000, length = 0x002000 RAMGS3 : origin = 0x016000, length = 0x002000 RAMGS4 : origin = 0x018000, length = 0x002000 /* Flash Banks (128 sectors each) */ FLASH_BANK0 : origin = 0x080002, length = 0x1FFFE // Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection FLASH_BANK1 : origin = 0x0A0000, length = 0x20000 // Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection FLASH_BANK2 : origin = 0x0C0000, length = 0x20000 // Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection // FLASH_BANK3 : origin = 0x0E0000, length = 0x20000 // Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection // FLASH_BANK4 : origin = 0x100000, length = 0x20000 // Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000400 CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000400 CLATOCPURAM : origin = 0x001480, length = 0x000080 CPUTOCLARAM : origin = 0x001500, length = 0x000080 CLATODMARAM : origin = 0x001680, length = 0x000080 DMATOCLARAM : origin = 0x001700, length = 0x000080 CANA_MSG_RAM : origin = 0x049000, length = 0x000800 CANB_MSG_RAM : origin = 0x04B000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002 } SECTIONS { codestart : > BEGIN .text : >> FLASH_BANK0 | FLASH_BANK1, ALIGN(8) .cinit : > FLASH_BANK0, ALIGN(8) .switch : > FLASH_BANK0, ALIGN(8) .reset : > RESET, TYPE = DSECT /* not used, */ .stack : > RAMLS7 #if defined(__TI_EABI__) .bss : >> RAMLS3 | RAMLS5 .bss:output : > RAMLS3 .init_array : > FLASH_BANK0, ALIGN(8) .const : > FLASH_BANK0, ALIGN(8) .data : >> RAMLS1 | RAMLS2 .sysmem : > RAMLS4 #else .pinit : > FLASH_BANK0, ALIGN(8) .ebss : >> RAMLS5 | RAMLS6 .econst : > FLASH_BANK0, ALIGN(8) .esysmem : > RAMLS5 #endif ramgs0 : > RAMGS0, type=NOINIT ramgs1 : > RAMGS1, type=NOINIT ramgs2 : > RAMGS2, type=NOINIT MSGRAM_CPU1_TO_CPU2 > CPU1TOCPU2RAM, type=NOINIT MSGRAM_CPU2_TO_CPU1 > CPU2TOCPU1RAM, type=NOINIT #if defined(__TI_EABI__) .TI.ramfunc : {} LOAD = FLASH_BANK0, RUN = RAMLS4, LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), ALIGN(8) #else .TI.ramfunc : {} LOAD = FLASH_BANK0, RUN = RAMLS4, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), ALIGN(8) #endif #if defined(__TI_EABI__) /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK0, RUN = RAMLS0, LOAD_START(Cla1ProgLoadStart), RUN_START(Cla1ProgRunStart), LOAD_SIZE(Cla1ProgLoadSize), ALIGN(4) #else /* CLA specific sections */ Cla1Prog : LOAD = FLASH_BANK0, RUN = RAMLS0, LOAD_START(_Cla1ProgLoadStart), RUN_START(_Cla1ProgRunStart), LOAD_SIZE(_Cla1ProgLoadSize), ALIGN(4) #endif Cla1ToCpuMsgRAM : > CLATOCPURAM CpuToCla1MsgRAM : > CPUTOCLARAM .scratchpad : > RAMLS1 .bss_cla : > RAMLS1 Cla1DataRam : > RAMLS2 cla_shared : > RAMLS1 CLADataLS1 : > RAMLS1 #if defined(__TI_EABI__) .const_cla : LOAD = FLASH_BANK0, RUN = RAMLS1, RUN_START(Cla1ConstRunStart), LOAD_START(Cla1ConstLoadStart), LOAD_SIZE(Cla1ConstLoadSize), ALIGN(4) #else .const_cla : LOAD = FLASH_BANK0, RUN = RAMLS1, RUN_START(_Cla1ConstRunStart), LOAD_START(_Cla1ConstLoadStart), LOAD_SIZE(_Cla1ConstLoadSize), ALIGN(4) #endif firfilt : > RAMLS1 firldb : > RAMLS1 revcoeff : > RAMLS1 dclfuncs : > RAMLS3, PAGE = 0 } /* //=========================================================================== // End of file. //=========================================================================== */