#include "DSP28x_Project.h" // Device Headerfile and Examples Include File // Note: I2C Macros used in this example can be found in the // DSP2833x_I2C_defines.h file // Prototype statements for functions found within this file. void I2CA_Init(void); Uint16 I2CA_WriteData(struct I2CMSG *msg); Uint16 I2CA_ReadData(struct I2CMSG *msg); interrupt void i2c_int1a_isr(void); void pass(void); void fail(void); int sendI2C(); int receiveI2C(); #define I2C_SLAVE_ADDR_W 0xC0 #define I2C_SLAVE_ADDR_R 0XC0 #define I2C_NUMBYTES 1 #define I2C_SUBADDR1 0x02 #define I2C_SUBADDR2 0x00 #define I2C_SUBADDR3 0x00 #define I2C_SUBADDR4 0x00 #define I2C_EEPROM_LOW_ADDR 0x30 // Global variables // Two bytes will be used for the outgoing address, // thus only setup 14 bytes maximum struct I2CMSG I2cMsgOut1={I2C_MSGSTAT_SEND_WITHSTOP, I2C_SLAVE_ADDR_W, I2C_NUMBYTES, I2C_SUBADDR1, I2C_EEPROM_LOW_ADDR, 0x80 // Msg Byte 1 }; struct I2CMSG I2cMsgIn1={ I2C_MSGSTAT_SEND_NOSTOP, I2C_SLAVE_ADDR_R, I2C_NUMBYTES, I2C_SUBADDR1, I2C_EEPROM_LOW_ADDR}; struct I2CMSG *CurrentMsgPtr; // Used in interrupts Uint16 PassCount; Uint16 FailCount; Uint16 Error; Uint16 i; char newByte; void main(void) { CurrentMsgPtr = &I2cMsgOut1; // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initalize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Setup only the GP I/O only for I2C functionality InitGpio(); InitI2CGpio(); //Set GPIO pins 48 and 49 as outputs. EALLOW; GpioCtrlRegs.GPBDIR.bit.GPIO48 = 1; //Drives PWDN pin on Camera. GpioCtrlRegs.GPBDIR.bit.GPIO49 = 1; //Drives reset pin on camera. //Power on Camera GpioDataRegs.GPBDAT.bit.GPIO48 = 0; GpioDataRegs.GPBDAT.bit.GPIO49 = 0; EDIS; // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.I2CINT1A = &i2c_int1a_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2833x_InitPeripherals.c // InitPeripherals(); // Not required for this example I2CA_Init(); // Step 5. User specific code // Clear Counters PassCount = 0; FailCount = 0; // Clear incoming message buffer for (i = 0; i < I2C_MAX_BUFFER_SIZE; i++) { I2cMsgIn1.MsgBuffer[i] = 0x0000; } // Enable I2C interrupt 1 in the PIE: Group 8 interrupt 1 PieCtrlRegs.PIEIER8.bit.INTx1 = 1; // Enable CPU INT8 which is connected to PIE group 8 IER |= M_INT8; EINT; while(sendI2C() == 0){} while(receiveI2C() == 0){} newByte = I2cMsgIn1.MsgBuffer[1]; } // end of main void I2CA_Init(void) { // Initialize I2C I2caRegs.I2CSAR = 0xC0; // Slave address - Camera control code #if (CPU_FRQ_150MHZ) // Default - For 150MHz SYSCLKOUT I2caRegs.I2CPSC.all = 14; // Prescaler - need 7-12 Mhz on module clk (150/15 = 10MHz) #endif #if (CPU_FRQ_100MHZ) // For 100 MHz SYSCLKOUT I2caRegs.I2CPSC.all = 9; // Prescaler - need 7-12 Mhz on module clk (100/10 = 10MHz) #endif I2caRegs.I2CCLKL = 10; // NOTE: must be non zero I2caRegs.I2CCLKH = 5; // NOTE: must be non zero I2caRegs.I2CIER.all = 0x24; // Enable SCD & ARDY interrupts I2caRegs.I2CMDR.all = 0x0020; // Take I2C out of reset // Stop I2C when suspended // Set to master mode I2caRegs.I2CFFTX.all = 0x6000; // Enable FIFO mode and TXFIFO I2caRegs.I2CFFRX.all = 0x2040; // Enable RXFIFO, clear RXFFINT, return; } int sendI2C() { ///////////////////////////////////// // Transmit data to Camera section // ///////////////////////////////////// if(I2cMsgOut1.MsgStatus == I2C_MSGSTAT_SEND_WITHSTOP) { Error = I2CA_WriteData(&I2cMsgOut1); // If communication is correctly initiated, set msg status to busy // and update CurrentMsgPtr for the interrupt service routine. // Otherwise, do nothing and try again next loop. Once message is // initiated, the I2C interrupts will handle the rest. Search for // ICINTR1A_ISR in the i2c_eeprom_isr.c file. if (Error == I2C_SUCCESS) { CurrentMsgPtr = &I2cMsgOut1; I2cMsgOut1.MsgStatus = I2C_MSGSTAT_WRITE_BUSY; return 1; } } // end of write section return 0; } int receiveI2C() { /////////////////////////////////// // Read data from Camera section // /////////////////////////////////// // Check outgoing message status. Bypass read section if status is // not inactive. if (I2cMsgOut1.MsgStatus == I2C_MSGSTAT_INACTIVE) { // Check incoming message status. if(I2cMsgIn1.MsgStatus == I2C_MSGSTAT_SEND_NOSTOP) { // Camera address setup portion while(I2CA_ReadData(&I2cMsgIn1) != I2C_SUCCESS) { //Attempt to read until successful. } // Update current message pointer and message status CurrentMsgPtr = &I2cMsgIn1; I2cMsgIn1.MsgStatus = I2C_MSGSTAT_SEND_NOSTOP_BUSY; } // Once message has progressed past setting up the internal address // send a restart to read the data bytes from the camera. // Complete the communique with a stop bit. MsgStatus is // updated in the interrupt service routine. else if(I2cMsgIn1.MsgStatus == I2C_MSGSTAT_RESTART) { // Read data portion while(I2CA_ReadData(&I2cMsgIn1) != I2C_SUCCESS) { // Maybe setup an attempt counter to break an infinite while // loop. } // Update current message pointer and message status CurrentMsgPtr = &I2cMsgIn1; I2cMsgIn1.MsgStatus = I2C_MSGSTAT_READ_BUSY; return 1; } } // end of read section return 0; } Uint16 I2CA_WriteData(struct I2CMSG *msg) { Uint16 i; // Wait until the STP bit is cleared from any previous master communication. // Clearing of this bit by the module is delayed until after the SCD bit is // set. If this bit is not checked prior to initiating a new message, the // I2C could get confused. if (I2caRegs.I2CMDR.bit.STP == 1) { return I2C_STP_NOT_READY_ERROR; } // Setup slave address I2caRegs.I2CSAR = msg->SlaveAddress; // Check if bus busy if (I2caRegs.I2CSTR.bit.BB == 1) { return I2C_BUS_BUSY_ERROR; } // Setup number of bytes to send // MsgBuffer + Address I2caRegs.I2CCNT = msg->NumOfBytes+1; // Setup data to send I2caRegs.I2CDXR = msg->MemoryHighAddr; // I2caRegs.I2CDXR = msg->MemoryLowAddr; // for (i=0; iNumOfBytes-2; i++) for (i=0; iNumOfBytes; i++) { I2caRegs.I2CDXR = *(msg->MsgBuffer+i); } // Send start as master transmitter I2caRegs.I2CMDR.all = 0x6E20 ; return I2C_SUCCESS; } Uint16 I2CA_ReadData(struct I2CMSG *msg) { // Wait until the STP bit is cleared from any previous master communication. // Clearing of this bit by the module is delayed until after the SCD bit is // set. If this bit is not checked prior to initiating a new message, the // I2C could get confused. if (I2caRegs.I2CMDR.bit.STP == 1) { return I2C_STP_NOT_READY_ERROR; } I2caRegs.I2CSAR = msg->SlaveAddress; if(msg->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP) { // Check if bus busy if (I2caRegs.I2CSTR.bit.BB == 1) { return I2C_BUS_BUSY_ERROR; } I2caRegs.I2CCNT = 1; I2caRegs.I2CDXR = msg->MemoryHighAddr; //I2caRegs.I2CDXR = msg->MemoryLowAddr; I2caRegs.I2CMDR.all = 0x2620; // Send data to setup camera address } else if(msg->MsgStatus == I2C_MSGSTAT_RESTART) { //I2caRegs.I2CSAR = 0xC1; I2caRegs.I2CCNT = msg->NumOfBytes+1; // Setup how many bytes to expect I2caRegs.I2CMDR.all = 0x2C20; // Send restart as master receiver } return I2C_SUCCESS; } interrupt void i2c_int1a_isr(void) // I2C-A { Uint16 IntSource, i; // Read interrupt source IntSource = I2caRegs.I2CISRC.all; // Interrupt source = stop condition detected if(IntSource == I2C_SCD_ISRC) { // If completed message was writing data, reset msg to inactive state if (CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_WRITE_BUSY) { CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE; } else { // If a message receives a NACK during the address setup portion of the // Camera read, the code further below included in the register access ready // interrupt source code will generate a stop condition. After the stop // condition is received (here), set the message status to try again. // User may want to limit the number of retries before generating an error. if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY) { CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_SEND_NOSTOP; } // If completed message was reading Camera data, reset msg to inactive state // and read data from FIFO. else if (CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_READ_BUSY) { CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE; for(i=0; i < I2C_NUMBYTES; i++) { CurrentMsgPtr->MsgBuffer[i] = I2caRegs.I2CDRR; } { // Check recieved data for(i=0; i < I2C_NUMBYTES; i++) { if(I2cMsgIn1.MsgBuffer[i] == I2cMsgOut1.MsgBuffer[i]) { PassCount++; } else { FailCount++; } } if(PassCount == I2C_NUMBYTES) { //pass(); } else { //fail(); } } } } } // end of stop condition detected // Interrupt source = Register Access Ready // This interrupt is used to determine when the Camera address setup portion of the // read data communication is complete. Since no stop bit is commanded, this flag // tells us when the message has been sent instead of the SCD flag. If a NACK is // received, clear the NACK bit and command a stop. Otherwise, move on to the read // data portion of the communication. else if(IntSource == I2C_ARDY_ISRC) { if(I2caRegs.I2CSTR.bit.NACK == 1) { I2caRegs.I2CMDR.bit.STP = 1; I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT; } else if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY) { CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_RESTART; } } // end of register access ready else { // Generate some error due to invalid interrupt source asm(" ESTOP0"); } // Enable future I2C (PIE Group 8) interrupts PieCtrlRegs.PIEACK.all = PIEACK_GROUP8; } void pass() { asm(" ESTOP0"); for(;;); } void fail() { asm(" ESTOP0"); for(;;); } //=========================================================================== // No more. //===========================================================================