//########################################################################### // // //########################################################################### // $TI Release: F2833x/F2823x Header Files and Peripheral Examples V142 $ // $Release Date: November 1, 2016 $ // $Copyright: Copyright (C) 2007-2016 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File void I2CA_Init(void); //Uint16 I2CA_WriteData(Uint16 slave_add, Uint16 add, Uint16 data); Uint16 I2CA_WriteData(struct I2CMSG *msg); void init_LCD(); void print_S();//print ‘spark’ void print_Format(); void print_N();//print num of spark void print_FVP();//print freq voltage and power // // defines // #define I2C_LCD 0x3E #define I2C_RGB 0x60 #define I2C_NUMBYTES 2 #define NU 0x00 #define I2C_Command 0x80 #define I2C_Data 0x40 // Globals // struct I2CMSG I2cMsgOut1= { I2C_MSGSTAT_SEND_WITHSTOP, I2C_LCD, I2C_NUMBYTES, NU, I2C_Command, 0x12, // Msg Byte 1 }; struct I2CMSG I2cMsgOut2= { I2C_MSGSTAT_SEND_WITHSTOP, I2C_RGB, I2C_NUMBYTES, NU, I2C_Command, 0x12, // Msg Byte 1 }; struct I2CMSG I2cMsgOut3= { I2C_MSGSTAT_SEND_WITHSTOP, I2C_LCD, I2C_NUMBYTES, NU, I2C_Data, 0x12, // Msg Byte 1 }; //#define Iref_min 0 //#define Vref 500 // To keep track of which way the compare value is moving //#define EPWM_CMP_UP 1 //#define EPWM_CMP_DOWN 0 //#define lapse_set 1 Uint16 num_call=0; Uint16 I2C_Format1[11]={'F',' ',' ',' ',' ','V',' ',' ',' ','P',' '}; //Uint16 I2C_Format2[9]={'P','=',' ',' ',' ','W',' ','N','='}; Uint16 I2C_Spark[5]={'S','P','A','R','K'}; Uint16 I2C_FVP[12]={'0','0','.','0',' ','0','0','0',' ','0','0','0'};// "00.0 000 000" ie 15.0(kHz) 450(V) 300(W) Uint16 I2C_N[4]={0x30,0x30,0x30,0x30};// "0000" number of spark Uint16 I2C_P[3]={0x30,0x30,0x30}; Uint16 Error;//i2C //int sci_temp1,sci_temp2,sci_temp3; void main(void) { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart); // Must have this line for ram download to dsp InitFlash(); InitSysCtrl(); // Step 2. Initialize GPIO, ADC, SCI: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // InitGpio14_15(); // Gpio14 for relay1, Gpio15 for relay2 InitI2CGpio(); // DELAY_US(1000); // DELAY_US(1000); // scib_xmit(0x2E); // Step 3. Clear all interrupts and initialize PIE vector table***************************** // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. InitPieCtrl(); // Define ADCCLK clock frequency ( less than or equal to 25 MHz ) // Assuming InitSysCtrl() has set SYSCLKOUT to 150 MHz // EALLOW; // SysCtrlRegs.HISPCP.all = 3; // Sysclkout/6=25MHz // EDIS; // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // scib_xmit(0x3E); // DELAY_US(10000); // Step 4. configure ePWM // Synch controlling ePWM *********************************************************** DELAY_US(100000); I2CA_Init();//init I2C // scib_xmit(0x4E); // Step 5. User specific code, enable interrupts: // DELAY_US(1000); //init lcd init_LCD(); DELAY_US(1000); //print_Format();//print Frequency format // Enable int1 which is connected to WAKEINT: // Step 6. IDLE loop. Just sit and loop forever (optional): for(;;) { int a=0; GpioDataRegs.GPBSET.bit.GPIO54 = 1 ; // Main LED //print_FVP(); I2cMsgOut1.MsgBuffer[0]=0x83; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0xC3; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r2c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0x83; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0xC3; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r2c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0x83; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0xC3; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r2c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } GpioDataRegs.GPBTOGGLE.bit.GPIO51 = 1 ;//LED blinking } } // main function end void I2CA_Init(void) { // Initialize I2C I2caRegs.I2CSAR = 0x3E; // Slave address - EEPROM control code #if (CPU_FRQ_150MHZ) // Default - For 150MHz SYSCLKOUT I2caRegs.I2CPSC.all = 14; // Prescaler - need 7-12 Mhz on module clk (150/15 = 10MHz) #endif #if (CPU_FRQ_100MHZ) // For 100 MHz SYSCLKOUT I2caRegs.I2CPSC.all = 9; // Prescaler - need 7-12 Mhz on module clk (100/10 = 10MHz) #endif I2caRegs.I2CCLKL = 10; // NOTE: must be non zero I2caRegs.I2CCLKH = 5; // NOTE: must be non zero // I2caRegs.I2CIER.all = 0x24; // Enable SCD & ARDY interrupts I2caRegs.I2CMDR.all = 0x0020; // Take I2C out of reset // Stop I2C when suspended I2caRegs.I2CFFTX.all = 0x6000; // Enable FIFO mode and TXFIFO I2caRegs.I2CFFRX.all = 0x2040; // Enable RXFIFO, clear RXFFINT, return; } Uint16 I2CA_WriteData(struct I2CMSG *msg) { // Uint16 i; // Wait until the STP bit is cleared from any previous master communication. // Clearing of this bit by the module is delayed until after the SCD bit is // set. If this bit is not checked prior to initiating a new message, the // I2C could get confused. if (I2caRegs.I2CMDR.bit.STP == 1) { return I2C_STP_NOT_READY_ERROR; } // Setup slave address I2caRegs.I2CSAR = msg->SlaveAddress; // Check if bus busy if (I2caRegs.I2CSTR.bit.BB == 1) { return I2C_BUS_BUSY_ERROR; } // Setup number of bytes to send // MsgBuffer + Address I2caRegs.I2CCNT = msg->NumOfBytes; // Setup data to send I2caRegs.I2CDXR = msg->MemoryLowAddr; I2caRegs.I2CDXR = *(msg->MsgBuffer); // Send start as master transmitter I2caRegs.I2CMDR.all = 0x6E20; // I2C_Count++; return I2C_SUCCESS; } void init_LCD()//70.5ms total { //init 3 times, function set int i; for(i=0;i<3;i++) { I2cMsgOut1.MsgBuffer[0]=0x28; Error=I2CA_WriteData(&I2cMsgOut1); DELAY_US(15000); } //display control I2cMsgOut1.MsgBuffer[0]=0x0C; Error=I2CA_WriteData(&I2cMsgOut1); DELAY_US(10000); //clear display I2cMsgOut1.MsgBuffer[0]=0x01; Error=I2CA_WriteData(&I2cMsgOut1); DELAY_US(12000); //entry mode set I2cMsgOut1.MsgBuffer[0]=0x06; Error=I2CA_WriteData(&I2cMsgOut1); DELAY_US(500); //set RGB reg mode 1, output, mode2 I2cMsgOut2.MemoryLowAddr=0x00; I2cMsgOut2.MsgBuffer[0]=0x00; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); I2cMsgOut2.MemoryLowAddr=0x08; I2cMsgOut2.MsgBuffer[0]=0xFF; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); I2cMsgOut2.MemoryLowAddr=0x01; I2cMsgOut2.MsgBuffer[0]=0x20; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); //set RGB white I2cMsgOut2.MemoryLowAddr=0x04; I2cMsgOut2.MsgBuffer[0]=0x80; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); I2cMsgOut2.MemoryLowAddr=0x03; I2cMsgOut2.MsgBuffer[0]=0x80; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); I2cMsgOut2.MemoryLowAddr=0x02; I2cMsgOut2.MsgBuffer[0]=0x80; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); // flag2=99; } // //following functions are not used // void print_Format() { int a; I2cMsgOut1.MsgBuffer[0]=0x81; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c0 DELAY_US(500); for(a=0;a<11;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Format1[a]; Error=I2CA_WriteData(&I2cMsgOut3); //Error=I2CA_WriteData(I2C_LCD,0x40,I2C_Format1[a]);// DELAY_US(500); } } void print_N() { int a; for(a=0;a<4;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_N[a]; Error=I2CA_WriteData(&I2cMsgOut3); //Error=I2CA_WriteData(I2C_LCD,0x40,I2C_N[a]);// DELAY_US(500); } } void print_S() { int a; I2cMsgOut1.MsgBuffer[0]=0x01; Error=I2CA_WriteData(&I2cMsgOut1);//clear display DELAY_US(10000); I2cMsgOut1.MsgBuffer[0]=0x83; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 DELAY_US(500); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(500); } } void print_FVP() { if(num_call==0) { I2cMsgOut1.MsgBuffer[0]=0xC0; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 } else { I2cMsgOut3.MsgBuffer[0]=I2C_FVP[num_call-1]; Error=I2CA_WriteData(&I2cMsgOut3); } num_call++; if(num_call==13) num_call=0; } //=========================================================================== // No more. //===========================================================================