/*
//###########################################################################
//
// FILE: 28069_RAM_CLA_C_lnk.cmd
//
// TITLE: Linker Command File For F28069 examples that run out of RAM
//
// This ONLY includes all SARAM blocks on the F28069 device.
// This does not include flash or OTP.
//
// Keep in mind that L0,L1,L2,L3 and L4 are protected by the code
// security module.
//
// What this means is in most cases you will want to move to
// another memory map file which has more memory defined.
//
//###########################################################################
// $TI Release: F2806x C/C++ Header Files and Peripheral Examples V136 $
// $Release Date: Apr 15, 2013 $
//###########################################################################
*/
/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in \F2806x_headers\cmd
//
// For BIOS applications add: F2806x_Headers_BIOS.cmd
// For nonBIOS applications add: F2806x_Headers_nonBIOS.cmd
========================================================= */
/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper
// locations within the memory map */
/* Uncomment this line to include file only for non-BIOS applications */
/* -l F2806x_Headers_nonBIOS.cmd */
/* Uncomment this line to include file only for BIOS applications */
/* -l F2806x_Headers_BIOS.cmd */
/* 2) In your project add the path to \F2806x_headers\cmd to the
library search path under project->build options, linker tab,
library search path (-i).
/*========================================================= */
/* Define the memory block start/length for the F2806x
PAGE 0 will be used to organize program sections
PAGE 1 will be used to organize data sections
Notes:
Memory blocks on F28069 are uniform (ie same
physical memory) in both PAGE 0 and PAGE 1.
That is the same memory region should not be
defined for both PAGE 0 and PAGE 1.
Doing so will result in corruption of program
and/or data.
Contiguous SARAM memory blocks can be combined
if required to create a larger memory block.
*/
_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x400
-stack 0x400
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
// CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
RAMM0 : origin = 0x000050, length = 0x0003B0
RAML5L8 : origin = 0x00C000, length = 0x008000
/* RAML0_L2 : origin = 0x008000, length = 0x001000 */
RAML3 : origin = 0x009000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
/* FPU Tables in Boot ROM */
FPUTABLES : origin = 0x3FD860, length = 0x0006A0
/* IQ Math Tables in Boot ROM */
IQTABLES : origin = 0x3FDF00, length = 0x000B50
IQTABLES2 : origin = 0x3FEA50, length = 0x00008C
IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA
BOOTROM : origin = 0x3FF3B0, length = 0x000C10
PAGE 1 :
/* Part of M0, BOOT rom will use this for stack */
BOOT_RSVD : origin = 0x000002, length = 0x00004E
/* on-chip RAM block M1 */
RAMM1 : origin = 0x000480, length = 0x000380
CLARAM0 : origin = 0x008800, length = 0x000400
CLARAM1 : origin = 0x008C00, length = 0x000400
CLARAM2 : origin = 0x008000, length = 0x000800
/* on-chip RAM block L4-L8 */
RAML4 : origin = 0x00A000, length = 0x002000
/* RAML5 : origin = 0x00C000, length = 0x002000 */
/* RAML6 : origin = 0x00E000, length = 0x002000 */
/* RAML7 : origin = 0x010000, length = 0x002000 */
/* RAML8 : origin = 0x012000, length = 0x002000 */
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
}
SECTIONS
{
/* Setup for "boot to SARAM" mode:
The codestart section (found in DSP28_CodeStartBranch.asm)
re-directs execution to the start of user code. */
codestart : > BEGIN, PAGE = 0
ramfuncs : > RAMM0, PAGE = 0
.text : > RAML5L8, PAGE = 0
.cinit : > RAMM0, PAGE = 0
.pinit : > RAMM0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAML4, PAGE = 1
.ebss : > RAML4, PAGE = 1
.econst : > RAML4, PAGE = 1
.esysmem : > RAML4, PAGE = 1
.sysmem : > RAML4, PAGE = 1
.cio : > RAML4, PAGE = 1
.bss_cla : > CLARAM1, PAGE = 1
.const_cla : > CLARAM1, PAGE = 1
IQmath : > RAML4, PAGE = 1
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
/* Allocate FPU math areas: */
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
Cla1Prog : > RAML3,
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
LOAD_SIZE(_Cla1funcsLoadSize),
RUN_START(_Cla1funcsRunStart),
PAGE = 0
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
Cla1DataRam0 : > CLARAM0, PAGE = 1
Cla1DataRam1 : > CLARAM1, PAGE = 1
Cla1DataRam2 : > CLARAM2, PAGE = 1
CLA1mathTables : > CLARAM1,
LOAD_START(_Cla1mathTablesLoadStart),
LOAD_END(_Cla1mathTablesLoadEnd),
LOAD_SIZE(_Cla1mathTablesLoadSize),
RUN_START(_Cla1mathTablesRunStart),
PAGE = 1
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > CLARAM1,
PAGE = 1
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib (IQmathTablesRam)
}
*/
/* Uncomment the section below if calling the IQNasin() or IQasin()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib (IQmathTablesRam)
}
*/
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/