//########################################################################### // // FILE: Example_2833xI2C_eeprom.c // // TITLE: I2C EEPROM Example // //! \addtogroup f2833x_example_list //!

I2C EEPROM (i2c_eeprom)

//! //! This program requires an external I2C EEPROM connected to //! the I2C bus at address 0x50. \n //! This program will write 1-14 words to EEPROM and read them back. //! The data written and the EEPROM address written to are contained //! in the message structure, \b I2cMsgOut1. The data read back will be //! contained in the message structure \b I2cMsgIn1. //! //! \b Watch \b Variables \n //! - I2cMsgIn1 //! - I2cMsgOut1 // //########################################################################### // $TI Release: F2833x Support Library v2.00.00.00 $ // $Release Date: Thu Oct 18 15:47:35 CDT 2018 $ // $Copyright: // Copyright (C) 2009-2018 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //########################################################################### // // Included Files // #include "DSP28x_Project.h" // Device Headerfile and Examples Include File // // Note: I2C Macros used in this example can be found in the // DSP2833x_I2C_defines.h file // // // Function Prototypes // void I2CA_Init(void); Uint16 I2CA_WriteData(struct I2CMSG *msg); //Uint16 I2CA_ReadData(struct I2CMSG *msg); //__interrupt void i2c_int1a_isr(void); void init_LCD(); void print_S();//print ‘spark’ void print_Format(); void print_N();//print num of spark void print_FVP();//print freq voltage and power #define I2C_LCD 0x3E #define I2C_RGB 0x60 #define I2C_NUMBYTES 2 #define NU 0x00 #define I2C_Command 0x80 #define I2C_Data 0x40 // // Defines // // // Globals // struct I2CMSG I2cMsgOut1= { I2C_MSGSTAT_SEND_WITHSTOP, I2C_LCD, I2C_NUMBYTES, NU, I2C_Command, 0x12, // Msg Byte 1 }; struct I2CMSG I2cMsgOut2= { I2C_MSGSTAT_SEND_WITHSTOP, I2C_RGB, I2C_NUMBYTES, NU, I2C_Command, 0x12, // Msg Byte 1 }; struct I2CMSG I2cMsgOut3= { I2C_MSGSTAT_SEND_WITHSTOP, I2C_LCD, I2C_NUMBYTES, NU, I2C_Data, 0x12, // Msg Byte 1 }; //struct I2CMSG I2cMsgIn1= //{ I2C_MSGSTAT_SEND_NOSTOP, // I2C_SLAVE_ADDR, // I2C_NUMBYTES, // I2C_EEPROM_HIGH_ADDR, // I2C_EEPROM_LOW_ADDR //}; // // Globals // //struct I2CMSG *CurrentMsgPtr; // Used in interrupts //Uint16 PassCount; //Uint16 FailCount; Uint16 num_call=0; Uint16 I2C_Format1[11]={'F',' ',' ',' ',' ','V',' ',' ',' ','P',' '}; //Uint16 I2C_Format2[9]={'P','=',' ',' ',' ','W',' ','N','='}; Uint16 I2C_Spark[5]={'S','P','A','R','K'}; Uint16 I2C_FVP[12]={'0','0','.','0',' ','0','0','0',' ','0','0','0'};// "00.0 000 000" ie 15.0(kHz) 450(V) 300(W) Uint16 I2C_N[4]={0x30,0x30,0x30,0x30};// "0000" number of spark Uint16 I2C_P[3]={0x30,0x30,0x30}; Uint16 Error; // // Main // void main(void) { // Uint16 Error; // Uint16 i; // CurrentMsgPtr = &I2cMsgOut1; // // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. // InitSysCtrl(); // // Step 2. Initialize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // //InitGpio(); // // Setup only the GP I/O only for I2C functionality // InitI2CGpio(); // // Step 3. Clear all interrupts and initialize PIE vector table // Disable CPU interrupts // DINT; // // Initialize PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. // InitPieCtrl(); // // Disable CPU interrupts and clear all CPU interrupt flags // IER = 0x0000; IFR = 0x0000; // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. // InitPieVectTable(); // // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. // // EALLOW; // This is needed to write to EALLOW protected registers // PieVectTable.I2CINT1A = &i2c_int1a_isr; // EDIS; // This is needed to disable write to EALLOW protected registers // // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2833x_InitPeripherals.c // // InitPeripherals(); // Not required for this example DELAY_US(100000); I2CA_Init(); // // Step 5. User specific code // // // Clear Counters // // PassCount = 0; // FailCount = 0; // // Clear incoming message buffer // // for (i = 0; i < I2C_MAX_BUFFER_SIZE; i++) // { // I2cMsgIn1.MsgBuffer[i] = 0x0000; // } // // Enable interrupts required for this example // // // // // Enable I2C interrupt 1 in the PIE: Group 8 interrupt 1 // // // PieCtrlRegs.PIEIER8.bit.INTx1 = 1; // // // // // Enable CPU INT8 which is connected to PIE group 8 // // // IER |= M_INT8; // EINT; init_LCD(); DELAY_US(1000); // // Application loop // for(;;) { int a=0; // GpioDataRegs.GPBSET.bit.GPIO54 = 1 ; // Main LED //print_FVP(); I2cMsgOut1.MsgBuffer[0]=0x83; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0xC3; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r2c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0x83; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0xC3; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r2c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0x83; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } I2cMsgOut1.MsgBuffer[0]=0xC3; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r2c3 DELAY_US(10000); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(1000); } GpioDataRegs.GPBTOGGLE.bit.GPIO51 = 1 ;//LED blinking } } // end of main // // I2CA_Init - // void I2CA_Init(void) { // // Initialize I2C // I2caRegs.I2CSAR = 0x3E; // Slave address - EEPROM control code #if (CPU_FRQ_150MHZ) // Default - For 150MHz SYSCLKOUT // // Prescaler - need 7-12 Mhz on module clk (150/15 = 10MHz) // I2caRegs.I2CPSC.all = 14; #endif #if (CPU_FRQ_100MHZ) // For 100 MHz SYSCLKOUT // // Prescaler - need 7-12 Mhz on module clk (100/10 = 10MHz) // I2caRegs.I2CPSC.all = 9; #endif I2caRegs.I2CCLKL = 10; // NOTE: must be non zero I2caRegs.I2CCLKH = 5; // NOTE: must be non zero // I2caRegs.I2CIER.all = 0x24; // Enable SCD & ARDY interrupts // // Take I2C out of reset // Stop I2C when suspended // I2caRegs.I2CMDR.all = 0x0020; I2caRegs.I2CFFTX.all = 0x6000; // Enable FIFO mode and TXFIFO I2caRegs.I2CFFRX.all = 0x2040; // Enable RXFIFO, clear RXFFINT, return; } // // I2CA_WriteData - // Uint16 I2CA_WriteData(struct I2CMSG *msg) { // Uint16 i; // // Wait until the STP bit is cleared from any previous master communication // Clearing of this bit by the module is delayed until after the SCD bit is // set. If this bit is not checked prior to initiating a new message, the // I2C could get confused. // if (I2caRegs.I2CMDR.bit.STP == 1) { return I2C_STP_NOT_READY_ERROR; } // // Setup slave address // I2caRegs.I2CSAR = msg->SlaveAddress; // // Check if bus busy // if (I2caRegs.I2CSTR.bit.BB == 1) { return I2C_BUS_BUSY_ERROR; } // // Setup number of bytes to send MsgBuffer + Address // I2caRegs.I2CCNT = msg->NumOfBytes; // // Setup data to send // //I2caRegs.I2CDXR = msg->MemoryHighAddr; I2caRegs.I2CDXR = msg->MemoryLowAddr; // for (i=0; iNumOfBytes; i++) // { // I2caRegs.I2CDXR = *(msg->MsgBuffer+i); // } I2caRegs.I2CDXR = *(msg->MsgBuffer); // // Send start as master transmitter // I2caRegs.I2CMDR.all = 0x6E20; return I2C_SUCCESS; } void init_LCD()//70.5ms total { //init 3 times, function set int i; for(i=0;i<3;i++) { I2cMsgOut1.MsgBuffer[0]=0x28; Error=I2CA_WriteData(&I2cMsgOut1); DELAY_US(15000); } //display control I2cMsgOut1.MsgBuffer[0]=0x0C; Error=I2CA_WriteData(&I2cMsgOut1); DELAY_US(10000); //clear display I2cMsgOut1.MsgBuffer[0]=0x01; Error=I2CA_WriteData(&I2cMsgOut1); DELAY_US(12000); //entry mode set I2cMsgOut1.MsgBuffer[0]=0x06; Error=I2CA_WriteData(&I2cMsgOut1); DELAY_US(500); //set RGB reg mode 1, output, mode2 I2cMsgOut2.MemoryLowAddr=0x00; I2cMsgOut2.MsgBuffer[0]=0x00; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); I2cMsgOut2.MemoryLowAddr=0x08; I2cMsgOut2.MsgBuffer[0]=0xFF; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); I2cMsgOut2.MemoryLowAddr=0x01; I2cMsgOut2.MsgBuffer[0]=0x20; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); //set RGB white I2cMsgOut2.MemoryLowAddr=0x04; I2cMsgOut2.MsgBuffer[0]=0x80; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); I2cMsgOut2.MemoryLowAddr=0x03; I2cMsgOut2.MsgBuffer[0]=0x80; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); I2cMsgOut2.MemoryLowAddr=0x02; I2cMsgOut2.MsgBuffer[0]=0x80; Error=I2CA_WriteData(&I2cMsgOut2); DELAY_US(500); } // //following functions are not used // void print_Format() { int a; I2cMsgOut1.MsgBuffer[0]=0x81; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c0 DELAY_US(500); for(a=0;a<11;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Format1[a]; Error=I2CA_WriteData(&I2cMsgOut3); //Error=I2CA_WriteData(I2C_LCD,0x40,I2C_Format1[a]);// DELAY_US(500); } } void print_N() { int a; for(a=0;a<4;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_N[a]; Error=I2CA_WriteData(&I2cMsgOut3); //Error=I2CA_WriteData(I2C_LCD,0x40,I2C_N[a]);// DELAY_US(500); } } void print_S() { int a; I2cMsgOut1.MsgBuffer[0]=0x01; Error=I2CA_WriteData(&I2cMsgOut1);//clear display DELAY_US(10000); I2cMsgOut1.MsgBuffer[0]=0x83; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 DELAY_US(500); for(a=0;a<5;a++) { I2cMsgOut3.MsgBuffer[0]=I2C_Spark[a]; Error=I2CA_WriteData(&I2cMsgOut3); DELAY_US(500); } } void print_FVP() { if(num_call==0) { I2cMsgOut1.MsgBuffer[0]=0xC0; Error=I2CA_WriteData(&I2cMsgOut1);//where to print r1c3 } else { I2cMsgOut3.MsgBuffer[0]=I2C_FVP[num_call-1]; Error=I2CA_WriteData(&I2cMsgOut3); } num_call++; if(num_call==13) num_call=0; } // // End of File //