//########################################################################### // // FILE: Example_2806xI2C_eeprom.c // // TITLE: I2C EEPROM Example // //! \addtogroup f2806x_example_list //!

I2C EEPROM(i2c_eeprom)

//! //! This program requires an external I2C EEPROM connected to //! the I2C bus at address 0x50. //! This program will write 1-14 words to EEPROM and read them back. //! The data written and the EEPROM address written to are contained //! in the message structure, \b I2cMsgOut1. The data read back will be //! contained in the message structure \b I2cMsgIn1. //! //! \note This program will only work on kits that have an on-board I2C EEPROM. //! //! \b Watch \b Variables \n //! - I2cMsgIn1 //! - I2cMsgOut1 // //########################################################################### // $TI Release: F2806x Support Library v2.04.00.00 $ // $Release Date: Mon May 27 06:46:38 CDT 2019 $ // $Copyright: // Copyright (C) 2009-2019 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //########################################################################### // // Included Files // #include "DSP28x_Project.h" // Device Headerfile and Examples Include File // // Note: I2C Macros used in this example can be found in the // F2806x_I2C_defines.h file // // // Function Prototypes // void I2CA_Init(void); Uint16 I2CA_WriteData(struct I2CMSG *msg); Uint16 I2CA_ReadData(struct I2CMSG *msg); __interrupt void i2c_int1a_isr(void); void pass(void); void fail(void); // // Defines // #define I2C_SLAVE_ADDR 0x50 #define I2C_NUMBYTES 2 #define I2C_EEPROM_HIGH_ADDR 0x00 #define I2C_EEPROM_LOW_ADDR 0x30 // // Globals // // Two bytes will be used for the outgoing address, // thus only setup 14 bytes maximum // struct I2CMSG I2cMsgOut1={I2C_MSGSTAT_SEND_WITHSTOP, I2C_SLAVE_ADDR, I2C_NUMBYTES, I2C_EEPROM_HIGH_ADDR, I2C_EEPROM_LOW_ADDR, 0x12, // Msg Byte 1 0x34 }; // Msg Byte 2 struct I2CMSG I2cMsgIn1={ I2C_MSGSTAT_SEND_NOSTOP, I2C_SLAVE_ADDR, I2C_NUMBYTES, I2C_EEPROM_HIGH_ADDR, I2C_EEPROM_LOW_ADDR}; struct I2CMSG *CurrentMsgPtr; // Used in interrupts Uint16 PassCount; Uint16 FailCount; // // Main // void main(void) { Uint16 Error; Uint16 i; CurrentMsgPtr = &I2cMsgOut1; // // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the F2806x_SysCtrl.c file. // InitSysCtrl(); // // Step 2. Initalize GPIO: // This example function is found in the F2806x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // //InitGpio(); // // Setup only the GP I/O only for I2C functionality // InitI2CGpio(); // // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts // DINT; // // Initialize PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the F2806x_PieCtrl.c file. // InitPieCtrl(); // // Disable CPU interrupts and clear all CPU interrupt flags // IER = 0x0000; IFR = 0x0000; // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in F2806x_DefaultIsr.c. // This function is found in F2806x_PieVect.c. // InitPieVectTable(); // // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. // EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.I2CINT1A = &i2c_int1a_isr; EDIS; // This is needed to disable write to EALLOW protected registers // // Step 4. Initialize all the Device Peripherals: // This function is found in F2806x_InitPeripherals.c // //InitPeripherals(); // Not required for this example I2CA_Init(); // // Step 5. User specific code // // // Clear Counters // PassCount = 0; FailCount = 0; // // Clear incoming message buffer // for (i = 0; i < I2C_MAX_BUFFER_SIZE; i++) { I2cMsgIn1.MsgBuffer[i] = 0x0000; } // // Enable interrupts required for this example // // // Enable I2C interrupt 1 in the PIE: Group 8 interrupt 1 // PieCtrlRegs.PIEIER8.bit.INTx1 = 1; // // Enable CPU INT8 which is connected to PIE group 8 // IER |= M_INT8; EINT; // // Application loop // for(;;) { // // Write data to EEPROM section // // // Check the outgoing message to see if it should be sent. // In this example it is initialized to send with a stop bit. // if(I2cMsgOut1.MsgStatus == I2C_MSGSTAT_SEND_WITHSTOP) { Error = I2CA_WriteData(&I2cMsgOut1); // // If communication is correctly initiated, set msg status to busy // and update CurrentMsgPtr for the interrupt service routine. // Otherwise, do nothing and try again next loop. Once message is // initiated, the I2C interrupts will handle the rest. Search for // i2c_int1a_isr in this file. // if (Error == I2C_SUCCESS) { CurrentMsgPtr = &I2cMsgOut1; I2cMsgOut1.MsgStatus = I2C_MSGSTAT_WRITE_BUSY; } } // // Read data from EEPROM section // // // Check outgoing message status. Bypass read section if status is // not inactive. // if (I2cMsgOut1.MsgStatus == I2C_MSGSTAT_INACTIVE) { // // Check incoming message status. // if(I2cMsgIn1.MsgStatus == I2C_MSGSTAT_SEND_NOSTOP) { // // EEPROM address setup portion // while(I2CA_ReadData(&I2cMsgIn1) != I2C_SUCCESS) { // // Maybe setup an attempt counter to break an infinite // while loop. The EEPROM will send back a NACK while it is // performing a write operation. Even though the write // communique is complete at this point, the EEPROM could // still be busy programming the data. Therefore, multiple // attempts are necessary. // } // // Update current message pointer and message status // CurrentMsgPtr = &I2cMsgIn1; I2cMsgIn1.MsgStatus = I2C_MSGSTAT_SEND_NOSTOP_BUSY; } // // Once message has progressed past setting up the internal address // of the EEPROM, send a restart to read the data bytes from the // EEPROM. Complete the communique with a stop bit. MsgStatus is // updated in the interrupt service routine. // else if(I2cMsgIn1.MsgStatus == I2C_MSGSTAT_RESTART) { // // Read data portion // while(I2CA_ReadData(&I2cMsgIn1) != I2C_SUCCESS) { // // Maybe setup an attempt counter to break an infinite // while loop. // } // // Update current message pointer and message status // CurrentMsgPtr = &I2cMsgIn1; I2cMsgIn1.MsgStatus = I2C_MSGSTAT_READ_BUSY; } } } } // // I2CA_Init - // void I2CA_Init(void) { // // Initialize I2C // I2caRegs.I2CSAR = I2C_SLAVE_ADDR; // Slave address - EEPROM control code I2caRegs.I2CPSC.all = 6; // Prescaler - need 7-12 Mhz on module clk I2caRegs.I2CCLKL = 10; // NOTE: must be non zero I2caRegs.I2CCLKH = 5; // NOTE: must be non zero I2caRegs.I2CIER.all = 0x24; // Enable SCD & ARDY interrupts // // Take I2C out of reset. Stop I2C when suspended // I2caRegs.I2CMDR.all = 0x0020; I2caRegs.I2CFFTX.all = 0x6000; // Enable FIFO mode and TXFIFO I2caRegs.I2CFFRX.all = 0x2040; // Enable RXFIFO, clear RXFFINT, return; } // // I2CA_WriteData - // Uint16 I2CA_WriteData(struct I2CMSG *msg) { Uint16 i; // // Wait until the STP bit is cleared from any previous master communication. // Clearing of this bit by the module is delayed until after the SCD bit is // set. If this bit is not checked prior to initiating a new message, the // I2C could get confused. // if (I2caRegs.I2CMDR.bit.STP == 1) { return I2C_STP_NOT_READY_ERROR; } // // Setup slave address // I2caRegs.I2CSAR = msg->SlaveAddress; // // Check if bus busy // if (I2caRegs.I2CSTR.bit.BB == 1) { return I2C_BUS_BUSY_ERROR; } // // Setup number of bytes to send MsgBuffer + Address // I2caRegs.I2CCNT = msg->NumOfBytes+2; // // Setup data to send // I2caRegs.I2CDXR = msg->MemoryHighAddr; I2caRegs.I2CDXR = msg->MemoryLowAddr; // for (i=0; iNumOfBytes-2; i++) for (i=0; iNumOfBytes; i++) { I2caRegs.I2CDXR = *(msg->MsgBuffer+i); } // // Send start as master transmitter // I2caRegs.I2CMDR.all = 0x6E20; return I2C_SUCCESS; } // // I2CA_ReadData - // Uint16 I2CA_ReadData(struct I2CMSG *msg) { // // Wait until the STP bit is cleared from any previous master communication. // Clearing of this bit by the module is delayed until after the SCD bit is // set. If this bit is not checked prior to initiating a new message, the // I2C could get confused. // if (I2caRegs.I2CMDR.bit.STP == 1) { return I2C_STP_NOT_READY_ERROR; } I2caRegs.I2CSAR = msg->SlaveAddress; if(msg->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP) { // // Check if bus busy // if (I2caRegs.I2CSTR.bit.BB == 1) { return I2C_BUS_BUSY_ERROR; } I2caRegs.I2CCNT = 2; I2caRegs.I2CDXR = msg->MemoryHighAddr; I2caRegs.I2CDXR = msg->MemoryLowAddr; // // Send data to setup EEPROM address // I2caRegs.I2CMDR.all = 0x2620; } else if(msg->MsgStatus == I2C_MSGSTAT_RESTART) { I2caRegs.I2CCNT = msg->NumOfBytes; // Setup how many bytes to expect I2caRegs.I2CMDR.all = 0x2C20; // Send restart as master receiver } return I2C_SUCCESS; } // // i2c_int1a_isr - I2C-A // __interrupt void i2c_int1a_isr(void) { Uint16 IntSource, i; // // Read interrupt source // IntSource = I2caRegs.I2CISRC.all; // // Interrupt source = stop condition detected // if(IntSource == I2C_SCD_ISRC) { // // If completed message was writing data, reset msg to inactive state // if (CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_WRITE_BUSY) { CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE; } else { // // If a message receives a NACK during the address setup portion // of the EEPROM read, the code further below included in the // register access ready interrupt source code will generate a stop // condition. After the stop condition is received (here), set the // message status to try again. User may want to limit the number // of retries before generating an error. // if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY) { CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_SEND_NOSTOP; } // // If completed message was reading EEPROM data, reset msg to // inactive state and read data from FIFO. // else if (CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_READ_BUSY) { CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE; for(i=0; i < I2C_NUMBYTES; i++) { CurrentMsgPtr->MsgBuffer[i] = I2caRegs.I2CDRR; } // // Check received data // for(i=0; i < I2C_NUMBYTES; i++) { if(I2cMsgIn1.MsgBuffer[i] == I2cMsgOut1.MsgBuffer[i]) { PassCount++; } else { FailCount++; } } if(PassCount == I2C_NUMBYTES) { pass(); } else { fail(); } } } } // // Interrupt source = Register Access Ready // This interrupt is used to determine when the EEPROM address setup // portion of the read data communication is complete. Since no stop bit is // commanded, this flag tells us when the message has been sent instead of // the SCD flag. If a NACK is received, clear the NACK bit and command a // stop. Otherwise, move on to the read data portion of the communication. // else if(IntSource == I2C_ARDY_ISRC) { if(I2caRegs.I2CSTR.bit.NACK == 1) { I2caRegs.I2CMDR.bit.STP = 1; I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT; } else if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY) { CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_RESTART; } } else { // // Generate some error due to invalid interrupt source // __asm(" ESTOP0"); } // // Enable future I2C (PIE Group 8) interrupts // PieCtrlRegs.PIEACK.all = PIEACK_GROUP8; } // // pass - // void pass() { __asm(" ESTOP0"); for(;;); } // // fail - // void fail(void) { __asm(" ESTOP0"); for(;;); } // // End of File //