// TI File $Revision: /main/2 $ // Checkin $Date: July 30, 2009 18:45:31 $ //########################################################################### //// FILE: Example_2833xSci_Echoback.c // // TITLE: DSP2833x Device SCI Echoback. // // ASSUMPTIONS: // // This program requires the DSP2833x header files. // As supplied, this project is configured for "boot to SARAM" operation. // // Connect the SCI-A port to a PC via a transciever and cable. // The PC application 'hypterterminal' can be used to view the data // from the SCI and to send information to the SCI. Characters recieved // by the SCI port are sent back to the host. // // As supplied, this project is configured for "boot to SARAM" // operation. The 2833x Boot Mode table is shown below. // For information on configuring the boot mode of an eZdsp, // please refer to the documentation included with the eZdsp, // $Boot_Table: // // GPIO87 GPIO86 GPIO85 GPIO84 // XA15 XA14 XA13 XA12 // PU PU PU PU // ========================================== // 1 1 1 1 Jump to Flash // 1 1 1 0 SCI-A boot // 1 1 0 1 SPI-A boot // 1 1 0 0 I2C-A boot // 1 0 1 1 eCAN-A boot // 1 0 1 0 McBSP-A boot // 1 0 0 1 Jump to XINTF x16 // 1 0 0 0 Jump to XINTF x32 // 0 1 1 1 Jump to OTP // 0 1 1 0 Parallel GPIO I/O boot // 0 1 0 1 Parallel XINTF boot // 0 1 0 0 Jump to SARAM <- "boot to SARAM" // 0 0 1 1 Branch to check boot mode // 0 0 1 0 Boot to flash, bypass ADC cal // 0 0 0 1 Boot to SARAM, bypass ADC cal // 0 0 0 0 Boot to SCI-A, bypass ADC cal // Boot_Table_End$ // // DESCRIPTION: // // // This test recieves and echo-backs data through the SCI-A port. // // 1) Configure hyperterminal: // Use the included hyperterminal configuration file SCI_96.ht. // To load this configuration in hyperterminal: file->open // and then select the SCI_96.ht file. // 2) Check the COM port. // The configuration file is currently setup for COM1. // If this is not correct, disconnect Call->Disconnect // Open the File-Properties dialog and select the correct COM port. // 3) Connect hyperterminal Call->Call // and then start the 2833x SCI echoback program execution. // 4) The program will print out a greeting and then ask you to // enter a character which it will echo back to hyperterminal. // // As is, the program configures SCI-A for 9600 baud with // SYSCLKOUT = 150MHz and LSPCLK = 37.5 MHz // SYSCLKOUT = 100MHz and LSPCLK = 25.0 Mhz // // // Watch Variables: // LoopCount for the number of characters sent // ErrorCount //########################################################################### // $TI Release: 2833x/2823x Header Files V1.32 $ // $Release Date: June 28, 2010 $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File #include //#include // Prototype statements for functions found within this file. void scib_echoback_init(void); void scib_fifo_init(void); interrupt void scib_rx_isr(void); void scib_msg(char *msg); void scib_xmit(int a); //Global counts used in this example Uint16 LoopCount; Uint16 ErrorCount; Uint16 b=0x0,c=0x0,d=0x0,e=0x0,f=0x0,g=0x0,h=0x0,j=0x0, ans=0x0; volatile Uint16 a=0; //Uint16 temp; float voltage=0,Vb=0; float v[50]; void main(void) { int i,l=0,j=0; char *msg,*temp; // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initalize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); Skipped for this example // For this example, only init the pins for the SCI-A port. // This function is found in the DSP2833x_Sci.c file. InitScibGpio(); // Configure GPIO32 as a GPIO output pin EALLOW; GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 0;//selecting pin as GPIO GpioCtrlRegs.GPADIR.bit.GPIO31 = 1;//setting the pin as output pin EDIS; //Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2833x_InitPeripherals.c // InitPeripherals(); // Not required for this example EnableInterrupts(); // Step 5. User specific code: LoopCount = 0; ErrorCount = 0; // factor = 0x2710; scib_fifo_init(); // Initialize the SCI FIFO scib_echoback_init(); // Initalize SCI for echoback for(;;) { // Wait for inc character while(ScibRegs.SCIFFRX.bit.RXFFST !=0) { } // wait for RXDY =1 for empty state,i.e until FIFO has one word a = ScibRegs.SCIRXBUF.all; // Get character if (a != '\0') // wait till transmission starts ,note that null condition will stand true even //if voltage data sends zero,to avoid that the flag bits being sent are other then zero { //DELAY_US(100000); //these delays required to observe thepukses for sensing receiving time. GpioDataRegs.GPADAT.bit.GPIO31 = 1; d=a & 0x70; // extracts the flag bitset at the tranciever to identify the bit(MSB/LSB) c=a & 0x0F; // extracts the actual databit //DELAY_US(100000); GpioDataRegs.GPADAT.bit.GPIO31 = 0; if(d==0x40) // MSB i.e. bit b3 { e=c*0x03E8; l++; } if(d==0x30) //bit b2 { f=c*0x64; l++; } if(d==0x20) //bit b1 { g=c*0xA; l++; } if(d==0x10) //bit b0 { h=c*0x01; l++; } ans=e+f+g+h; // DELAY_US(300000); if(l==4) { voltage = (ans * 3.3)/4096; Vb = voltage/0.04394; sprintf(temp,"\r\n Message: %u",Vb); scib_msg(temp); if(j<51) { v[j]= Vb; j++; } else { j=0; v[j]= Vb; j++; } l=0; } LoopCount++; } } } // Test 1,SCIA DLB, 8-bit word, baud rate 0x000F, default, 1 STOP bit, no parity void scib_echoback_init() // Note: Clocks were turned on to the SCIA peripheral // in the InitSysCtrl() function { ScibRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback // No parity,8 char bits, // async mode, idle-line protocol ScibRegs.SCICTL1.all =0x0003; // disable TX, enable RX, internal SCICLK,(earlier 0003 correct one) // Disable RX ERR, SLEEP, TXWAKE ScibRegs.SCICTL2.all =0x0003; // initially the correct oneis 0003 //ScibRegs.SCICTL2.bit.TXINTENA =1; ScibRegs.SCICTL2.bit.RXBKINTENA =1; ScibRegs.SCICTL2.bit.TXINTENA =1; #if (CPU_FRQ_150MHZ) ScibRegs.SCIHBAUD =0x0001; // 9600 baud @LSPCLK = 37.5MHz. ScibRegs.SCILBAUD =0x00E7; #endif #if (CPU_FRQ_100MHZ) ScibRegs.SCIHBAUD =0x0001; // 9600 baud @LSPCLK = 20MHz. ScibRegs.SCILBAUD =0x0044; #endif ScibRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset(initially 0023) } // Transmit a character from the SCI void scib_xmit(int a) { while (ScibRegs.SCIFFTX.bit.TXFFST != 0) {} ScibRegs.SCITXBUF=a; } // Initalize the SCI FIFO void scib_msg(char *msg) { int i=0; while(msg[i] != '\0') { scib_xmit(msg[i]); i++; } } void scib_fifo_init() { // ScibRegs.SCIFFTX.all=0xE040; ScibRegs.SCIFFRX.all=0x204f; ScibRegs.SCIFFCT.all=0x0; SciaRegs.SCIFFCT.all=0x0; }