//#############################################################################
//
//  File:   f2802x_examples_ccsv4/spi_loopback_interrupts/Example_F2802xSpi_FFDLB_int.c
//
//  Title:  F2802x Device Spi Digital Loop Back with Interrupts Example.
//
//  Group:          C2000
//  Target Device:  TMS320F2802x
//
//! \addtogroup example_list
//!  <h1>SPI Digital Loop Back with Interrupts</h1>
//!
//!   This program is a SPI-A example that uses the internal loopback of
//!   the peripheral.  Both interrupts and the SPI FIFOs are used.
//!
//!   A stream of data is sent and then compared to the received stream.
//!
//!   The sent data looks like this:
//!   0000 0001 \n
//!   0001 0002 \n
//!   0002 0003 \n
//!   ....      \n
//!   FFFE FFFF \n
//!   FFFF 0000 \n
//!    etc..
//!
//!   This pattern is repeated forever.
//!
//!
//!   Watch Variables:
//!   - sdata[2] - Data to send
//!   - rdata[2] - Received data
//!   - rdata_point - Used to keep track of the last position in
//!                   the receive stream for error checking.
//
//  (C) Copyright 2012, Texas Instruments, Inc.
//#############################################################################
// $TI Release: f2802x Support Library v210 $
// $Release Date: Mon Sep 17 09:13:31 CDT 2012 $
//#############################################################################

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

#include "f2802x_common/include/adc.h"
#include "f2802x_common/include/clk.h"
#include "f2802x_common/include/flash.h"
#include "f2802x_common/include/gpio.h"
#include "f2802x_common/include/pie.h"
#include "f2802x_common/include/pll.h"
#include "f2802x_common/include/spi.h"
#include "f2802x_common/include/wdog.h"

// Prototype statements for functions found within this file.
// interrupt void ISRTimer2(void);
//interrupt void spiTxFifoIsr(void);
//interrupt void spiRxFifoIsr(void);
interrupt void spiTxIsr(void);
interrupt void spiRxIsr(void);
void delay_loop(void);
void spi_init(void);
void spi_fifo_init(void);
void error();

uint16_t sdata;      // Send data buffer
uint16_t rdata;      // Receive data buffer
uint16_t rdata_point;   // Keep track of where we are
                        // in the data stream to check received data

#define SLAVE_ACK 111
                     
ADC_Handle myAdc;
CLK_Handle myClk;
FLASH_Handle myFlash;
GPIO_Handle myGpio;
PIE_Handle myPie;
SPI_Handle mySpi;

void main(void)
{
  //  uint16_t i;
    
    CPU_Handle myCpu;
    PLL_Handle myPll;
    WDOG_Handle myWDog;
    
    // Initialize all the handles needed for this application    
    myAdc = ADC_init((void *)ADC_BASE_ADDR, sizeof(ADC_Obj));
    myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj));
    myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj));
    myFlash = FLASH_init((void *)FLASH_BASE_ADDR, sizeof(FLASH_Obj));
    myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj));
    myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj));
    myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj));
    mySpi = SPI_init((void *)SPIA_BASE_ADDR, sizeof(SPI_Obj));
    myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj));
    
    // Perform basic system initialization    
    WDOG_disable(myWDog);
    CLK_enableAdcClock(myClk);
    (*Device_cal)();
    
    //Enable SPI-A Clock
    CLK_enableSpiaClock(myClk);

    //Select the internal oscillator 1 as the clock source
    CLK_setOscSrc(myClk, CLK_OscSrc_Internal);
    
    // Setup the PLL for x12 /2 which will yield 60Mhz = 10Mhz * 12 / 2
    PLL_setup(myPll, PLL_Multiplier_12, PLL_DivideSelect_ClkIn_by_2);
    
    // Disable the PIE and all interrupts
    PIE_disable(myPie);
    PIE_disableAllInts(myPie);
    CPU_disableGlobalInts(myCpu);
    CPU_clearIntFlags(myCpu);
    
    // If running from flash copy RAM only functions to RAM   
#ifdef _FLASH
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif   

    // Initalize GPIO
    GPIO_setPullUp(myGpio, GPIO_Number_16, GPIO_PullUp_Enable);
    GPIO_setPullUp(myGpio, GPIO_Number_17, GPIO_PullUp_Enable);
    GPIO_setPullUp(myGpio, GPIO_Number_18, GPIO_PullUp_Enable);
    GPIO_setPullUp(myGpio, GPIO_Number_19, GPIO_PullUp_Enable);
    GPIO_setQualification(myGpio, GPIO_Number_16, GPIO_Qual_ASync);
    GPIO_setQualification(myGpio, GPIO_Number_17, GPIO_Qual_ASync);
    GPIO_setQualification(myGpio, GPIO_Number_18, GPIO_Qual_ASync);
    GPIO_setQualification(myGpio, GPIO_Number_19, GPIO_Qual_ASync);
    GPIO_setMode(myGpio, GPIO_Number_16, GPIO_16_Mode_SPISIMOA);
    GPIO_setMode(myGpio, GPIO_Number_17, GPIO_17_Mode_SPISOMIA);
    GPIO_setMode(myGpio, GPIO_Number_18, GPIO_18_Mode_SPICLKA);
    GPIO_setMode(myGpio, GPIO_Number_19, GPIO_19_Mode_SPISTEA_NOT);

    // Another Chip Select (CS)
    GPIO_setPullUp(myGpio, GPIO_Number_12, GPIO_PullUp_Enable);
    GPIO_setMode(myGpio, GPIO_Number_12, GPIO_12_Mode_GeneralPurpose);
    GPIO_setDirection(myGpio, GPIO_Number_12, GPIO_Direction_Output );

    GPIO_setPullUp(myGpio, GPIO_Number_34, GPIO_PullUp_Enable);
    GPIO_setMode(myGpio, GPIO_Number_34, GPIO_34_Mode_GeneralPurpose);
    GPIO_setDirection(myGpio, GPIO_Number_34, GPIO_Direction_Output );

    // Setup a debug vector table and enable the PIE
    PIE_setDebugIntVectorTable(myPie);
    PIE_enable(myPie);

    // Register interrupt handlers in the PIE vector table
    //PIE_registerPieIntHandler(myPie, PIE_GroupNumber_6, PIE_SubGroupNumber_1, (intVec_t)&spiRxFifoIsr);
    //PIE_registerPieIntHandler(myPie, PIE_GroupNumber_6, PIE_SubGroupNumber_2, (intVec_t)&spiTxFifoIsr);
    PIE_registerPieIntHandler(myPie, PIE_GroupNumber_6, PIE_SubGroupNumber_1, (intVec_t)&spiRxIsr);
   // PIE_registerPieIntHandler(myPie, PIE_GroupNumber_6, PIE_SubGroupNumber_2, (intVec_t)&spiTxIsr);

    // Initialize the SPI only
    spi_init();


    // Initalize the send data buffer
    //for(i=0; i<2; i++)
    //{
    //  sdata[i] = i;
    //}
    rdata = 0;
    sdata = 222;   // Master
    rdata_point = 0;

    // Enable interrupts required for this example
    PIE_enableInt(myPie, PIE_GroupNumber_6, PIE_InterruptSource_SPIARX);
   // PIE_enableInt(myPie, PIE_GroupNumber_6, PIE_InterruptSource_SPIATX);
    CPU_enableInt(myCpu, CPU_IntNumber_6);
    CPU_enableGlobalInts(myCpu);

    for(;;) {

    	GPIO_setLow(myGpio, GPIO_Number_19); // low SPISTE // Master
    	//GPIO_setLow(myGpio, GPIO_Number_34);

    	SPI_write(mySpi, sdata);

    	GPIO_setHigh(myGpio, GPIO_Number_19);
    	//GPIO_setHigh(myGpio, GPIO_Number_34);
    	asm(" NOP");

    	// Check whether the master receive ACK
    	if(rdata == SLAVE_ACK)
    	{
    		sdata++;					// Master
    		asm(" NOP");
    		asm(" NOP");
    		rdata = 0;
    	}

        asm(" NOP");
    }

}

// Some Useful local functions
void delay_loop()
{
    long      i;
    
    for (i = 0; i < 1000000; i++) {
    }
    
    return;
}

void error(void)
{
    asm("     ESTOP0");     //Test failed!! Stop!
    for (;;){
        asm(" NOP");
    }
}


void spi_init()
{

    SPI_reset(mySpi);
    SPI_enable(mySpi);

    // Reset on, rising edge, 16-bit char bits
    SPI_setCharLength(mySpi, SPI_CharLength_16_Bits);
    //SPI_setCharLength(mySpi, SPI_CharLength_8_Bits); // 8 bits
    //SPI_enableLoopBack(mySpi);
    SPI_disableLoopBack(mySpi); // no loopback

    // Enable master mode, normal phase,
    // enable talk, and SPI int disabled.
    SPI_setMode(mySpi, SPI_Mode_Master); // MASTER mode
    SPI_enableTx(mySpi);
    SPI_enableOverRunInt(mySpi);
    SPI_enableInt(mySpi);

    SPI_setBaudRate(mySpi, (SPI_BaudRate_e)0x63); // 150K baud rate


//    // Initialize SPI FIFO registers
    SPI_disableTxFifoEnh(mySpi);
    //SPI_enableFifoEnh(mySpi);
    //SPI_enableChannels(mySpi);
    //SPI_resetTxFifo(mySpi);
    //SPI_clearTxFifoInt(mySpi);
    //SPI_setTxFifoIntLevel(mySpi, SPI_FifoLevel_2_Words);
    //SPI_enableTxFifoInt(mySpi);

    //SPI_resetRxFifo(mySpi);
    //SPI_setRxFifoIntLevel(mySpi, SPI_FifoLevel_2_Words);
    //SPI_enableRxFifoInt(mySpi);
    //SPI_clearRxFifoInt(mySpi);

    //SPI_setTxDelay(mySpi, 0);

    // Set so breakpoints don't disturb xmission
    SPI_setPriority(mySpi, SPI_Priority_FreeRun);

    SPI_enable(mySpi);

    //SPI_enableTxFifo(mySpi);
    //SPI_enableRxFifo(mySpi);

}
/*
interrupt void spiTxIsr(void)
{
     uint16_t i;

        // Send data
        //SPI_write(mySpi, sdata[0]);

        // Increment data for next cycle
        sdata[0]++;

    // Clear Interrupt flag
    //SPI_clearTxFifoInt(mySpi);


    // Issue PIE ACK
    PIE_clearInt(myPie, PIE_GroupNumber_6);

    return;
}
*/
interrupt void spiRxIsr(void)
{

        // Read data
        rdata = SPI_read(mySpi);


    rdata_point++;

    // Clear Overflow flag
    //SPI_clearRxFifoOvf(mySpi);

    // Clear Interrupt flag
    //SPI_clearRxFifoInt(mySpi);

    // Issue PIE ack
    PIE_clearInt(myPie, PIE_GroupNumber_6);

    return;
}

//===========================================================================
// No more.
//===========================================================================