// TI File $Revision: /main/9 $ // Checkin $Date: July 2, 2008 14:31:12 $ //########################################################################### // // FILE: DSP2833x_Examples.h // // TITLE: DSP2833x Device Definitions. // //########################################################################### // $TI Release: DSP2833x/DSP2823x C/C++ Header Files V1.31 $ // $Release Date: August 4, 2009 $ //########################################################################### #ifndef DSP2833x_EXAMPLES_H #define DSP2833x_EXAMPLES_H #ifdef __cplusplus extern "C" { #endif /*----------------------------------------------------------------------------- Specify the PLL control register (PLLCR) and divide select (DIVSEL) value. -----------------------------------------------------------------------------*/ //#define DSP28_DIVSEL 0 // Enable /4 for SYSCLKOUT //#define DSP28_DIVSEL 1 // Enable /4 for SYSCKOUT #define DSP28_DIVSEL 2 // Enable /2 for SYSCLKOUT //#define DSP28_DIVSEL 3 // Enable /1 for SYSCLKOUT #define DSP28_PLLCR 10 //#define DSP28_PLLCR 9 //#define DSP28_PLLCR 8 //#define DSP28_PLLCR 7 //#define DSP28_PLLCR 6 //#define DSP28_PLLCR 5 //#define DSP28_PLLCR 4 //#define DSP28_PLLCR 3 //#define DSP28_PLLCR 2 //#define DSP28_PLLCR 1 //#define DSP28_PLLCR 0 // PLL is bypassed in this mode //---------------------------------------------------------------------------- /*----------------------------------------------------------------------------- Specify the clock rate of the CPU (SYSCLKOUT) in nS. Take into account the input clock frequency and the PLL multiplier selected in step 1. Use one of the values provided, or define your own. The trailing L is required tells the compiler to treat the number as a 64-bit value. Only one statement should be uncommented. Example 1:150 MHz devices: CLKIN is a 30MHz crystal. In step 1 the user specified PLLCR = 0xA for a 150Mhz CPU clock (SYSCLKOUT = 150MHz). In this case, the CPU_RATE will be 6.667L Uncomment the line: #define CPU_RATE 6.667L Example 2: 100 MHz devices: CLKIN is a 20MHz crystal. In step 1 the user specified PLLCR = 0xA for a 100Mhz CPU clock (SYSCLKOUT = 100MHz). In this case, the CPU_RATE will be 10.000L Uncomment the line: #define CPU_RATE 10.000L -----------------------------------------------------------------------------*/ #define CPU_RATE 6.667L // for a 150MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 7.143L // for a 140MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 8.333L // for a 120MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 10.000L // for a 100MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 13.330L // for a 75MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 20.000L // for a 50MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 33.333L // for a 30MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 41.667L // for a 24MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 50.000L // for a 20MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 66.667L // for a 15MHz CPU clock speed (SYSCLKOUT) //#define CPU_RATE 100.000L // for a 10MHz CPU clock speed (SYSCLKOUT) //---------------------------------------------------------------------------- /*----------------------------------------------------------------------------- Target device (in DSP2833x_Device.h) determines CPU frequency (for examples) - either 150 MHz (for 28335 and 28334) or 100 MHz (for 28332). User does not have to change anything here. -----------------------------------------------------------------------------*/ #if DSP28_28332 // DSP28_28332 device only #define CPU_FRQ_100MHZ 1 // 100 Mhz CPU Freq (20 MHz input freq) #define CPU_FRQ_150MHZ 0 #else #define CPU_FRQ_100MHZ 0 // DSP28_28335||DSP28_28334 #define CPU_FRQ_150MHZ 1 // 150 MHz CPU Freq (30 MHz input freq) by DEFAULT #endif //--------------------------------------------------------------------------- // Include Example Header Files: // #include "DSP2833x_GlobalPrototypes.h" // Prototypes for global functions within the // .c files. #include "DSP2833x_ePwm_defines.h" // Macros used for PWM examples. #include "DSP2833x_Dma_defines.h" // Macros used for DMA examples. #include "DSP2833x_I2C_defines.h" // Macros used for I2C examples. #define PARTNO_28335 0xEF #define PARTNO_28334 0xEE #define PARTNO_28332 0xED #define PARTNO_28235 0xE8 #define PARTNO_28234 0xE7 #define PARTNO_28232 0xE6 // Include files not used with DSP/BIOS #ifndef DSP28_BIOS #include "DSP2833x_DefaultISR.h" #endif // DO NOT MODIFY THIS LINE. #define DELAY_US(A) DSP28x_usDelay(((((long double) A * 1000.0L) / (long double)CPU_RATE) - 9.0L) / 5.0L) #ifdef __cplusplus } #endif /* extern "C" */ #endif // end of DSP2833x_EXAMPLES_H definition //=========================================================================== // End of file. //===========================================================================