// TI File $Revision: /main/2 $ // Checkin $Date: July 30, 2009 18:45:31 $ //########################################################################### // // FILE: Example_2833xSci_Echoback.c // // TITLE: DSP2833x Device SCI Echoback. // // ASSUMPTIONS: // // This program requires the DSP2833x header files. // As supplied, this project is configured for "boot to SARAM" operation. // // Connect the SCI-A port to a PC via a transciever and cable. // The PC application 'hypterterminal' can be used to view the data // from the SCI and to send information to the SCI. Characters recieved // by the SCI port are sent back to the host. // // As supplied, this project is configured for "boot to SARAM" // operation. The 2833x Boot Mode table is shown below. // For information on configuring the boot mode of an eZdsp, // please refer to the documentation included with the eZdsp, // // $Boot_Table: // // GPIO87 GPIO86 GPIO85 GPIO84 // XA15 XA14 XA13 XA12 // PU PU PU PU // ========================================== // 1 1 1 1 Jump to Flash // 1 1 1 0 SCI-A boot // 1 1 0 1 SPI-A boot // 1 1 0 0 I2C-A boot // 1 0 1 1 eCAN-A boot // 1 0 1 0 McBSP-A boot // 1 0 0 1 Jump to XINTF x16 // 1 0 0 0 Jump to XINTF x32 // 0 1 1 1 Jump to OTP // 0 1 1 0 Parallel GPIO I/O boot // 0 1 0 1 Parallel XINTF boot // 0 1 0 0 Jump to SARAM <- "boot to SARAM" // 0 0 1 1 Branch to check boot mode // 0 0 1 0 Boot to flash, bypass ADC cal // 0 0 0 1 Boot to SARAM, bypass ADC cal // 0 0 0 0 Boot to SCI-A, bypass ADC cal // Boot_Table_End$ // // DESCRIPTION: // // // This test recieves and echo-backs data through the SCI-A port. // // 1) Configure hyperterminal: // Use the included hyperterminal configuration file SCI_96.ht. // To load this configuration in hyperterminal: file->open // and then select the SCI_96.ht file. // 2) Check the COM port. // The configuration file is currently setup for COM1. // If this is not correct, disconnect Call->Disconnect // Open the File-Properties dialog and select the correct COM port. // 3) Connect hyperterminal Call->Call // and then start the 2833x SCI echoback program execution. // 4) The program will print out a greeting and then ask you to // enter a character which it will echo back to hyperterminal. // // As is, the program configures SCI-A for 9600 baud with // SYSCLKOUT = 150MHz and LSPCLK = 37.5 MHz // SYSCLKOUT = 100MHz and LSPCLK = 25.0 Mhz // // // Watch Variables: // LoopCount for the number of characters sent // ErrorCount // // //########################################################################### // $TI Release: DSP2833x/DSP2823x C/C++ Header Files V1.31 $ // $Release Date: August 4, 2009 $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File // Prototype statements for functions found within this file. void scia_echoback_init(void); void scia_fifo_init(void); void scia_xmit(int a); void scia_msg(char *msg); interrupt void sciaRxFifoIsr(void); // Global counts used in this example Uint16 LoopCount; Uint16 ErrorCount; Uint16 ReceivedChar; char *msg; void main(void) { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initalize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); Skipped for this example // For this example, only init the pins for the SCI-A port. // This function is found in the DSP2833x_Sci.c file. InitSciaGpio(); // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.SCIRXINTA = &sciaRxFifoIsr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2833x_InitPeripherals.c // InitPeripherals(); // Not required for this example IER |= 0x0100; // Turn INT9 ON EnableInterrupts(); // Enable PIE and global interrupts // Step 5. User specific code: LoopCount = 0; ErrorCount = 0; scia_fifo_init(); // Initialize the SCI FIFO scia_echoback_init(); // Initalize SCI for echoback msg = "\r\n\n\nHello World!\0"; scia_msg(msg); msg = "\r\nYou will enter a character, and the DSP will echo it back! \n\0"; scia_msg(msg); ReceivedChar = 1; for(;;) { //msg = "\r\nEnter a character: \0"; //scia_msg(msg); // Wait for inc character //while(SciaRegs.SCIFFRX.bit.RXFFST !=1) { } // wait for XRDY =1 for empty state // Get character //ReceivedChar = SciaRegs.SCIRXBUF.all; // Echo character back //msg = " You sent: \0"; //scia_msg(msg); //scia_xmit(ReceivedChar); //LoopCount++; } } // Test 1,SCIA DLB, 8-bit word, baud rate 0x000F, default, 1 STOP bit, no parity void scia_echoback_init() { // Note: Clocks were turned on to the SCIA peripheral // in the InitSysCtrl() function SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback // No parity,8 char bits, // async mode, idle-line protocol SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK, // Disable RX ERR, SLEEP, TXWAKE SciaRegs.SCICTL2.all =0x0003; //SciaRegs.SCICTL2.bit.TXINTENA = 1; //SciaRegs.SCICTL2.bit.RXBKINTENA = 1; SciaRegs.SCIHBAUD =0x0000; // 38400 baud @LSPCLK = 37.5MHz. SciaRegs.SCILBAUD =0x0079; SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset } // Transmit a character from the SCI void scia_xmit(int a) { while (SciaRegs.SCIFFTX.bit.TXFFST != 0) {} SciaRegs.SCITXBUF=a; } void scia_msg(char * msg) { int i; i = 0; while(msg[i] != '\0') { scia_xmit(msg[i]); i++; } } // Initalize the SCI FIFO void scia_fifo_init() { SciaRegs.SCIFFTX.all=0xE060; SciaRegs.SCIFFRX.all=0x2061; SciaRegs.SCIFFCT.all=0x0; } interrupt void sciaRxFifoIsr(void) { msg = "In Interrupt \0"; scia_msg(msg); ReceivedChar = SciaRegs.SCIRXBUF.all; SciaRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag SciaRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack } //=========================================================================== // No more. //===========================================================================