[Start: Blackhawk XDS560v2-USB System Trace Emulator_0] Execute the command: %ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\eleanki\AppData\Local\TEXASI~1\ CCS\ti\0\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 560/2xx-class product. This utility will load the program 'bh560v2u.out'. Loaded FPGA Image: C:\ti\ccsv8\ccs_base\common\uscif\dtc_top.jbc The library build date was 'Feb 8 2018'. The library build time was '17:29:28'. The library package version is '7.0.188.0'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. The controller has a version number of '6' (0x00000006). The controller has an insertion length of '0' (0x00000000). The cable+pod has a version number of '8' (0x00000008). The cable+pod has a capability number of '7423' (0x00001cff). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- The scan-path will be reset by toggling the JTAG TRST signal. The controller is the Nano-TBC VHDL. The link is a 560-class second-generation-560 cable. The software is configured for Nano-TBC VHDL features. The controller will be software reset via its registers. The controller has a logic ONE on its EMU[0] input pin. The controller has a logic ONE on its EMU[1] input pin. The controller will use falling-edge timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '2' (0x0002). The utility logic has not previously detected a power-loss. The utility logic is not currently detecting a power-loss. Loaded FPGA Image: C:\ti\ccsv8\ccs_base\common\uscif\dtc_top.jbc -----[The log-file for the JTAG TCLK output generated from the PLL]---------- Test Size Coord MHz Flag Result Description ~~~~ ~~~~ ~~~~~~~ ~~~~~~~~ ~~~~ ~~~~~~~~~~~ ~~~~~~~~~~~~~~~~~~~ 1 none - 01 00 500.0kHz - similar isit internal clock 2 none - 01 09 570.3kHz {-} similar isit internal clock 3 64 - 01 00 500.0kHz O good value measure path length 4 16 - 01 00 500.0kHz ? bad value auto step initial 5 64 - 01 00 500.0kHz ? bad value auto power initial 6 64 - 01 00 500.0kHz ? bad value auto power delta 7 64 - 02 32 445.3kHz ? bad value auto margin initial 8 64 - 02 26 398.4kHz ? bad value auto margin delta 9 64 - 02 1B 355.5kHz ? bad value auto margin delta 10 64 - 02 12 320.3kHz ? bad value auto margin delta 11 64 - 02 0A 289.1kHz ? bad value auto margin delta 12 64 - 02 02 257.8kHz ? bad value auto margin delta 13 64 - 03 36 230.5kHz ? bad value auto margin delta 14 64 - 03 2A 207.0kHz ? bad value auto margin delta 15 64 - 03 1F 185.5kHz ? bad value auto margin delta 16 64 - 03 15 166.0kHz ? bad value auto margin delta 17 64 - 03 0C 148.4kHz ? bad value auto margin delta 18 64 - 03 04 132.8kHz ? bad value auto margin delta 19 64 - 04 3A 119.1kHz ? bad value auto margin delta 20 64 - 04 2D 106.4kHz ? bad value auto margin delta 21 64 - 04 22 95.70kHz ? bad value auto margin delta 22 64 - 04 18 85.94kHz ? bad value auto margin delta 23 64 - 04 0F 77.15kHz ? bad value auto margin delta 24 64 - 04 07 69.33kHz ? bad value auto margin delta 25 64 - 04 00 62.50kHz ? bad value auto margin delta 26 64 - 05 32 55.66kHz ? bad value auto margin delta 27 64 - 05 26 49.80kHz ? bad value auto margin delta 28 64 - 05 1B 44.43kHz ? bad value auto margin delta 29 64 - 05 12 40.04kHz ? bad value auto margin delta 30 64 - 05 0A 36.13kHz ? bad value auto margin delta 31 64 - 05 02 32.23kHz ? bad value auto margin delta 32 64 - 06 36 28.81kHz ? bad value auto margin delta 33 64 - 06 2A 25.88kHz ? bad value auto margin delta 34 64 - 06 1F 23.19kHz ? bad value auto margin delta 35 64 - 06 15 20.75kHz ? bad value auto margin delta 36 64 - 06 0C 18.55kHz ? bad value auto margin delta 37 64 - 06 04 16.60kHz ? bad value auto margin delta 38 64 - 07 3A 14.89kHz ? bad value auto margin delta 39 64 - 07 2D 13.30kHz ? bad value auto margin delta 40 64 - 07 22 11.96kHz ? bad value auto margin delta 41 64 - 07 18 10.74kHz ? bad value auto margin delta 42 64 - 07 0F 9.643kHz ? bad value auto margin delta 43 64 - 07 07 8.666kHz ? bad value auto margin delta 44 64 - 07 00 7.812kHz ? bad value auto margin delta 45 64 - 08 32 6.958kHz ? bad value auto margin delta 46 64 - 08 26 6.225kHz ? bad value auto margin delta 47 64 - 08 1B 5.554kHz ? bad value auto margin delta 48 64 - 08 12 5.004kHz ? bad value auto margin delta 49 64 - 08 0A 4.516kHz ? bad value auto margin delta 50 64 - 08 02 4.028kHz ? bad value auto margin delta 51 64 - 09 36 3.601kHz ? bad value auto margin delta 52 64 - 09 2A 3.234kHz ? bad value auto margin delta 53 64 - 09 1F 2.899kHz ? bad value auto margin delta 54 64 - 09 15 2.593kHz ? bad value auto margin delta 55 64 - 09 0C 2.319kHz ? bad value auto margin delta 56 64 - 09 04 2.075kHz ? bad value auto margin delta 57 64 - 0A 3A 1.861kHz ? bad value auto margin delta 58 64 - 0A 2D 1.663kHz ? bad value auto margin delta 59 64 - 0A 22 1.495kHz ? bad value auto margin delta 60 64 - 0A 18 1.342kHz ? bad value auto margin delta 61 64 - 0A 0F 1.205kHz ? bad value auto margin delta 62 64 - 0A 07 1.083kHz ? bad value auto margin delta 63 64 - 0A 00 976.0Hz ? bad value auto margin delta 64 64 - 0B 32 869.0Hz ? bad value auto margin delta 65 64 - 0B 26 778.0Hz ? bad value auto margin delta 66 64 - 0B 1B 694.0Hz ? bad value auto margin delta 67 64 - 0B 12 625.0Hz ? bad value auto margin delta 68 64 - 0B 0A 564.0Hz ? bad value auto margin delta 69 64 - 0B 02 503.0Hz ? bad value auto margin delta 70 64 - 0B 00 488.0Hz {?} bad value auto margin delta The first internal/external clock test resuts are: The expect frequency was 500000Hz. The actual frequency was 499110Hz. The delta frequency was 890Hz. The second internal/external clock test resuts are: The expect frequency was 570312Hz. The actual frequency was 569976Hz. The delta frequency was 336Hz. In the scan-path tests: The test length was 2048 bits. The JTAG IR length was 6 bits. The JTAG DR length was 1 bits. The IR/DR scan-path tests used 70 frequencies. The IR/DR scan-path tests used 500.0kHz as the initial frequency. The IR/DR scan-path tests used 570.3kHz as the highest frequency. The IR/DR scan-path tests used 488.0Hz as the final frequency. -----[Measure the source and frequency of the final JTAG TCLKR input]-------- The frequency of the JTAG TCLKR input is measured as 488.0Hz. The frequency of the JTAG TCLKR input and TCLKO output signals are similar. The target system likely uses the TCLKO output from the emulator PLL. -----[Perform the standard path-length test on the JTAG IR and DR]----------- This path-length test uses blocks of 64 32-bit words. The test for the JTAG IR instruction path-length succeeded. The JTAG IR instruction path-length is 6 bits. The test for the JTAG DR bypass path-length succeeded. The JTAG DR bypass path-length is 1 bits. -----[Perform the Integrity scan-test on the JTAG IR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Test 4 Word 0: scanned out 0x01FC1F1D and scanned in 0x01FC1E3D. Test 4 Word 1: scanned out 0x01FC1F1D and scanned in 0x01FC1E3D. Test 4 Word 2: scanned out 0x01FC1F1D and scanned in 0x01FC1E3D. Test 4 Word 3: scanned out 0x01FC1F1D and scanned in 0x01FC1E3D. Test 4 Word 4: scanned out 0x01FC1F1D and scanned in 0x01FC1E3D. Test 4 Word 5: scanned out 0x01FC1F1D and scanned in 0x01FC1E3D. Test 4 Word 6: scanned out 0x01FC1F1D and scanned in 0x01FC1E3D. Test 4 Word 7: scanned out 0x01FC1F1D and scanned in 0x01FC1E3D. The details of the first 8 errors have been provided. The utility will now report only the count of failed tests. Scan tests: 4, skipped: 0, failed: 1 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 2 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 3 Some of the values were corrupted - 49.2 percent. The JTAG IR Integrity scan-test has failed. -----[Perform the Integrity scan-test on the JTAG DR]------------------------ This test will use blocks of 64 32-bit words. This test will be applied just once. Do a test using 0xFFFFFFFF. Scan tests: 1, skipped: 0, failed: 0 Do a test using 0x00000000. Scan tests: 2, skipped: 0, failed: 0 Do a test using 0xFE03E0E2. Scan tests: 3, skipped: 0, failed: 0 Do a test using 0x01FC1F1D. Scan tests: 4, skipped: 0, failed: 0 Do a test using 0x5533CCAA. Scan tests: 5, skipped: 0, failed: 0 Do a test using 0xAACC3355. Scan tests: 6, skipped: 0, failed: 0 All of the values were scanned correctly. The JTAG DR Integrity scan-test has succeeded. [End: Blackhawk XDS560v2-USB System Trace Emulator_0]