// TI File $Revision: /main/2 $ // Checkin $Date: July 30, 2009 18:44:23 $ //########################################################################### // // FILE: Example_2833xECanBack2Back.c // // TITLE: DSP2833x eCAN Back-to-back transmission and reception in // SELF-TEST mode // // ASSUMPTIONS: // // This program requires the DSP2833x header files. // // This progrm uses the peripheral's self test mode. // Other then boot mode configuration, no other hardware configuration // is required. // // As supplied, this project is configured for "boot to SARAM" // operation. The 2833x Boot Mode table is shown below. // For information on configuring the boot mode of an eZdsp, // please refer to the documentation included with the eZdsp, // // $Boot_Table: // // GPIO87 GPIO86 GPIO85 GPIO84 // XA15 XA14 XA13 XA12 // PU PU PU PU // ========================================== // 1 1 1 1 Jump to Flash // 1 1 1 0 SCI-A boot // 1 1 0 1 SPI-A boot // 1 1 0 0 I2C-A boot // 1 0 1 1 eCAN-A boot // 1 0 1 0 McBSP-A boot // 1 0 0 1 Jump to XINTF x16 // 1 0 0 0 Jump to XINTF x32 // 0 1 1 1 Jump to OTP // 0 1 1 0 Parallel GPIO I/O boot // 0 1 0 1 Parallel XINTF boot // 0 1 0 0 Jump to SARAM <- "boot to SARAM" // 0 0 1 1 Branch to check boot mode // 0 0 1 0 Boot to flash, bypass ADC cal // 0 0 0 1 Boot to SARAM, bypass ADC cal // 0 0 0 0 Boot to SCI-A, bypass ADC cal // Boot_Table_End$ // // DESCRIPTION: // // This test transmits data back-to-back at high speed without // stopping. // The received data is verified. Any error is flagged. // MBX0 transmits to MBX16, MBX1 transmits to MBX17 and so on.... // This program illustrates the use of self-test mode // //########################################################################### // Original Author H.J. // // $TI Release: 2833x/2823x Header Files V1.32 $ // $Release Date: June 28, 2010 $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File #define TXCOUNT 1000 // Transmission will take place (TXCOUNT) times.. long i; int j; long loopcount = 0; void mailbox_check(int32 T1, int32 T2, int32 T3); void mailbox_read(int16 i); // Global variable for this example Uint32 ErrorCount; Uint32 PassCount; Uint32 MessageReceivedCount; Uint32 TestMbox1 = 0; Uint32 TestMbox2 = 0; Uint32 TestMbox3 = 0; void main(void) { Uint16 j; // eCAN control registers require read/write access using 32-bits. Thus we // will create a set of shadow registers for this example. These shadow // registers will be used to make sure the access is 32-bits and not 16. struct ECAN_REGS ECanaShadow; // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initalize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // For this example, configure CAN pins using GPIO regs here // This function is found in DSP2833x_ECan.c InitECanGpio(); // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // Step 4. Initialize all the Device Peripherals: // This function is found in DSP2833x_InitPeripherals.c // InitPeripherals(); // Not required for this example // Step 5. User specific code, enable interrupts: MessageReceivedCount = 0; ErrorCount = 0; PassCount = 0; InitECana(); // Initialize eCAN-A module // Mailboxs can be written to 16-bits or 32-bits at a time // Write to the MSGID field of TRANSMIT mailboxes MBOX0 - 15 ECanaMboxes.MBOX0.MSGID.all = 0x9555AAA0; ECanaMboxes.MBOX1.MSGID.all = 0x9555AAA1; ECanaMboxes.MBOX2.MSGID.all = 0x9555AAA2; ECanaMboxes.MBOX3.MSGID.all = 0x9555AAA3; ECanaMboxes.MBOX4.MSGID.all = 0x9555AAA4; ECanaMboxes.MBOX5.MSGID.all = 0x9555AAA5; ECanaMboxes.MBOX6.MSGID.all = 0x9555AAA6; ECanaMboxes.MBOX7.MSGID.all = 0x9555AAA7; ECanaMboxes.MBOX8.MSGID.all = 0x9555AAA8; ECanaMboxes.MBOX9.MSGID.all = 0x9555AAA9; ECanaMboxes.MBOX10.MSGID.all = 0x9555AAAA; ECanaMboxes.MBOX11.MSGID.all = 0x9555AAAB; ECanaMboxes.MBOX12.MSGID.all = 0x9555AAAC; ECanaMboxes.MBOX13.MSGID.all = 0x9555AAAD; ECanaMboxes.MBOX14.MSGID.all = 0x9555AAAE; ECanaMboxes.MBOX15.MSGID.all = 0x9555AAAF; // Write to the MSGID field of RECEIVE mailboxes MBOX16 - 31 ECanaMboxes.MBOX16.MSGID.all = 0x9555AAA0; ECanaMboxes.MBOX17.MSGID.all = 0x9555AAA1; ECanaMboxes.MBOX18.MSGID.all = 0x9555AAA2; ECanaMboxes.MBOX19.MSGID.all = 0x9555AAA3; ECanaMboxes.MBOX20.MSGID.all = 0x9555AAA4; ECanaMboxes.MBOX21.MSGID.all = 0x9555AAA5; ECanaMboxes.MBOX22.MSGID.all = 0x9555AAA6; ECanaMboxes.MBOX23.MSGID.all = 0x9555AAA7; ECanaMboxes.MBOX24.MSGID.all = 0x9555AAA8; ECanaMboxes.MBOX25.MSGID.all = 0x9555AAA9; ECanaMboxes.MBOX26.MSGID.all = 0x9555AAAA; ECanaMboxes.MBOX27.MSGID.all = 0x9555AAAB; ECanaMboxes.MBOX28.MSGID.all = 0x9555AAAC; ECanaMboxes.MBOX29.MSGID.all = 0x9555AAAD; ECanaMboxes.MBOX30.MSGID.all = 0x9555AAAE; ECanaMboxes.MBOX31.MSGID.all = 0x9555AAAF; ECanaMboxes.MBOX16.MDL.all = 0; ECanaMboxes.MBOX16.MDH.all = 0; ECanaMboxes.MBOX17.MDL.all = 0; ECanaMboxes.MBOX17.MDH.all = 0; ECanaMboxes.MBOX18.MDL.all = 0; ECanaMboxes.MBOX18.MDH.all = 0; ECanaMboxes.MBOX19.MDL.all = 0; ECanaMboxes.MBOX19.MDH.all = 0; ECanaMboxes.MBOX20.MDL.all = 0; ECanaMboxes.MBOX20.MDH.all = 0; ECanaMboxes.MBOX21.MDL.all = 0; ECanaMboxes.MBOX21.MDH.all = 0; ECanaMboxes.MBOX22.MDL.all = 0; ECanaMboxes.MBOX22.MDH.all = 0; ECanaMboxes.MBOX23.MDL.all = 0; ECanaMboxes.MBOX23.MDH.all = 0; ECanaMboxes.MBOX24.MDL.all = 0; ECanaMboxes.MBOX24.MDH.all = 0; ECanaMboxes.MBOX25.MDL.all = 0; ECanaMboxes.MBOX25.MDH.all = 0; ECanaMboxes.MBOX26.MDL.all = 0; ECanaMboxes.MBOX26.MDH.all = 0; ECanaMboxes.MBOX27.MDL.all = 0; ECanaMboxes.MBOX27.MDH.all = 0; ECanaMboxes.MBOX28.MDL.all = 0; ECanaMboxes.MBOX28.MDH.all = 0; ECanaMboxes.MBOX29.MDL.all = 0; ECanaMboxes.MBOX29.MDH.all = 0; ECanaMboxes.MBOX30.MDL.all = 0; ECanaMboxes.MBOX30.MDH.all = 0; ECanaMboxes.MBOX31.MDL.all = 0; ECanaMboxes.MBOX31.MDH.all = 0; // Configure Mailboxes 0-15 as Tx, 16-31 as Rx // Since this write is to the entire register (instead of a bit // field) a shadow register is not required. ECanaRegs.CANMD.all = 0xFFFF0000; // Enable all Mailboxes */ // Since this write is to the entire register (instead of a bit // field) a shadow register is not required. ECanaRegs.CANME.all = 0xFFFFFFFF; // Specify that 8 bits will be sent/received ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX1.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX3.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX4.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX6.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX7.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX8.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX9.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX10.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX11.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX12.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX14.MSGCTRL.bit.DLC = 8; ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8; // Write to the mailbox RAM field of MBOX0 - 15 ECanaMboxes.MBOX0.MDL.all = 0x9555AAA0; ECanaMboxes.MBOX0.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX1.MDL.all = 0x9555AAA1; ECanaMboxes.MBOX1.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX2.MDL.all = 0x9555AAA2; ECanaMboxes.MBOX2.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX3.MDL.all = 0x9555AAA3; ECanaMboxes.MBOX3.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX4.MDL.all = 0x9555AAA4; ECanaMboxes.MBOX4.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX5.MDL.all = 0x9555AAA5; ECanaMboxes.MBOX5.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX6.MDL.all = 0x9555AAA6; ECanaMboxes.MBOX6.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX7.MDL.all = 0x9555AAA7; ECanaMboxes.MBOX7.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX8.MDL.all = 0x9555AAA8; ECanaMboxes.MBOX8.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX9.MDL.all = 0x9555AAA9; ECanaMboxes.MBOX9.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX10.MDL.all = 0x9555AAAA; ECanaMboxes.MBOX10.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX11.MDL.all = 0x9555AAAB; ECanaMboxes.MBOX11.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX12.MDL.all = 0x9555AAAC; ECanaMboxes.MBOX12.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX13.MDL.all = 0x9555AAAD; ECanaMboxes.MBOX13.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX14.MDL.all = 0x9555AAAE; ECanaMboxes.MBOX14.MDH.all = 0x89ABCDEF; ECanaMboxes.MBOX15.MDL.all = 0x9555AAAF; ECanaMboxes.MBOX15.MDH.all = 0x89ABCDEF; // Since this write is to the entire register (instead of a bit // field) a shadow register is not required. EALLOW; ECanaRegs.CANMIM.all = 0xFFFFFFFF; // Configure the eCAN for self test mode // Enable the enhanced features of the eCAN. EALLOW; ECanaShadow.CANMC.all = ECanaRegs.CANMC.all; ECanaShadow.CANMC.bit.STM = 0; // Configure CAN for self-test mode ECanaRegs.CANMC.all = ECanaShadow.CANMC.all; EDIS; // Begin transmitting for(i=0; i < TXCOUNT; i++) { ECanaRegs.CANTA.all = 0xFFFFFFFF; ECanaRegs.CANTRS.all = 0x0000FFFF; // Set TRS for all transmit mailboxes while(ECanaRegs.CANTA.all != 0x0000FFFF ) {} // Wait for all TAn bits to be set.. ECanaRegs.CANTA.all = 0x0000FFFF; // Clear all TAn loopcount++; MessageReceivedCount++; //Read from Receive mailboxes and begin checking for data */ for(j=0; j<16; j++) // Read & check 16 mailboxes { mailbox_read(j); // This func reads the indicated mailbox data mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data } } } // This function reads out the contents of the indicated // by the Mailbox number (MBXnbr). void mailbox_read(int16 MBXnbr) { volatile struct MBOX *Mailbox; Mailbox = &ECanaMboxes.MBOX0 + MBXnbr; TestMbox1 = Mailbox->MDL.all; // = 0x9555AAAn (n is the MBX number) TestMbox2 = Mailbox->MDH.all; // = 0x89ABCDEF (a constant) TestMbox3 = Mailbox->MSGID.all;// = 0x9555AAAn (n is the MBX number) } // MSGID of a rcv MBX is transmitted as the MDL data. void mailbox_check(int32 T1, int32 T2, int32 T3) { if((T1 != T3) || ( T2 != 0x89ABCDEF)) { ErrorCount++; } else { PassCount++; } } //=========================================================================== // No more. //===========================================================================