// The user must define CLA_C in the project linker settings if using the // CLA C compiler // Project Properties -> C2000 Linker -> Advanced Options -> Command File // Preprocessing -> --define #ifndef CLA_C #error CLA_C must be predefined in C2000 Linker! #endif #ifdef CLA_C // Define a size for the CLA scratchpad area that will be used // by the CLA compiler for local symbols and temps // Also force references to the special symbols that mark the // scratchpad are. CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start #endif //CLA_C MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 RAMM0 : origin = 0x000122, length = 0x0002DE RAMD0 : origin = 0x00B000, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x002000 // RAMLS3 : origin = 0x009800, length = 0x000800 // RAMLS4 : origin = 0x00A000, length = 0x000800 // RAMLS5 : origin = 0x00A800, length = 0x000800 RAMGS6 : origin = 0x012000, length = 0x001000 RAMGS7 : origin = 0x013000, length = 0x001000 RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors */ FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */ FLASHB : origin = 0x082000, length = 0x008000 /* on-chip Flash */ FLASHC : origin = 0x08A000, length = 0x006000 /* on-chip Flash */ FLASHD : origin = 0x090000, length = 0x008000 /* on-chip Flash */ FLASHE : origin = 0x098000, length = 0x008000 /* on-chip Flash */ FLASHF : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */ FLASHG : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */ FLASHH : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */ PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS1 : origin = 0x008800, length = 0x000800 FLASHI : origin = 0x0B8000, length = 0x008000 /* on-chip Flash */ RAMGS0 : origin = 0x00C000, length = 0x003000 RAMGS1 : origin = 0x00F000, length = 0x001000 RAMGS2 : origin = 0x010000, length = 0x001000 RAMGS3 : origin = 0x011000, length = 0x001000 CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 } SECTIONS { /* Allocate program areas: */ .cinit : > FLASHB PAGE = 0, ALIGN(4) .pinit : > FLASHB, PAGE = 0, ALIGN(4) .text : > FLASHB PAGE = 0, ALIGN(4) codestart : > BEGIN PAGE = 0, ALIGN(4) // ramfuncs : LOAD = FLASHD, // RUN = RAMLS4, // LOAD_START(_RamfuncsLoadStart), // LOAD_SIZE(_RamfuncsLoadSize), // LOAD_END(_RamfuncsLoadEnd), // RUN_START(_RamfuncsRunStart), // RUN_SIZE(_RamfuncsRunSize), // RUN_END(_RamfuncsRunEnd), // PAGE = 0, ALIGN(4) /* Allocate uninitalized data sections: */ .stack : > RAMM1 PAGE = 1 .ebss : > RAMGS0 PAGE = 1 .esysmem : > RAMGS1 PAGE = 1 /* Initalized sections go in Flash */ .econst : > FLASHB PAGE = 0, ALIGN(4) .switch : > FLASHB PAGE = 0, ALIGN(4) .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ // Filter_RegsFile : > RAMGS0, PAGE = 1 /* CLA specific sections */ Cla1Prog : LOAD = FLASHG, RUN = RAMLS2, LOAD_START(_Cla1funcsLoadStart), LOAD_END(_Cla1funcsLoadEnd), RUN_START(_Cla1funcsRunStart), LOAD_SIZE(_Cla1funcsLoadSize), PAGE = 0, ALIGN(4) // // The address "0x01001870" is taken from TRM - 3.22.1.2. It tells the linker that the math tables // are located at this address in ROM, and its a NOLOAD section i.e. don't do anything at load time. // F28075 has an inbuild ROM that has ClaMathTables and so we are using the ROM variant of CLAMATH Library. // This saves some RAM space. // // CLA1mathTables :> 0x01001870, PAGE=0, TYPE = NOLOAD // // The CLA data rom is dual mapped, the above mentioned address is the c28x side address - We should actually use the // CLA mapping of the space when we define the section in the linker command file, so // CLA1mathTables :> 0x000F870, PAGE=1, TYPE = DSECT // // Use the following definition only when you are not using the ROM variant of CLAMATH Library // /* CLA1mathTables : LOAD = FLASHE, RUN = RAMLS0, RUN_START(_CLA1mathTablesRunStart), LOAD_START(_CLA1mathTablesLoadStart), LOAD_SIZE(_CLA1mathTablesLoadSize), PAGE = 0, ALIGN(4) */ // CLADataLS0 : > RAMLS1, PAGE=1 // CLADataLS1 : > RAMLS2, PAGE=1 Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 .TI.ramfunc : {} LOAD = FLASHC, RUN = RAMGS6, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(4) #endif #endif /* The following section definition are for SDFM examples */ Filter1_RegsFile : > RAMGS3, PAGE = 1, fill=0x1111 Filter2_RegsFile : > RAMGS3, PAGE = 1, fill=0x2222 #ifdef CLA_C /* CLA C compiler sections */ // // Must be allocated to memory the CLA has write access to // CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMLS0, PAGE = 1 .scratchpad : > RAMLS1, PAGE = 1 .bss_cla : > RAMLS1, PAGE = 1 .const_cla : LOAD = FLASHF, RUN = RAMLS1, RUN_START(_Cla1ConstRunStart), LOAD_START(_Cla1ConstLoadStart), LOAD_SIZE(_Cla1ConstLoadSize), PAGE = 1 #endif //CLA_C } /* //=========================================================================== // End of file. //=========================================================================== */