;//########################################################################### ;// ;// FILE: F2807x_CodeStartBranch.asm ;// ;// TITLE: Branch for redirecting code execution after boot. ;// ;// For these examples, code_start is the first code that is executed after ;// exiting the boot ROM code. ;// ;// The codestart section in the linker cmd file is used to physically place ;// this code at the correct memory location. This section should be placed ;// at the location the BOOT ROM will re-direct the code to. For example, ;// for boot to FLASH this code will be located at 0x3f7ff6. ;// ;// In addition, the example F2807x projects are setup such that the codegen ;// entry point is also set to the code_start label. This is done by linker ;// option -e in the project build options. When the debugger loads the code, ;// it will automatically set the PC to the "entry point" address indicated by ;// the -e linker option. In this case the debugger is simply assigning the PC, ;// it is not the same as a full reset of the device. ;// ;// The compiler may warn that the entry point for the project is other then ;// _c_init00. _c_init00 is the C environment setup and is run before ;// main() is entered. The code_start code will re-direct the execution ;// to _c_init00 and thus there is no worry and this warning can be ignored. ;// ;//########################################################################### ;// $TI Release: F2807x Support Library v3.06.00.00 $ ;// $Release Date: Mon May 27 06:53:35 CDT 2019 $ ;// $Copyright: ;// Copyright (C) 2014-2019 Texas Instruments Incorporated - http://www.ti.com/ ;// ;// Redistribution and use in source and binary forms, with or without ;// modification, are permitted provided that the following conditions ;// are met: ;// ;// Redistributions of source code must retain the above copyright ;// notice, this list of conditions and the following disclaimer. ;// ;// Redistributions in binary form must reproduce the above copyright ;// notice, this list of conditions and the following disclaimer in the ;// documentation and/or other materials provided with the ;// distribution. ;// ;// Neither the name of Texas Instruments Incorporated nor the names of ;// its contributors may be used to endorse or promote products derived ;// from this software without specific prior written permission. ;// ;// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS ;// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT ;// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR ;// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT ;// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, ;// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT ;// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, ;// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY ;// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT ;// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE ;// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. ;// $ ;//########################################################################### *********************************************************************** WD_DISABLE .set 1 ;set to 1 to disable WD, else set to 0 .ref _c_int00 .global _r_start_ebss .global _r_size_ebss .global code_start *********************************************************************** * Function: codestart section * * Description: Branch to code starting point *********************************************************************** .sect "codestart" code_start: .if WD_DISABLE == 1 LB wd_disable ;Branch to watchdog disable code .else ;Code to zero initialise ebss section before calling _c_init00 which performs direct initialisations movl XAR0,#_r_start_ebss mov AL,#0 mov AH,#(_r_size_ebss - 1) rpt AH || mov *XAR0++,AL ;End of zero-init code LB _c_int00 ;Branch to start of boot._asm in RTS library .endif ;end codestart section *********************************************************************** * Function: wd_disable * * Description: Disables the watchdog timer *********************************************************************** .if WD_DISABLE == 1 .text wd_disable: SETC OBJMODE ;Set OBJMODE for 28x object code EALLOW ;Enable EALLOW protected register access MOVZ DP, #7029h>>6 ;Set data page for WDCR register MOV @7029h, #0068h ;Set WDDIS bit in WDCR to disable WD EDIS ;Disable EALLOW protected register access ;Code to zero initialise ebss section before calling _c_init00 which performs direct initialisations movl XAR0,#_r_start_ebss mov AL,#0 mov AH,#(_r_size_ebss - 1) rpt AH || mov *XAR0++,AL ;End of zero-init code LB _c_int00 ;Branch to start of boot._asm in RTS library .endif ;end wd_disable .end ;// ;// End of file. ;//