MEMORY { PAGE 0: /* Program Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */ ZONE0 : origin = 0x004000, length = 0x001000 /* XINTF zone 0 */ RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */ RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */ /* RAML1 : origin = 0x009000, length = 0x001000*/ /* on-chip RAM block L1 */ /* RAML2 : origin = 0x00A000, length = 0x001000*/ /* on-chip RAM block L2 */ /* RAML3 : origin = 0x00B000, length = 0x001000*/ /* on-chip RAM block L3 */ /* ZONE6 : origin = 0x0100000, length = 0x100000*/ /* XINTF zone 6 */ /* ZONE7A : origin = 0x0200000, length = 0x00FC00*/ /* XINTF zone 7 - program space */ // FLASHH : origin = 0x300000, length = 0x008000 /* on-chip FLASH */ // FLASHG : origin = 0x308000, length = 0x008000 /* on-chip FLASH */ // FLASHF : origin = 0x310000, length = 0x008000 /* on-chip FLASH */ // FLASHE : origin = 0x318000, length = 0x008000 /* on-chip FLASH */ // FLASHD : origin = 0x320000, length = 0x008000 /* on-chip FLASH */ // FLASHH_B : origin = 0x300000, length = 0x037F80 /* on-chip FLASH, 留出FLASHB最后面长度为0x80的区域用来放CSM_RSVD,BEGIN和CSM_PWL */ // FLASHF_B : origin = 0x310000, length = 0x027F80 /* on-chip FLASH, 留出FLASHB最后面长度为0x80的区域用来放CSM_RSVD,BEGIN和CSM_PWL */ FLASHE_B : origin = 0x318000, length = 0x01FF80 /* on-chip FLASH, 留出FLASHB最后面长度为0x80的区域用来放CSM_RSVD,BEGIN和CSM_PWL */ // FLASHD_B : origin = 0x320000, length = 0x017F80 /* on-chip FLASH, 留出FLASHB最后面长度为0x80的区域用来放CSM_RSVD,BEGIN和CSM_PWL */ // FLASHC_B : origin = 0x328000, length = 0x00FF80 /* on-chip FLASH, 留出FLASHB最后面长度为0x80的区域用来放CSM_RSVD,BEGIN和CSM_PWL */ // FLASHC_B : origin = 0x328000, length = 0x010000 /* on-chip FLASH */ // FLASHA : origin = 0x338000, length = 0x007F80 /* on-chip FLASH */ // CSM_RSVD : origin = 0x33FF80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ // BEGIN : origin = 0x33FFF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ // CSM_PWL : origin = 0x33FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ CSM_RSVD : origin = 0x337F80, length = 0x000076 /* Part of FLASHB. Program with all 0x0000 when CSM is in use. */ BEGIN : origin = 0x337FF6, length = 0x000002 /* Part of FLASHB. Used for "boot to Flash" bootloader mode. */ CSM_PWL : origin = 0x337FF8, length = 0x000008 /* Part of FLASHB. CSM password locations in FLASHA */ OTP : origin = 0x380400, length = 0x000400 /* on-chip OTP */ ADC_CAL : origin = 0x380080, length = 0x000009 /* ADC_cal function in Reserved memory */ IQTABLES : origin = 0x3FE000, length = 0x000b50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEB50, length = 0x00008c /* IQ Math Tables in Boot ROM */ FPUTABLES : origin = 0x3FEBDC, length = 0x0006A0 /* FPU Tables in Boot ROM */ ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */ /* Registers remain on PAGE1 */ BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ /* RAMM0 : origin = 0x000050, length = 0x0003B0*/ /* on-chip RAM block M0 */ RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ /* RAML0_7 : origin = 0x008000, length = 0x008000*/ /* on-chip RAM block L1 */ RAML1_7 : origin = 0x009000, length = 0x007000 /* on-chip RAM block L1 */ /* RAML4 : origin = 0x00C000, length = 0x001000*/ /* on-chip RAM block L1 */ /* RAML5 : origin = 0x00D000, length = 0x001000*/ /* on-chip RAM block L1 */ /* RAML6 : origin = 0x00E000, length = 0x001000*/ /* on-chip RAM block L1 */ /* RAML7 : origin = 0x00F000, length = 0x001000*/ /* on-chip RAM block L1 */ ZONE6 : origin = 0x0100000, length = 0x100000 /* XINTF zone 6 */ /* ZONE7B : origin = 0x20FC00, length = 0x000400*/ /* XINTF zone 7 - data space */ ZONE7 : origin = 0x200000, length = 0x010000 /* XINTF zone 7 - data space */ /* FLASHB : origin = 0x330000, length = 0x008000*/ /* on-chip FLASH */ } /* Allocate sections to memory blocks. Note: codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code execution when booting to flash ramfuncs user defined section to store functions that will be copied from Flash into RAM */ SECTIONS { /* Allocate program areas: */ .cinit : > FLASHE_B PAGE = 0 .pinit : > FLASHE_B, PAGE = 0 .text : > FLASHE_B PAGE = 0 codestart : > BEGIN PAGE = 0 ramdelay : LOAD = FLASHE_B, RUN = RAML0, LOAD_START(_RamdelayLoadStart), LOAD_END(_RamdelayLoadEnd), RUN_START(_RamdelayRunStart), PAGE = 0 ramfuncs : LOAD = FLASHE_B, RUN = RAML0, LOAD_START(_RamfuncsLoadStart), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), PAGE = 0 csmpasswds : > CSM_PWL PAGE = 0 csm_rsvd : > CSM_RSVD PAGE = 0 /* Allocate uninitalized data sections: */ .stack : > RAMM1 PAGE = 1 .ebss : > RAML1_7 PAGE = 1 data : > RAML1_7 PAGE = 1 .esysmem : > RAML1_7 PAGE = 1 /* Initalized sections go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .econst : > FLASHE_B PAGE = 0 .switch : > FLASHE_B PAGE = 0 .sysmem : > RAML1_7 PAGE = 1 .cio : > RAML1_7 PAGE = 1 /* Allocate IQ math areas: */ IQmath : > FLASHE_B PAGE = 0 /* Math Code */ IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD /* Allocate DMA-accessible RAM sections: */ DMARAML4 : > RAML1_7, PAGE = 1 DMARAML5 : > RAML1_7, PAGE = 1 DMARAML6 : > RAML1_7, PAGE = 1 DMARAML7 : > RAML1_7, PAGE = 1 /* Allocate 0x400 of XINTF Zone 7 to storing data */ /* ZONE7DATA : > ZONE7B, PAGE = 1*/ /* .reset is a standard section used by the compiler. It contains the */ /* the address of the start of _c_int00 for C Code. /* /* When using the boot ROM this section and the CPU vector */ /* table is not needed. Thus the default type is set here to */ /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */ .adc_cal : load = ADC_CAL, PAGE = 0, TYPE = NOLOAD }