/* //########################################################################### // FILE: F28M35H52C1_c28.cmd // TITLE: Linker Command File For F28M35H52C1 Device //########################################################################### // $TI Release: F28M35x Support Library v201 $ // $Release Date: Fri Jun 7 10:51:13 CDT 2013 $ //########################################################################### */ /* ====================================================== // For Code Composer Studio V2.2 and later // --------------------------------------- // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within // the memory map. // The header linker files are found in \F28M35x_headers\cmd // For BIOS applications add: F28M35x_Headers_BIOS.cmd // For nonBIOS applications add: F28M35x_Headers_nonBIOS.cmd ========================================================= */ /* Define the memory block start/length for the F28M35x PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F28M35x are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. Contiguous SARAM memory blocks or flash sectors can be be combined if required to create a larger memory block. */ MEMORY { PAGE 0: /* Program Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */ RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */ RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */ CSM_PWL_P0 : origin = 0x13FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ ECSL_PWL_P0 : origin = 0x13FFF4, length = 0x000004 /* Part of FLASHA. ECSL password locations in FLASHA */ FLASH_EXE_ONLY_P0 : origin = 0x13FFF2, length = 0x000002 /* Part of FLASHA. Flash execute only locations in FLASHA */ BEGIN : origin = 0x13FFF0, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_RSVD : origin = 0x13FF80, length = 0x000070 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ FLASHA : origin = 0x13E000, length = 0x001F80 /* on-chip FLASH */ FLASHB : origin = 0x13C000, length = 0x002000 /* on-chip FLASH */ FPUTABLES : origin = 0x3FD258, length = 0x0006A0 /* FPU Tables in Boot ROM */ IQTABLES : origin = 0x3FD8F8, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FE448, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FE4D4, length = 0x0000AA /* IQ Math Tables in Boot ROM */ BOOTROM : origin = 0x3FEDA8, length = 0x001200 /* Boot ROM */ PIEMISHNDLR : origin = 0x3FFFBE, length = 0x000002 /* part of boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */ /* Registers remain on PAGE1 */ /*C28 Pheripheral Register Memory Region*/ PIE_CTRL : origin = 0x000CE0, length = 0x000020 /* PIE control registers */ PIE_VECT : origin = 0x000D00, length = 0x000100 /* PIE Vector Table */ PIE_VECT_CP : origin = 0x000E00, length = 0x000100 /* PIE Vector Table Copy */ DEV_EMU : origin = 0x000880, length = 0x000180 /* device emulation registers */ CSM : origin = 0x000AE0, length = 0x000020 /* code security module registers */ ADC1_RESULT : origin = 0x000B00, length = 0x000020 /* ADC1 Results register */ ADC2_RESULT : origin = 0x000B40, length = 0x000020 /* ADC2 Results register */ CPU_TIMER0 : origin = 0x000C00, length = 0x000008 /* CPU Timer0 registers */ CPU_TIMER1 : origin = 0x000C08, length = 0x000008 /* CPU Timer1 registers */ CPU_TIMER2 : origin = 0x000C10, length = 0x000008 /* CPU Timer2 registers */ DMA : origin = 0x001000, length = 0x000200 /* DMA registers */ ASYSCTRLCONFIG : origin = 0x001700, length = 0x000080 /* Analog System Control Configuration Registers */ FLASH_REGS : origin = 0x004000, length = 0x000300 /* Flash Control registers */ FLASH_ECC : origin = 0x004300, length = 0x000040 /* Flash/OTP ECC Error Log registers */ M3PLL : origin = 0x004400, length = 0x000010 /* M3 PLL Clock Configuration Registers */ EPI_REGS : origin = 0x004430, length = 0x000010 /* EPI Registers */ RAM_REGS : origin = 0x004900, length = 0x000080 /* RAM Control registers */ RAM_ERR_REGS : origin = 0x004A00, length = 0x000080 /* RAM ECC/PARITY/ACCESS Error Log Registers */ CM_MC_IPC : origin = 0x004E00, length = 0x000040 /* C28 Control to Master IPC registers */ MCBSPA : origin = 0x005000, length = 0x000040 /* McBSP-A registers */ EPWM1 : origin = 0x005100, length = 0x000080 /* EPWM1 + HRPWM registers */ EPWM2 : origin = 0x005180, length = 0x000080 /* EPWM2 + HRPWM registers */ EPWM3 : origin = 0x005200, length = 0x000080 /* EPWM3 + HRPWM registers */ EPWM4 : origin = 0x005280, length = 0x000080 /* EPWM4 + HRPWM registers */ EPWM5 : origin = 0x005300, length = 0x000080 /* EPWM5 + HRPWM registers */ EPWM6 : origin = 0x005380, length = 0x000080 /* EPWM6 + HRPWM registers */ EPWM7 : origin = 0x005400, length = 0x000080 /* EPWM7 + HRPWM registers */ EPWM8 : origin = 0x005480, length = 0x000080 /* EPWM8 + HRPWM registers */ EPWM9 : origin = 0x005500, length = 0x000080 /* EPWM9 registers (no HRPWM) */ ECAP1 : origin = 0x005A00, length = 0x000020 /* Enhanced Capture 1 registers */ ECAP2 : origin = 0x005A20, length = 0x000020 /* Enhanced Capture 2 registers */ ECAP3 : origin = 0x005A40, length = 0x000020 /* Enhanced Capture 3 registers */ ECAP4 : origin = 0x005A60, length = 0x000020 /* Enhanced Capture 4 registers */ ECAP5 : origin = 0x005A80, length = 0x000020 /* Enhanced Capture 5 registers */ ECAP6 : origin = 0x005AA0, length = 0x000020 /* Enhanced Capture 6 registers */ EQEP1 : origin = 0x005B00, length = 0x000040 /* Enhanced QEP 1 registers */ EQEP2 : origin = 0x005B40, length = 0x000040 /* Enhanced QEP 2 registers */ EQEP3 : origin = 0x005B80, length = 0x000040 /* Enhanced QEP 3 registers */ GPIOG1CTRL : origin = 0x005F80, length = 0x000040 /* GPIO control registers */ GPIOG1DAT : origin = 0x005FC0, length = 0x000020 /* GPIO data registers */ GPIOG1TRIP : origin = 0x005FE0, length = 0x000020 /* GPIO trip/LPM registers */ COMP1 : origin = 0x006400, length = 0x000020 /* Comparator + DAC 1 registers */ COMP2 : origin = 0x006420, length = 0x000020 /* Comparator + DAC 2 registers */ COMP3 : origin = 0x006440, length = 0x000020 /* Comparator + DAC 3 registers */ COMP4 : origin = 0x006460, length = 0x000020 /* Comparator + DAC 4 registers */ COMP5 : origin = 0x006480, length = 0x000020 /* Comparator + DAC 5 registers */ COMP6 : origin = 0x0064A0, length = 0x000020 /* Comparator + DAC 6 registers */ GPIOG2CTRL : origin = 0x006F80, length = 0x000040 /* GPIO control registers */ GPIOG2DAT : origin = 0x006FC0, length = 0x000020 /* GPIO data registers */ SYSTEM : origin = 0x007010, length = 0x000020 /* System control registers */ SPIA : origin = 0x007040, length = 0x000010 /* SPI-A registers */ SCIA : origin = 0x007050, length = 0x000010 /* SCI-A registers */ NMIINTRUPT : origin = 0x007060, length = 0x000010 /* NMI Watchdog Interrupt Registers */ XINTRUPT : origin = 0x007070, length = 0x000010 /* external interrupt registers */ ADC1 : origin = 0x007100, length = 0x000080 /* ADC1 registers */ ADC2 : origin = 0x007180, length = 0x000080 /* ADC2 registers */ I2CA : origin = 0x007900, length = 0x000040 /* I2C-A registers */ /*End of C28 Pheripheral region and start of RAM section*/ /* RAM Memory */ BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */ RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAML2 : origin = 0x00A000, length = 0x001000 /* on-chip RAM block L2 */ RAML3 : origin = 0x00B000, length = 0x001000 /* on-chip RAM block L3 */ RAMS0 : origin = 0x00C000, length = 0x001000 /* on-chip Shared RAM block S0 */ RAMS1 : origin = 0x00D000, length = 0x001000 /* on-chip Shared RAM block S1 */ RAMS2 : origin = 0x00E000, length = 0x001000 /* on-chip Shared RAM block S2 */ RAMS3 : origin = 0x00F000, length = 0x001000 /* on-chip Shared RAM block S3 */ RAMS4 : origin = 0x010000, length = 0x001000 /* on-chip Shared RAM block S4 */ RAMS5 : origin = 0x011000, length = 0x001000 /* on-chip Shared RAM block S5 */ RAMS6 : origin = 0x012000, length = 0x001000 /* on-chip Shared RAM block S6 */ RAMS7 : origin = 0x013000, length = 0x001000 /* on-chip Shared RAM block S7 */ CTOMRAM : origin = 0x03F800, length = 0x000380 /* C28 to M3 Message RAM */ MTOCRAM : origin = 0x03FC00, length = 0x000380 /* M3 to C28 Message RAM */ FLASH_EXE_ONLY : origin = 0x13FFF2, length = 0x000002 /* FLASH execution only locations */ ECSL_PWL : origin = 0x13FFF4, length = 0x000004 /* FLASH ECSL password locations */ CSM_PWL : origin = 0x13FFF8, length = 0x000008 /* FLASH CSM password locations. */ } /* Allocate sections to memory blocks. Note: codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code execution when booting to flash ramfuncs user defined section to store functions that will be copied from Flash into RAM */ SECTIONS { /*** PIE Vect Table and Boot ROM Variables Structures ***/ UNION run = PIE_VECT, PAGE = 1 { PieVectTableFile GROUP { EmuKeyVar EmuBModeVar FlashCallbackVar FlashScalingVar } } /* Allocate program areas: */ .cinit : > FLASHA, PAGE = 0, ALIGN(4) .pinit : > FLASHA, PAGE = 0, ALIGN(4) .text : > FLASHA, PAGE = 0, ALIGN(4) codestart : > BEGIN, PAGE = 0, ALIGN(4) #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 GROUP { .TI.ramfunc { -l F021_API_C28x_FPU32.lib} } LOAD = FLASHA, RUN = RAML0, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), RUN_START(_RamfuncsRunStart), PAGE = 0, ALIGN(4) #else GROUP { ramfuncs { -l F021_API_C28x_FPU32.lib} } LOAD = FLASHA, RUN = RAML0, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), RUN_START(_RamfuncsRunStart), PAGE = 0, ALIGN(4) #endif #endif flashexeonly : > FLASH_EXE_ONLY_P0 PAGE = 0, ALIGN(4) ecslpasswds : > ECSL_PWL_P0 PAGE = 0, ALIGN(4) csmpasswds : > CSM_PWL_P0 PAGE = 0, ALIGN(4) csm_rsvd : > CSM_RSVD PAGE = 0, ALIGN(4) /*** Peripheral Frame 0 Register Structures ***/ DevEmuRegsFile : > DEV_EMU, PAGE = 1 CsmRegsFile : > CSM, PAGE = 1 UNION run = ADC1_RESULT, PAGE = 1 { AdcResultFile Adc1ResultFile } Adc2ResultFile : > ADC2_RESULT, PAGE = 1 CpuTimer0RegsFile : > CPU_TIMER0, PAGE = 1 CpuTimer1RegsFile : > CPU_TIMER1, PAGE = 1 CpuTimer2RegsFile : > CPU_TIMER2, PAGE = 1 PieCtrlRegsFile : > PIE_CTRL, PAGE = 1 PieVectTableCopyFile : > PIE_VECT_CP, PAGE = 1 DmaRegsFile : > DMA, PAGE = 1 AnalogSysctrlRegsFile : > ASYSCTRLCONFIG, PAGE = 1 /*** Peripheral Frame 1 Register Structures ***/ FlashCtrlRegsFile : > FLASH_REGS, PAGE = 1 FlashEccRegsFile : > FLASH_ECC, PAGE = 1 M3PllRegsFile : > M3PLL, PAGE = 1 EpiRegsFile : > EPI_REGS PAGE = 1 RAMRegsFile : > RAM_REGS, PAGE = 1 RAMErrRegsFile : > RAM_ERR_REGS,PAGE = 1 CtoMIpcRegsFile : > CM_MC_IPC, PAGE = 1 /*** Peripheral Frame 2 Register Structures ***/ SysCtrlRegsFile : > SYSTEM, PAGE = 1 SpiaRegsFile : > SPIA, PAGE = 1 SciaRegsFile : > SCIA, PAGE = 1 NmiIntruptRegsFile: > NMIINTRUPT, PAGE = 1 XIntruptRegsFile : > XINTRUPT, PAGE = 1 UNION run = ADC1, PAGE = 1 { AdcRegsFile Adc1RegsFile } Adc2RegsFile : > ADC2, PAGE = 1 I2caRegsFile : > I2CA, PAGE = 1 /*** Peripheral Frame 3 Register Structures ***/ McbspaRegsFile : > MCBSPA, PAGE = 1 EPwm1RegsFile : > EPWM1, PAGE = 1 EPwm2RegsFile : > EPWM2, PAGE = 1 EPwm3RegsFile : > EPWM3, PAGE = 1 EPwm4RegsFile : > EPWM4, PAGE = 1 EPwm5RegsFile : > EPWM5, PAGE = 1 EPwm6RegsFile : > EPWM6, PAGE = 1 EPwm7RegsFile : > EPWM7, PAGE = 1 EPwm8RegsFile : > EPWM8, PAGE = 1 EPwm9RegsFile : > EPWM9, PAGE = 1 ECap1RegsFile : > ECAP1, PAGE = 1 ECap2RegsFile : > ECAP2, PAGE = 1 ECap3RegsFile : > ECAP3, PAGE = 1 ECap4RegsFile : > ECAP4, PAGE = 1 ECap5RegsFile : > ECAP5, PAGE = 1 ECap6RegsFile : > ECAP6, PAGE = 1 EQep1RegsFile : > EQEP1, PAGE = 1 EQep2RegsFile : > EQEP2, PAGE = 1 EQep3RegsFile : > EQEP3, PAGE = 1 UNION run = GPIOG1CTRL, PAGE = 1 { GpioCtrlRegsFile GpioG1CtrlRegsFile } UNION run = GPIOG1DAT, PAGE = 1 { GpioDataRegsFile GpioG1DataRegsFile } UNION run = GPIOG1TRIP, PAGE = 1 { GpioTripRegsFile GpioG1TripRegsFile } Comp1RegsFile : > COMP1, PAGE = 1 Comp2RegsFile : > COMP2, PAGE = 1 Comp3RegsFile : > COMP3, PAGE = 1 Comp4RegsFile : > COMP4, PAGE = 1 Comp5RegsFile : > COMP5, PAGE = 1 Comp6RegsFile : > COMP6, PAGE = 1 GpioG2CtrlRegsFile : > GPIOG2CTRL, PAGE = 1 GpioG2DataRegsFile : > GPIOG2DAT, PAGE = 1 /* The following section definitions are required when using the IPC API Drivers */ GROUP : > CTOMRAM, PAGE = 1 { PUTBUFFER PUTWRITEIDX GETREADIDX } GROUP : > MTOCRAM, PAGE = 1 { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT } /* Allocate uninitalized data sections: */ .stack : > RAMM0 PAGE = 1 .ebss : > RAML2 PAGE = 1 .esysmem : > RAML2 PAGE = 1 /* Initalized sections go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .econst : > FLASHA PAGE = 0, ALIGN(4) .switch : > FLASHA PAGE = 0, ALIGN(4) /* Allocate IQ math areas: */ IQmath : > FLASHA PAGE = 0 , ALIGN(4) /* Math Code */ IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD, ALIGN(4) /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD, ALIGN(4) DMARAML2 : > RAML2, PAGE = 1 DMARAML3 : > RAML3, PAGE = 1 /* Uncomment the section below if calling the IQNexp() or IQexp() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD { IQmath.lib (IQmathTablesRam) } */ /* Uncomment the section below if calling the IQNasin() or IQasin() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD { IQmath.lib (IQmathTablesRam) } */ /* .reset is a standard section used by the compiler. It contains the */ /* the address of the start of _c_int00 for C Code. /* /* When using the boot ROM this section and the CPU vector */ /* table is not needed. Thus the default type is set here to */ /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT, ALIGN(4) vectors : > VECTORS, PAGE = 0, TYPE = DSECT, ALIGN(4) /*** Code Security Module Register Structures ***/ FlashExeOnlyFile : > FLASH_EXE_ONLY, PAGE = 1 EcslPwlFile : > ECSL_PWL, PAGE = 1 CsmPwlFile : > CSM_PWL, PAGE = 1 } /* */