/* //########################################################################### // FILE: flash_programming_cpu1_FLASH.cmd // TITLE: Linker Command File For all F28X7x devices //########################################################################### // $TI Release: F2837xD Support Library v200 $ // $Release Date: Tue Jun 21 13:00:02 CDT 2016 $ // $Copyright: Copyright (C) 2013-2016 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### */ /* ====================================================== // For Code Composer Studio V2.2 and later // --------------------------------------- // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within // the memory map. // The header linker files are found in \F2837xD_headers\cmd // For BIOS applications add: F28X7x_Headers_BIOS.cmd // For nonBIOS applications add: F28X7x_Headers_nonBIOS.cmd ========================================================= */ /* Define the memory block start/length for the F28X7x PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F28M3Xx are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. Contiguous SARAM memory blocks or flash sectors can be be combined if required to create a larger memory block. */ MEMORY { PAGE 0: /* Program Memory */ /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */ /* BEGIN is used for the "boot to Flash" bootloader mode */ BEGIN : origin = 0x086000, length = 0x000002 RAMM0 : origin = 0x000122, length = 0x0002DE RAMD0 : origin = 0x00B000, length = 0x000800 RAMLS03 : origin = 0x008000, length = 0x002000 /* RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 */ RAMLS4 : origin = 0x00A000, length = 0x000800 RAMGS14 : origin = 0x01A000, length = 0x001000 RAMGS15 : origin = 0x01B000, length = 0x001000 RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors */ FLASHA : origin = 0x080000, length = 0x002000 /* on-chip Flash */ FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */ FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */ FLASHD : origin = 0x086002, length = 0x001FFE /* on-chip Flash */ FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */ FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */ FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */ FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */ FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */ FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */ FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */ FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */ FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */ FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */ BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAMD1 : origin = 0x00B800, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x000800 RAMGS0 : origin = 0x00C000, length = 0x00B000 /*RAMGS1 : origin = 0x00D000, length = 0x001000*/ /*RAMGS2 : origin = 0x00E000, length = 0x001000*/ /*RAMGS3 : origin = 0x00F000, length = 0x001000 RAMGS4 : origin = 0x010000, length = 0x001000 RAMGS5 : origin = 0x011000, length = 0x001000 RAMGS6 : origin = 0x012000, length = 0x001000 RAMGS7 : origin = 0x013000, length = 0x001000 RAMGS8 : origin = 0x014000, length = 0x001000 RAMGS9 : origin = 0x015000, length = 0x001000 RAMGS10 : origin = 0x016000, length = 0x001000*/ RAMGS11 : origin = 0x017000, length = 0x001000 RAMGS12 : origin = 0x018000, length = 0x001000 RAMGS13 : origin = 0x019000, length = 0x001000 CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400 CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400 } SECTIONS { /* Allocate program areas: */ .cinit : > FLASHD PAGE = 0, ALIGN(8) .pinit : > FLASHD, PAGE = 0, ALIGN(8) .text : >> FLASHD |FLASHE | FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(8) codestart : > BEGIN PAGE = 0, ALIGN(8) GROUP { ramfuncs dclfuncs { -l F021_API_F2837xD_FPU32.lib} } LOAD = FLASHE, RUN = RAMLS03, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(8) /* Allocate uninitalized data sections: */ .stack : > RAMM1 PAGE = 1 .ebss : >> RAMLS5 | RAMGS0 PAGE = 1 .esysmem : > RAMLS5 PAGE = 1 /* Initalized sections go in Flash */ .econst : >> FLASHE | FLASHF | FLASHG PAGE = 0, ALIGN(8) .switch : > FLASHE PAGE = 0, ALIGN(8) .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ Filter_RegsFile : > RAMGS0, PAGE = 1 SHARERAMGS0 : > RAMGS0, PAGE = 1 SHARERAMGS1 : > RAMGS11, PAGE = 1 /* Flash Programming Buffer */ BufferDataSection : > RAMD1, PAGE = 1, ALIGN(4) /* The following section definitions are required when using the IPC API Drivers */ GROUP : > CPU1TOCPU2RAM, PAGE = 1 { PUTBUFFER PUTWRITEIDX GETREADIDX } GROUP : > CPU2TOCPU1RAM, PAGE = 1 { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT } } /* //=========================================================================== // End of file. //=========================================================================== */