#define LLC_BUS_FREQUENCY							(100e6)
#define LLC_MAX_FREQUENCY                   		((float32_t)350000.0)
#define LLC_PERIOD_RELOAD_RATIO						(2u)

#define LLC_MIN_PRD_UD_MODE_COUNT					(uint32_t)((LLC_BUS_FREQUENCY / (float32_t)(LLC_MAX_FREQUENCY * LLC_PERIOD_RELOAD_RATIO)))

#define LLC_PWM_HR_TRANSFORM(Count)					(uint32_t)((uint32_t)Count << 16u)

#define NOF_PWMs_PRIMARY_STAGE						(4u)
#define NOF_PWMs_SECONDARY_STAGE					(4u)
#define NOF_LLC_PWMs								(NOF_PWMs_PRIMARY_STAGE + NOF_PWMs_SECONDARY_STAGE)


#define LLC_PRI_LEG1_HS_PWM_MODULE					(EPWM1_BASE)
#define LLC_PRI_LEG1_LS_PWM_MODULE					(EPWM18_BASE)
#define LLC_PRI_LEG2_HS_PWM_MODULE					(EPWM3_BASE)
#define LLC_PRI_LEG2_LS_PWM_MODULE					(EPWM12_BASE)

#define LLC_SEC_LEG1_HS_PWM_MODULE					(EPWM13_BASE)
#define LLC_SEC_LEG1_LS_PWM_MODULE					(EPWM2_BASE)
#define LLC_SEC_LEG2_HS_PWM_MODULE					(EPWM7_BASE)
#define LLC_SEC_LEG2_LS_PWM_MODULE					(EPWM9_BASE)


typedef enum LLC_PWM_Out_e {
	PWM_OutA = 1,
	PWM_OutB = 2,
} LLC_PWM_Out_t;



typedef enum LLCBRIDGE_Position_e {
	FB_H1L2_BRIDGE = 1u,
	FB_H2L1_BRIDGE = 2u,
} LLCBRIDGE_Position_t;



typedef struct /*ABS_LLC_PWMsTab_Descriptor_s */{
	uint32_t				PWM_BaseAddress;
	LLC_PWM_Out_t			PWM_Out;
	LLCBRIDGE_Position_t	PWM_Position;
} ABS_LLC_PWMsTab_Descriptor_t;



static ABS_LLC_PWMsTab_Descriptor_t TAB_ePWM_LLC_TableDescriptor[NOF_LLC_PWMs] = {
	{	LLC_PRI_LEG1_HS_PWM_MODULE, PWM_OutA, FB_H1L2_BRIDGE },
	{	LLC_PRI_LEG1_LS_PWM_MODULE,	PWM_OutB, FB_H2L1_BRIDGE },
	{	LLC_PRI_LEG2_HS_PWM_MODULE, PWM_OutA, FB_H2L1_BRIDGE },
	{	LLC_PRI_LEG2_LS_PWM_MODULE, PWM_OutA, FB_H1L2_BRIDGE },

	{	LLC_SEC_LEG1_HS_PWM_MODULE,	PWM_OutB, FB_H1L2_BRIDGE },
	{	LLC_SEC_LEG1_LS_PWM_MODULE, PWM_OutA, FB_H2L1_BRIDGE },
	{	LLC_SEC_LEG2_HS_PWM_MODULE, PWM_OutA, FB_H2L1_BRIDGE },
	{	LLC_SEC_LEG2_LS_PWM_MODULE, PWM_OutA, FB_H1L2_BRIDGE },




static void ABS_LLC_ConfigSingleLLC_DrivingAndSyncMosfet(uint32_t BaseAddress, uint16_t PeriodCountReload, LLCBRIDGE_Position_t Position)
{

    uint32_t pwmPeriod_ticks;


	/*
	 * compute PERIOD reload value to be loaded in HR registers
	 */
	pwmPeriod_ticks = (uint32_t)((float32_t)PeriodCountReload * 65536.0f);/* polyspace MISRA2012:10.8 [Justified:Low] "cast needed by application" */



    /*
	 * Direct access to HR PERIOD register
	 * should be faster than using drivers
	 */
    HRPWM_setTimeBasePeriod(BaseAddress, pwmPeriod_ticks);


    HRPWM_setTimeBaseCounter(BaseAddress, 0);
    HRPWM_setPhaseShift(BaseAddress, 0);
    HRPWM_setTimeBaseCounterMode(BaseAddress, EPWM_COUNTER_MODE_UP_DOWN);
    HRPWM_setEmulationMode(BaseAddress, EPWM_EMULATION_FREE_RUN);
	
	/**< Set the dividers in order to match the value of EPWMCLK_LLC **/
	HRPWM_setClockPrescaler(BaseAddress, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_2);



	/**< Loads TBPRD on PERIOD **/
    HRPWM_setPeriodLoadMode(BaseAddress, EPWM_PERIOD_SHADOW_LOAD);





	/*
	 *
	 * Action Qualifier Configuration in case of LLC_SYNCRECT_BY_PWM_TIMED
	 * If Position == H1L2
	 * - TBCTR = CMPA @UP -> PWMx HIGH
	 * - TBCTR = TBPRD -> PWMx LOW
	 *
	 * If Position == H2L1
	 * - TBCTR = CMPB @DOWN -> PWMx HIGH
	 * - TBCTR = ZERO -> PWMx LOW
	 */

    HWREGH(BaseAddress + EPWM_O_AQCTLA) = 0x0000;

	/*
	 * Generates PWM_A either from CMPA or CMPB (depends on Position)
	 */

	/**< Loads CMPA / CMPB on ZERO **/
	HRPWM_setCounterCompareShadowLoadMode(BaseAddress, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO);
	HRPWM_setCounterCompareShadowLoadMode(BaseAddress, EPWM_COUNTER_COMPARE_B, EPWM_COMP_LOAD_ON_CNTR_ZERO);

	if (Position == FB_H1L2_BRIDGE) {

 		/**< Writes the init value into CMPA --> writes PRD in order to keep the output A LOW **/
		HRPWM_setCounterCompareValue(BaseAddress, HRPWM_COUNTER_COMPARE_A, LLC_PWM_HR_TRANSFORM(0x000A));
		HRPWM_setCounterCompareValue(BaseAddress, HRPWM_COUNTER_COMPARE_B, LLC_PWM_HR_TRANSFORM(0x009C));

		HRPWM_setActionQualifierAction(BaseAddress, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
		HRPWM_setActionQualifierAction(BaseAddress, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
	}

	else if (Position == FB_H2L1_BRIDGE) {

 		/**< Writes the init value into CMPB --> writes ZERO in order to keep the output B LOW **/
		HRPWM_setCounterCompareValue(BaseAddress, HRPWM_COUNTER_COMPARE_A, LLC_PWM_HR_TRANSFORM(0x009C));
		HRPWM_setCounterCompareValue(BaseAddress, HRPWM_COUNTER_COMPARE_B, LLC_PWM_HR_TRANSFORM(0x000A));

		HRPWM_setActionQualifierAction(BaseAddress, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
		HRPWM_setActionQualifierAction(BaseAddress, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB);
	}

	else {
		/** does nothing **/
	}






	/*
	 * This setup is necessary in case of activation of HR (High Resolution) registers
	 * --> see 18.7.2 Dead-band Submodule Additional Operating Modes
	 * Otherwise the DB clock can be set as EPWM_DB_COUNTER_CLOCK_FULL_CYCLE
	 */

    /**< Deadband bypassed on RED **/
	HRPWM_setDeadBandDelayMode(BaseAddress, EPWM_DB_RED, LLC_DB_RED_DELAY_MODE_DISABLE);
    /**< Deadband bypassed on FED --> this is not actually necessary since OUTB is generated by ePWM_A (RED)**/
	HRPWM_setDeadBandDelayMode(BaseAddress, EPWM_DB_FED, LLC_DB_RED_DELAY_MODE_DISABLE);

	/**< OUTA from ePWM_A **/
	HRPWM_setDeadBandOutputSwapMode(BaseAddress, EPWM_DB_OUTPUT_A, false);

	/**< OUTB from ePWM_A **/
	HRPWM_setDeadBandOutputSwapMode(BaseAddress, EPWM_DB_OUTPUT_B, true);










	/*
	 * High Resolution registers activation
	 */
	/*
	 * this configuration is recommended if the HighResolution feature shall be used
	 * see par. 18.15.1.5.4.1 High-Resolution Period Configuration
	 */
	/**< MEP control of rising edge (CMPAHR) **/
    HRPWM_setMEPEdgeSelect(BaseAddress, HRPWM_CHANNEL_A, HRPWM_MEP_CTRL_RISING_EDGE);
	/**< MEP control of rising edge (CMPBHR) **/
    HRPWM_setMEPEdgeSelect(BaseAddress, HRPWM_CHANNEL_B, HRPWM_MEP_CTRL_RISING_EDGE);


	/** NOTE FROM TRM
	* If the HRPWM module is configured in UP-DOWN counter mode, the shadow mode for the HRPWM
	* registers must be set to load on both ZERO AND PERIOD. New values from the user are loaded to
	* the shadow registers only at CTR=ZERO, but the shadow mode of for the registers must be set to
	* both ZERO AND PERIOD.
	**/
	/**< HRCMPA loaded on ZERO **/
	HRPWM_setCounterCompareShadowLoadEvent(BaseAddress, HRPWM_CHANNEL_A, HRPWM_LOAD_ON_CNTR_ZERO_PERIOD);
	/**< HRCMPB loaded on ZERO **/
	HRPWM_setCounterCompareShadowLoadEvent(BaseAddress, HRPWM_CHANNEL_B, HRPWM_LOAD_ON_CNTR_ZERO_PERIOD);

    HRPWM_setMEPControlMode(BaseAddress, HRPWM_CHANNEL_A, HRPWM_MEP_DUTY_PERIOD_CTRL);
	HRPWM_setMEPControlMode(BaseAddress, HRPWM_CHANNEL_B, HRPWM_MEP_DUTY_PERIOD_CTRL);

    HRPWM_enableAutoConversion(BaseAddress);

    HRPWM_enablePeriodControl(BaseAddress);

}








/**--------------------------------------------------------------------------
 * @fn			void ABS_LLC_ConfigPWMs_LLCBridges(void)
 * @brief		configures LLC ePWMs peripherals in order to generate synchronous rectification switching ON the synchronous PWM
 *				in sync with driving PWM, and switching OFF based on CMPSSx output
 * @details		Configures Phase Shift, SYNC Input source, TBPRD register link, CMPA/CMPB register link
 * @param[in]
 * @calls
 * @return
 */
static void ABS_LLC_ConfigPWMs_LLCBridges(void)
{

	uint8_least Counter;

	Counter = 0;
	
	/*
	 *< REMARK FOR TI SUPPORT
	 * THIS LOOP CONFIGURES THE PWMs OF CLLC BRIDGE, DEPENDING ON THEIR POSITION IN THE BRIDGE
	 * USES FUNCTION ABS_LLC_ConfigSingleLLC_DrivingAndSyncMosfet THAT IS WRITTEN ABOVE
	 */
	while (Counter < NOF_LLC_PWMs) {
		ABS_LLC_PWMsTab_Descriptor_t *LLCTabDescriptorPtr;

		LLCTabDescriptorPtr = &TAB_ePWM_LLC_TableDescriptor[Counter];

		/*
		 * Configures the single pwm depending on the PWM position in LLC bridge
		 * All PWMS are configured as UP DOWN counter
		 */
		ABS_LLC_ConfigSingleLLC_DrivingAndSyncMosfet(LLCTabDescriptorPtr->PWM_BaseAddress, (uint16_t)LLC_MIN_PRD_UD_MODE_COUNT, LLCTabDescriptorPtr->PWM_Position);

		Counter = Counter + 1u;
	}




	/*
	 * Sets the shift phase and register links between ePWMs
	 */
	/**< PWM PRI LEG1 HS --> generates SYNCOUT **/
	EPWM_disablePhaseShiftLoad(LLC_PRI_LEG1_HS_PWM_MODULE);
	EPWM_enableSyncOutPulseSource(LLC_PRI_LEG1_HS_PWM_MODULE, EPWM_SYNC_OUT_PULSE_ON_CNTR_ZERO);



	/*
	 * PWM PRI LEG1 LS
	 * Takes the SYNC IN from PRI LEG1 HS (ePWM1) to synchronize the TB counter
	 * TBPRD is linked to PRI LEG1 HS
	 */
    EPWM_enablePhaseShiftLoad(LLC_PRI_LEG1_LS_PWM_MODULE);
	/** Sets the Sync In from Sync Out of the master (PWM8) **/
	EPWM_setSyncInPulseSource(LLC_PRI_LEG1_LS_PWM_MODULE, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
    /** Count up after sync **/
	EPWM_setCountModeAfterSync(LLC_PRI_LEG1_LS_PWM_MODULE, EPWM_COUNT_MODE_UP_AFTER_SYNC);
	/** TBPRD linked to TBPRD of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_PRI_LEG1_LS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_TBPRD);



	/*
	 * PWM PRI LEG2 HS
	 * Takes the SYNC IN from PRI LEG1 HS (ePWM1) to synchronize the TB counter
	 * TBPRD is linked to PRI LEG1 HS
	 * CMPB register is linked to PRI LEG1 LS
	 */
    EPWM_enablePhaseShiftLoad(LLC_PRI_LEG2_HS_PWM_MODULE);
	/** Sets the Sync In from Sync Out of the master (PWM8) **/
	EPWM_setSyncInPulseSource(LLC_PRI_LEG2_HS_PWM_MODULE, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
    /** Count up after sync **/
	EPWM_setCountModeAfterSync(LLC_PRI_LEG2_HS_PWM_MODULE, EPWM_COUNT_MODE_UP_AFTER_SYNC);
	/** TBPRD linked to TBPRD of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_PRI_LEG2_HS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_TBPRD);
	/** CMPB linked to CMPB of PRI 1 LS (ePWM18) **/
	EPWM_setupEPWMLinks(LLC_PRI_LEG2_HS_PWM_MODULE, EPWM_LINK_WITH_EPWM_18, EPWM_LINK_COMP_B);

	/** CMPA linked to CMPA of PRI 1 LS (ePWM18) **/
	EPWM_setupEPWMLinks(LLC_PRI_LEG2_HS_PWM_MODULE, EPWM_LINK_WITH_EPWM_18, EPWM_LINK_COMP_A);



	/*
	 * PWM PRI LEG2 LS
	 * Takes the SYNC IN from PRI LEG1 HS (ePWM1) to synchronize the TB counter
	 * TBPRD is linked to PRI LEG1 HS
	 * CMPA register is linked to PRI LEG1 HS
	 */
    EPWM_enablePhaseShiftLoad(LLC_PRI_LEG2_LS_PWM_MODULE);
	/** Sets the Sync In from Sync Out of the master (PWM8) **/
	EPWM_setSyncInPulseSource(LLC_PRI_LEG2_LS_PWM_MODULE, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
    /** Count up after sync **/
	EPWM_setCountModeAfterSync(LLC_PRI_LEG2_LS_PWM_MODULE, EPWM_COUNT_MODE_UP_AFTER_SYNC);
	/** TBPRD linked to TBPRD of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_PRI_LEG2_LS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_TBPRD);
	/** CMPA linked to CMPA of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_PRI_LEG2_LS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_COMP_A);

	/** CMPB linked to CMPB of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_PRI_LEG2_LS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_COMP_B);


	/**< Enables the ONE SHOT SYNC output --> used by PRI GATING BURST PWM to sync when entering BURST MODE **/
	/**< This needs also the standard sync out enabled, because the synch-ed output takes as source the std sync out  **/
	/**< PAY ATTENTION: this is only a enable: SYNC must be commanded by sw **/
	EPWM_enableSyncOutPulseSource(LLC_PRI_LEG2_LS_PWM_MODULE, EPWM_SYNC_OUT_PULSE_ON_CNTR_ZERO);
	EPWM_enableOneShotSync(LLC_PRI_LEG2_LS_PWM_MODULE);







	/*
	 * PWM SEC LEG1 HS
	 * Takes the SYNC IN from PRI LEG1 HS (ePWM1) to synchronize the TB counter
	 * TBPRD is linked to PRI LEG1 HS
	 * CMPA register is linked to PRI LEG1 HS
	 */
    EPWM_enablePhaseShiftLoad(LLC_SEC_LEG1_HS_PWM_MODULE);
	/** Sets the Sync In from Sync Out of the master (PWM8) **/
	EPWM_setSyncInPulseSource(LLC_SEC_LEG1_HS_PWM_MODULE, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
    /** Count up after sync **/
	EPWM_setCountModeAfterSync(LLC_SEC_LEG1_HS_PWM_MODULE, EPWM_COUNT_MODE_UP_AFTER_SYNC);
	/** TBPRD linked to TBPRD of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG1_HS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_TBPRD);
	/** CMPA linked to CMPA of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG1_HS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_COMP_A);



	/*
	 * PWM SEC LEG1 LS
	 * Takes the SYNC IN from PRI LEG1 HS (ePWM1) to synchronize the TB counter
	 * TBPRD is linked to PRI LEG1 HS
	 * CMPB register is linked to PRI LEG1 LS
	 */
    EPWM_enablePhaseShiftLoad(LLC_SEC_LEG1_LS_PWM_MODULE);
	/** Sets the Sync In from Sync Out of the master (PWM8) **/
	EPWM_setSyncInPulseSource(LLC_SEC_LEG1_LS_PWM_MODULE, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
    /** Count up after sync **/
	EPWM_setCountModeAfterSync(LLC_SEC_LEG1_LS_PWM_MODULE, EPWM_COUNT_MODE_UP_AFTER_SYNC);
	/** TBPRD linked to TBPRD of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG1_LS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_TBPRD);

	/** CMPA linked to CMPA of PRI 1 LS (ePWM18) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG1_LS_PWM_MODULE, EPWM_LINK_WITH_EPWM_18, EPWM_LINK_COMP_A);



	/*
	 * PWM SEC LEG2 HS
	 * Takes the SYNC IN from PRI LEG1 HS (ePWM1) to synchronize the TB counter
	 * TBPRD is linked to PRI LEG1 HS
	 * CMPB register is linked to PRI LEG1 LS
	 */
    EPWM_enablePhaseShiftLoad(LLC_SEC_LEG2_HS_PWM_MODULE);
	/** Sets the Sync In from Sync Out of the master (PWM8) **/
	EPWM_setSyncInPulseSource(LLC_SEC_LEG2_HS_PWM_MODULE, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
    /** Count up after sync **/
	EPWM_setCountModeAfterSync(LLC_SEC_LEG2_HS_PWM_MODULE, EPWM_COUNT_MODE_UP_AFTER_SYNC);
	/** TBPRD linked to TBPRD of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG2_HS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_TBPRD);

	/** CMPA linked to CMPA of SEC 1 LS (ePWM7) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG2_HS_PWM_MODULE, EPWM_LINK_WITH_EPWM_18, EPWM_LINK_COMP_A);

	/** CMPB linked to CMPB of PRI 1 LS (ePWM18) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG2_HS_PWM_MODULE, EPWM_LINK_WITH_EPWM_2, EPWM_LINK_COMP_B);




	/*
	 * PWM SEC LEG2 LS
	 * Takes the SYNC IN from PRI LEG1 HS (ePWM1) to synchronize the TB counter
	 * TBPRD is linked to PRI LEG1 HS
	 * CMPA register is linked to PRI LEG1 HS
	 */
    EPWM_enablePhaseShiftLoad(LLC_SEC_LEG2_LS_PWM_MODULE);
	/** Sets the Sync In from Sync Out of the master (PWM8) **/
	EPWM_setSyncInPulseSource(LLC_SEC_LEG2_LS_PWM_MODULE, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
    /** Count up after sync **/
	EPWM_setCountModeAfterSync(LLC_SEC_LEG2_LS_PWM_MODULE, EPWM_COUNT_MODE_UP_AFTER_SYNC);
	/** TBPRD linked to TBPRD of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG2_LS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_TBPRD);
	/** CMPA linked to CMPA of PRI 1 HS (ePWM1) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG2_LS_PWM_MODULE, EPWM_LINK_WITH_EPWM_1, EPWM_LINK_COMP_A);


	/** CMP3 linked to CMP3 of SEC 1 HS (ePWM13) **/
	EPWM_setupEPWMLinks(LLC_SEC_LEG2_LS_PWM_MODULE, EPWM_LINK_WITH_EPWM_13, EPWM_LINK_COMP_B);



	/**< Enables the ONE SHOT SYNC output --> used by SEC GATING BURST PWM to sync when entering BURST MODE **/
	/**< This needs also the standard sync out enabled, because the synch-ed output takes as source the std sync out  **/
	/**< PAY ATTENTION: this is only a enable: SYNC must be commanded by sw **/
	EPWM_enableSyncOutPulseSource(LLC_SEC_LEG2_LS_PWM_MODULE, EPWM_SYNC_OUT_PULSE_ON_CNTR_ZERO);
	EPWM_enableOneShotSync(LLC_SEC_LEG2_LS_PWM_MODULE);









	/*
	 * Sets the initial compare value of CMPC --> used to trigger AD conversion of HVDC I / HVDC V
	 * CMPC is set in the middle of duty cycle of PWMxA HIGH
	 * This feature is used only with Primary LLC pwm to generate a SOC for IBAT and VBAT
	 */
	EPWM_setCounterCompareValue(LLC_PRI_LEG1_HS_PWM_MODULE, EPWM_COUNTER_COMPARE_C, (LLC_MIN_PRD_UD_MODE_COUNT >> 1u));


	/*
	 * Sets the LoadMode of CMPC --> used to trigger AD conversion
	 */
	EPWM_setCounterCompareShadowLoadMode(LLC_PRI_LEG1_HS_PWM_MODULE, EPWM_COUNTER_COMPARE_C, EPWM_COMP_LOAD_ON_CNTR_ZERO);

}










/**< This function provides the clock to PWM used **/
void ABS_LLC_Enable_ePWM_Peripherals(void)
{


	/** Safety Manual par 4.2.6 - comma 1 - CLK14-Peripheral clock gating **/
    /* Peripherals for Primary LLC */
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM1);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM18);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM3);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM12);

	/**< Burst mode gating primary **/
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM17);




	/* Peripherals for Secondary LLC */
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM13);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM2);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM7);
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM9);

	/**< Burst mode gating Secondary **/
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM10);








	/* This is necessary to use the High Resolution modulator --> see par. 18.15.1.2 HRPWM Source Clock */
	/** Safety Manual par 4.2.6 - comma 1 - CLK14-Peripheral clock gating **/
	SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_HRCAL0);
	SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_HRCAL1);
	SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_HRCAL2);

}