/* // TI File $Revision: /main/4 $ // Checkin $Date: November 9, 2009 15:09:12 $ //########################################################################### // // FILE: F2808.cmd // // TITLE: Linker Command File For F2808 Device // // // For BIOS applications add: DSP2803x_Headers_BIOS.cmd // For nonBIOS applications add: DSP2803x_Headers_nonBIOS.cmd ========================================================= */ /* ====================================================== // For Code Composer Studio prior to V2.2 // -------------------------------------- // 1) Use one of the following -l statements to include the // header linker command file in the project. The header linker // file is required to link the peripheral structures to the proper // locations within the memory map */ /* Uncomment this line to include file only for non-BIOS applications */ /* -l DSP2803x_Headers_nonBIOS.cmd */ /* Uncomment this line to include file only for BIOS applications */ /* -l DSP2803x_Headers_BIOS.cmd */ /* 2) In your project add the path to \DSP2803x_headers\cmd to the library search path under project->build options, linker tab, library search path (-i). /*========================================================= */ /*********************************************************************/ /* F28035 Memory Map */ /* */ /* Note: M0M1MAP and VMAP signals tied high on PICCOLO core */ /* */ /* 0x000000 - 0x0003ff M0 SARAM (Prog and Data) */ /* 0x000400 - 0x0007ff M1 SARAM (Prog and Data) */ /* 0x000800 - 0x001fff Peripheral Frame0 (PF0) (Data only) */ /* 0x006000 - 0x0063ff Peripheral Frame1A (PF1A)(Data only) */ /* 0x006400 - 0x0069ff Peripheral Frame3 (PF3) (Data only) */ /* 0x006a00 - 0x006fff Peripheral Frame1 (PF1B)(Data only) */ /* 0x007000 - 0x007fff Peripheral Frame2 (PF2) (Data only) */ /* 0x008000 - 0x0087ff L0 SARAM (Prog and Data) */ /* 0x008800 - 0x0087ff L1 SARAM (Prog and Data) */ /* 0x008c00 - 0x008bff L2 SARAM (Prog and Data) */ /* 0x009000 - 0x009fff L3 SARAM (Prog and Data) */ /* 0x3d7800 - 0x3d7bff OTP (Prog and Data) */ /* 0x3d7c80 - 0x3d7cbf Device Cal (TI OTP) (Prog and Data) */ /* 0x3d7cc0 - 0x3d7cff Boot Get Mode (TI OTP) (Prog and Data) */ /* 0x3d7e80 - 0x3d7e80 PARTID value (Prog and Data) */ /* 0x3d7e82 - 0x3d7eb0 Calibration Data (Prog and Data) */ /* 0x3e8000 - 0x3f7fff FLASH (Prog and Data) */ /* 0x3f8000 - 0x3f87ff L0 SARAM Mirror (Prog and Data) */ /* 0x3fe000 - 0x3fffff BOOT ROM (Prog and Data) */ /********************************************************************/ /* Define the memory block start/length for the F28035 PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F2803x are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. L0 memory block is mirrored - that is it can be accessed in high memory or low memory. For simplicity only one instance is used in this linker file. Contiguous SARAM memory blocks or flash sectors can be be combined if required to create a larger memory block. */ MEMORY { PAGE 0: /* Program Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */ RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */ RAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */ OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP ONE TIME PROGRAMABLE MEMORY*/ FLASH : origin = 0x3E8000, length = 0x00FF80 /* FLASH, All sectors combined */ CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM CODE SECURITY MODULE is in use. */ BEGIN_FLASH : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */ /* Registers remain on PAGE1 */ BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 *///RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 * RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAMM2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 DATARAM : origin = 0x008C00, length = 0x000400 */ RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */ FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */ } /* Allocate sections to memory blocks. Note: codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code execution when booting to flash ramfuncs user defined section to store functions that will be copied from Flash into RAM */ SECTIONS { /*** Compiler Required Sections ***/ /* Program memory (PAGE 0) sections */ .text : {} > FLASH, PAGE = 0 .cinit : > FLASH, PAGE = 0 .const : > FLASH, PAGE = 0 .econst : > FLASH, PAGE = 0 .pinit : > FLASH, PAGE = 0 .switch : > FLASH, PAGE = 0 /* Data Memory (PAGE 1) sections */ .ebss : > RAMM0, PAGE = 1 //Table which Init global variables .cinit : > RAMM0, PAGE = 1 //global and static variables .bss > RAMM0, PAGE = 1 //global Varibles .cio : > RAMM0, PAGE = 1 //bUFFER for SDIO functions .stack : > RAMM1, PAGE = 1 //System stack .esysmem : > RAMM1, PAGE = 1 //memory for far malloc functions .switch : > RAMM1, PAGE = 1 //jump tables /*** User Defined Sections ***/ csmpasswds : > CSM_PWL_P0 PAGE = 0 csm_rsvd : > CSM_RSVD PAGE = 0 codestart : > BEGIN_FLASH, PAGE = 0 /* Used by file CodeStartBranch.asm */ csm_rsvd : > CSM_RSVD, PAGE = 0 /* Used by file passwords.asm */ dataram : > RAMM0, PAGE = 1 //new ramfuncs : LOAD = FLASH, /*load from flash */ RUN = RAML0, /* Run in RAML0 */ LOAD_START(_RamfuncsLoadStart), /* Starting Address */ LOAD_SIZE(_RamfuncsLoadSize), RUN_START(_RamfuncsRunStart), PAGE = 0 dataram : LOAD = FLASH, /*load from flash to their run address in SARAM*/ RUN = RAMM0, LOAD_START(_DataLoadStart), LOAD_SIZE(_DataLoadSize), RUN_START(_DataRunStart), PAGE = 1 /* Initalized sections go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .econst : > FLASH PAGE = 0 /* econst constants (e.g. const int k = 3;) FLASH */ .switch : > FLASH PAGE = 0 /* Allocate IQ math areas: */ IQmath : > FLASH PAGE = 0 /* Math Code */ IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Uncomment the section below if calling the IQNexp() or IQexp() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD { IQmath.lib (IQmathTablesRam) } */ /* Uncomment the section below if calling the IQNasin() or IQasin() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD { IQmath.lib (IQmathTablesRam) } */ /* .reset is a standard section used by the compiler. It contains the */ /* the address of the start of _c_int00 for C Code. /* /* When using the boot ROM this section and the CPU vector */ /* table is not needed. Thus the default type is set here to */ /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT } /* //=========================================================================== // End of file. //=========================================================================== */