// TI File $Revision: /main/11 $ // Checkin $Date: May 12, 2008 14:24:12 $ //########################################################################### // // FILE: Example_2833xSci_FFDLB.c // // TITLE: DSP2833x Device SCI FIFO Digital Loop Back Test. // // ASSUMPTIONS: // // This program requires the DSP2833x header files. // // This program uses the internal loop back test mode of the peripheral. // Other then boot mode pin configuration, no other hardware configuration // is required. // // As supplied, this project is configured for "boot to SARAM" // operation. The 2833x Boot Mode table is shown below. // For information on configuring the boot mode of an eZdsp, // please refer to the documentation included with the eZdsp, // // $Boot_Table: // // GPIO87 GPIO86 GPIO85 GPIO84 // XA15 XA14 XA13 XA12 // PU PU PU PU // ========================================== // 1 1 1 1 Jump to Flash // 1 1 1 0 SCI-A boot // 1 1 0 1 SPI-A boot // 1 1 0 0 I2C-A boot // 1 0 1 1 eCAN-A boot // 1 0 1 0 McBSP-A boot // 1 0 0 1 Jump to XINTF x16 // 1 0 0 0 Jump to XINTF x32 // 0 1 1 1 Jump to OTP // 0 1 1 0 Parallel GPIO I/O boot // 0 1 0 1 Parallel XINTF boot // 0 1 0 0 Jump to SARAM <- "boot to SARAM" // 0 0 1 1 Branch to check boot mode // 0 0 1 0 Boot to flash, bypass ADC cal // 0 0 0 1 Boot to SARAM, bypass ADC cal // 0 0 0 0 Boot to SCI-A, bypass ADC cal // Boot_Table_End$ // // DESCRIPTION: // // This test uses the loopback test mode of the SCI module to send // characters starting with 0x00 through 0xFF. The test will send // a character and then check the receive buffer for a correct match. // // Watch Variables: // LoopCount Number of characters sent // ErrorCount Number of errors detected // SendChar Character sent // ReceivedChar Character recieved // // //########################################################################### // // Original Author: S.S. // // $TI Release: DSP2833x/DSP2823x C/C++ Header Files V1.31 $ // $Release Date: August 4, 2009 $ //########################################################################### #include "DSP28x_Project.h" // Device Headerfile and Examples Include File // Prototype statements for functions found within this file. void scia_loopback_init(void); void scia_fifo_init(void); void scia_xmit(int a); void error(); interrupt void scia_rx_isr(void); interrupt void scia_tx_isr(void); // Global counts used in this example Uint16 LoopCount; Uint16 ErrorCount; Uint16 SendChar; Uint16 ReceivedChar; void main(void) { // Step 1. Initialize System Control registers, PLL, WatchDog, Clocks to default state: // This function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); // Step 2. Select GPIO for the device or for the specific application: // This function is found in the DSP2833x_Gpio.c file. // InitGpio(); skip this as this is example selects the I/O // for SCI-A in this file itself InitSciGpio(); // Step 3. Initialize PIE vector table: // The PIE vector table is initialized with pointers to shell Interrupt // Service Routines (ISR). The shell routines are found in DSP2833x_DefaultIsr.c. // Insert user specific ISR code in the appropriate shell ISR routine in // the DSP28_DefaultIsr.c file. // Disable and clear all CPU interrupts: DINT; IER = 0x0000; IFR = 0x0000; // Initialize Pie Control Registers To Default State: // This function is found in the DSP2833x_PieCtrl.c file. // InitPieCtrl(); PIE is not used for this example // Initialize the PIE Vector Table To a Known State: // This function is found in DSP2833x_PieVect.c. // This function populates the PIE vector table with pointers // to the shell ISR functions found in DSP2833x_DefaultIsr.c. InitPieVectTable(); EALLOW; PieVectTable.SCIRXINTA = &scia_rx_isr; PieVectTable.SCITXINTA = &scia_tx_isr; EDIS; // Enable CPU and PIE interrupts // This example function is found in the DSP2833x_PieCtrl.c file. EnableInterrupts(); IER|= M_INT9; PieCtrlRegs.PIEIER9.bit.INTx1 = 1; PieCtrlRegs.PIEIER9.bit.INTx2 = 1; EINT; ERTM; // EALLOW; //SysCtrlRegs.LOSPCP.bit.LSPCLK= 0; //EDIS; // Step 4. Initialize all the Device Peripherals to a known state: // This function is found in DSP2833x_InitPeripherals.c // InitPeripherals(); skip this for SCI tests // Step 5. User specific functions, Reassign vectors (optional), Enable Interrupts: LoopCount = 0; ErrorCount = 0; // scia_fifo_init(); // Initialize the SCI FIFO scia_loopback_init(); // Initalize SCI for digital loop back // Note: Autobaud lock is not required for this example // Send a character starting with 0 SendChar = 10; // Step 6. Send Characters forever starting with 0x00 and going through // 0xFF. After sending each, check the recieve buffer for the correct value for(;;) { scia_xmit(SendChar); // SendChar=SciaRegs.SCIRXEMU; // while(SciaRegs.SCIFFRX.bit.RXFFST !=1) { } // wait for RRDY/RXFFST =1 for 1 data available in FIFO // Check received character // ReceivedChar=SciaRegs.SCIRXBUF.all; //scia_xmit(ReceivedChar); // if(ReceivedChar != SendChar) error(); DELAY_US(10000); // Move to the next character and repeat the test SendChar++; // SendChar &= 0x00FF; // Limit the character to 8-bits LoopCount++; } } interrupt void scia_rx_isr(void) { ReceivedChar=SciaRegs.SCIRXBUF.all; PieCtrlRegs.PIEACK.all = PIEACK_GROUP9; } interrupt void scia_tx_isr(void) { } // Step 7. Insert all local Interrupt Service Routines (ISRs) and functions here: void error() { ErrorCount++; // asm(" ESTOP0"); // Uncomment to stop the test here // for (;;); } // Test 1,SCIA DLB, 8-bit word, baud rate 0x000F, default, 1 STOP bit, no parity void scia_loopback_init() { // Note: Clocks were turned on to the SCIA peripheral // in the InitSysCtrl() function SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback // No parity,8 char bits, // async mode, idle-line protocol SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK, // Disable RX ERR, SLEEP, TXWAKE SciaRegs.SCICTL2.all =0x0003; SciaRegs.SCICTL2.bit.TXINTENA =1; SciaRegs.SCICTL2.bit.RXBKINTENA =1; SciaRegs.SCIHBAUD =0x0000; SciaRegs.SCILBAUD =0x1000; // SciaRegs.SCICCR.bit.LOOPBKENA =1; // Enable loop back SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset // EALLOW; // All Zones--------------------------------- // Timing for all zones based on XTIMCLK = SYSCLKOUT // XintfRegs.XINTCNF2.bit.XTIMCLK = 1; // to check system frequency // XCLKOUT is enabled // XintfRegs.XINTCNF2.bit.CLKOFF = 0; // XCLKOUT = XTIMCLK // XintfRegs.XINTCNF2.bit.CLKMODE = 0; // 37.5MHZ // EDIS; } // Transmit a character from the SCI' void scia_xmit(int a) { SciaRegs.SCITXBUF=a; } // Initalize the SCI FIFO void scia_fifo_init() { SciaRegs.SCIFFTX.all=0xE040; //SciaRegs.SCIFFRX.bit.RXFIFORESET = 0; SciaRegs.SCIFFRX.all=0x204f; // SciaRegs.SCIFFRX.bit.RXFFST= 0; SciaRegs.SCIFFCT.all=0x0; } //=========================================================================== // No more. //===========================================================================