/* this linker command file is to be included if user wants to use the DCSM feature on the device * DCSM means Dual Zone Code Security Module. * This linker command file works as an addendum ot the already existing Flash/RAM linker command file * that the project has. * The sections in the *_ZoneSelectBlock.asm source file is linked as per the commands given in the file * NOTE - please note fill=0xFFFF, this helps if users include this file in the project by mistake and * doesn't provide the needed proper *_ZoneSelectBlock.asm sources . * Please refer to the Blinky DCSM example in the controlsuite examples for proper usage of this. * * Once users are confident that they want to program the passwords in OTP, the DSECT section type can be removed. * */ MEMORY { PAGE 0 : /* Program Memory */ /* Z1 OTP. LinkPointers */ DCSM_OTP_Z1_LINKPOINTER : origin = 0x78000, length = 0x00000C /* Z1 OTP. PSWDLOCK/RESERVED */ DCSM_OTP_Z1_PSWDLOCK : origin = 0x78010, length = 0x000004 /* Z1 OTP. CRCLOCK/RESERVED */ DCSM_OTP_Z1_CRCLOCK : origin = 0x78014, length = 0x000004 /* Z1 OTP. RESERVED/BOOTCTRL */ DCSM_OTP_Z1_BOOTCTRL : origin = 0x7801C, length = 0x000004 /* DCSM Z1 Zone Select Contents (!!Movable!!) */ /* Z1 OTP. Z1 password locations / Flash and RAM partitioning */ DCSM_ZSEL_Z1_P0 : origin = 0x78020, length = 0x000010 /* Z2 OTP. LinkPointers */ DCSM_OTP_Z2_LINKPOINTER : origin = 0x78200, length = 0x00000C /* Z2 OTP. GPREG1/GPREG2 */ DCSM_OTP_Z2_GPREG : origin = 0x7820C, length = 0x000004 /* Z2 OTP. PSWDLOCK/RESERVED */ DCSM_OTP_Z2_PSWDLOCK : origin = 0x78210, length = 0x000004 /* Z2 OTP. CRCLOCK/RESERVED */ DCSM_OTP_Z2_CRCLOCK : origin = 0x78214, length = 0x000004 /* Z2 OTP. GPREG3/BOOTCTRL */ /* DCSM_OTP_Z2_BOOTCTRL : origin = 0x7821C, length = 0x000004*/ /* DCSM Z1 Zone Select Contents (!!Movable!!) */ /* Z2 OTP. Z2 password locations / Flash and RAM partitioning */ DCSM_ZSEL_Z2_P0 : origin = 0x78220, length = 0x000010 PAGE 1 : /* Z2 OTP. GPREG3/BOOTCTRL */ DCSM_OTP_Z2_BOOTCTRL : origin = 0x7821C, length = 0x000004 } SECTIONS { dcsm_otp_z1_linkpointer : > DCSM_OTP_Z1_LINKPOINTER PAGE = 0, type = DSECT dcsm_otp_z1_pswdlock : > DCSM_OTP_Z1_PSWDLOCK PAGE = 0, type = DSECT dcsm_otp_z1_crclock : > DCSM_OTP_Z1_CRCLOCK PAGE = 0, type = DSECT dcsm_otp_z1_bootctrl : > DCSM_OTP_Z1_BOOTCTRL PAGE = 0, type = DSECT dcsm_zsel_z1 : > DCSM_ZSEL_Z1_P0 PAGE = 0, type = DSECT dcsm_otp_z2_linkpointer : > DCSM_OTP_Z2_LINKPOINTER PAGE = 0, type = DSECT dcsm_otp_z2_pswdlock : > DCSM_OTP_Z2_PSWDLOCK PAGE = 0, type = DSECT dcsm_otp_z2_crclock : > DCSM_OTP_Z2_CRCLOCK PAGE = 0, type = DSECT dcsm_otp_z2_bootctrl : > DCSM_OTP_Z2_BOOTCTRL PAGE = 1 dcsm_zsel_z2 : > DCSM_ZSEL_Z2_P0 PAGE = 0, type = DSECT } /* //=========================================================================== // End of file. //=========================================================================== */