MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x080000, length = 0x000002 RAMM0 : origin = 0x0000A2, length = 0x00035E RAMD0 : origin = 0x00B000, length = 0x000800 RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ RAMGS15 : origin = 0x01B000, length = 0x000FF8 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ // RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors */ FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */ FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */ FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */ FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */ FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */ FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */ FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */ FLASHN : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */ // FLASHN_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x0000A0 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMD1 : origin = 0x00B800, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x000800 RAMGS0 : origin = 0x00C000, length = 0x001000 RAMGS1 : origin = 0x00D000, length = 0x001000 RAMGS2 : origin = 0x00E000, length = 0x001000 RAMGS3 : origin = 0x00F000, length = 0x001000 RAMGS4 : origin = 0x010000, length = 0x001000 RAMGS5 : origin = 0x011000, length = 0x001000 RAMGS6 : origin = 0x012000, length = 0x001000 RAMGS7 : origin = 0x013000, length = 0x001000 RAMGS8 : origin = 0x014000, length = 0x001000 RAMGS9 : origin = 0x015000, length = 0x001000 RAMGS10 : origin = 0x016000, length = 0x001000 CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400 CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400 GPIOMUX: origin = 0x007C00, length = 0x000180 /* GPIO mux registers */ GPIODAT: origin = 0x007F00, length = 0x000030 /* GPIO data registers */ IpcRegs : origin = 0x00050000, length = 0x000024 /* IPC Registers */ PieVectRegs : origin = 0x00000D00, length = 0x000200 /* PieVect Registers */ PieCtrlRegs : origin = 0x00000CE0, length = 0x000020 /* PieVect Registers */ WdRegs : origin = 0x00007000, length = 0x00003F } SECTIONS { /* Allocate program areas: */ .cinit : > FLASHG PAGE = 0, ALIGN(8) .text : >> FLASHH | FLASHI | FLASHJ | FLASHK PAGE = 0, ALIGN(8) // .text : >> FLASHC | FLASHD | FLASHE | FLASHF | FLASHG PAGE = 0, ALIGN(8) codestart : > BEGIN PAGE = 0, ALIGN(8) /* Allocate uninitalized data sections: */ .stack : > RAMM1 PAGE = 1 /* Initalized sections go in Flash */ .switch : > FLASHN PAGE = 0, ALIGN(8) .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ #if defined(__TI_EABI__) .init_array : > FLASHN, PAGE = 0, ALIGN(8) .bss : >> RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4 | RAMD0 PAGE = 0 .bss:output : > RAMLS3, PAGE = 0 .bss:cio : > RAMLS5, PAGE = 1 .data : > RAMLS5, PAGE = 1 .sysmem : > RAMLS5, PAGE = 1 /* Initalized sections go in Flash */ .const : > FLASHG, PAGE = 0, ALIGN(8) #else .pinit : > FLASHN, PAGE = 0, ALIGN(8) .ebss : >> RAMLS5 | RAMGS3 | RAMGS4, PAGE = 1 .esysmem : > RAMLS5, PAGE = 1 .cio : > RAMLS5, PAGE = 1 /* Initalized sections go in Flash */ .econst : >> FLASHG PAGE = 0, ALIGN(8) #endif /*SHARERAMGS0 : > RAMGS0, PAGE = 1 SHARERAMGS1 : > RAMGS1, PAGE = 1 SHARERAMGS2 : > RAMGS2, PAGE = 1*/ #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 #if defined(__TI_EABI__) .TI.ramfunc : {} LOAD = FLASHG, RUN = RAMLS0, LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), PAGE = 0, ALIGN(8) #else .TI.ramfunc : {} LOAD = FLASHG, RUN = RAMLS0, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(8) #endif #else ramfuncs : LOAD = FLASHG, RUN = RAMLS0, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(8) #endif #endif /* The following section definitions are required when using the IPC API Drivers */ GROUP : > CPU2TOCPU1RAM, PAGE = 1 { PUTBUFFER PUTWRITEIDX GETREADIDX } GROUP : > CPU1TOCPU2RAM, PAGE = 1 { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT } GpioMuxRegsFile: load = GPIOMUX PAGE = 1 GpioDataRegsFile: load = GPIODAT PAGE = 1 IpcRegsFile: load = IpcRegs PAGE = 1 PieVectRegsFile: load = PieVectRegs PAGE = 1 PieCtrlRegsFile: load = PieCtrlRegs PAGE = 1 SHARERAMGS0: load = RAMGS0 PAGE = 1 SHARERAMGS1: load = RAMGS1 PAGE = 1 SHARERAMGS2: load = RAMGS2 PAGE = 1 WdRegsFile: load = WdRegs PAGE = 1 } /* //=========================================================================== // End of file. //=========================================================================== */