#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File #include "DSP2833x_Examples.h" // DSP2833x Examples Include File // Prototype statements for functions found within this file. interrupt void cpu_timer0_isr(void); void main(void) { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the DSP2833x_SysCtrl.c file. InitSysCtrl(); // Step 2. Initalize GPIO: // This example function is found in the DSP2833x_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // Skipped for this example // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the DSP2833x_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in DSP2833x_DefaultIsr.c. // This function is found in DSP2833x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.TINT0 = &cpu_timer0_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize the Device Peripheral. This function can be // found in DSP2833x_CpuTimers.c InitCpuTimers(); // For this example, only initialize the Cpu Timers #if (CPU_FRQ_150MHZ) // Configure CPU-Timer 0 to interrupt every 500 milliseconds: // 150MHz CPU Freq, 50 millisecond Period (in uSeconds) ConfigCpuTimer(&CpuTimer0, 150, 500000); #endif #if (CPU_FRQ_100MHZ) // Configure CPU-Timer 0 to interrupt every 500 milliseconds: // 100MHz CPU Freq, 50 millisecond Period (in uSeconds) ConfigCpuTimer(&CpuTimer0, 100, 500000); #endif // To ensure precise timing, use write-only instructions to write to the entire register. Therefore, if any // of the configuration bits are changed in ConfigCpuTimer and InitCpuTimers (in DSP2833x_CpuTimers.h), the // below settings must also be updated. CpuTimer0Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0 // Step 5. User specific code, enable interrupts: // Configure GPIO32 as a GPIO output pin EALLOW; GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 0; GpioCtrlRegs.GPBDIR.bit.GPIO32 = 1; EDIS; // Enable CPU INT1 which is connected to CPU-Timer 0: IER |= M_INT1; // Enable TINT0 in the PIE: Group 1 interrupt 7 PieCtrlRegs.PIEIER1.bit.INTx7 = 1; // Enable global Interrupts and higher priority real-time debug events: EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM // Step 6. IDLE loop. Just sit and loop forever (optional): for(;;); } interrupt void cpu_timer0_isr(void) { CpuTimer0.InterruptCount++; GpioDataRegs.GPBTOGGLE.bit.GPIO32 = 1; // Toggle GPIO32 once per 500 milliseconds // Acknowledge this interrupt to receive more interrupts from group 1 PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; }