Help for Command line programmers --------------------------------- Programmers are named by device or function. Example: Prog20zx is a programmer for products starting with BQ20Z Prog30z5 is a programmer for products starting with BQ30Z5 ProgBQFS is a programmer that can program any BQFS file (I2C or HDQ based) Prog2754X is a programmer for all products starting with BQ2754 and bq34Z. It also programs other flash based products in BQ27XXX family. Examples are BQ27541, BQ27542, BQ27545, BQ27546, BQ27500, BQ27501, BQ27510, BQ27520, BQ34Z100, BQ34100 Prog78350 is a programmer for BQ78350 family of products Usage: Prog20zx.exe -i -p SrecFilename -m0 -i for I2C and SMB, defaults to HDQ if not specified -p enables pullups on MKS-SAI-001. Pullups are required for communication -m0 is for channel 0 or use any available MKS-SAI-001. Additional software required to enable channel number mapping. EXE can be run in parallel from different command console to program 2 or more targets at the same time. Programming times vary from 5 seconds to 1 minute. ---------------------------------