static void switch_active_program_to_pflash01(void) { //------------------------------------------------------------------------------------ // assumed entry state: program being executed is stored in pflash blocks 2 and 3 // backup copy is in blocks 0 and 1 // UPON ENTRY // block 0: address = 0x10000 // MFBALR1: 0x0060 MFBAHR1: 0x10000 // block 1: address = 0x18000 // MFBALR17: 0x8060 MFBAHR17: 0x10000 // block 2: address = 0x00000 // MFBALR18: 0x0060 MFBAHR18: 0x00000 // block 3: address = 0x08000 // MFBALR19: 0x8060 MFBAHR19: 0x00000 //------------------------------------------------------------------------------------ // temporarily set size of blocks 2 and 3 to 0kB by setting MFBALRx.BLOCK_SIZE = 0 (x = 18,19) // setting MFBALRx.BLOCK_SIZE = 0 disables these blocks // this is necessary as you cannot map two blocks to the same address // doing so will result in a data abort exception DecRegs.MFBALR18.all = 0x0000; // block 2, size = 0 KBytes DecRegs.MFBALR19.all = 0x8000; // block 3, size = 0 KBytes DecRegs.MFBAHR1.all = 0x0000; // map block 0 to address 0x00000 (MFBAHL1 = 0x0060) DecRegs.MFBAHR17.all = 0x0000; // map block 1 to address 0x08000 (MFBAHL17 = 0x8060) DecRegs.MFBAHR18.all = 0x0001; // map block 2 to address 0x10000 (MFBAHL18 = 0x0000) DecRegs.MFBAHR19.all = 0x0001; // map block 3 to address 0x18000 (MFBAHL19 = 0x8000) DecRegs.MFBALR18.all = 0x0060; // block 2, size = 32Kbytes DecRegs.MFBALR19.all = 0x8060; // block 3, size = 32Kbytes } static void switch_active_program_to_pflash23(void) { //------------------------------------------------------------------------------------ // assumed entry state: program being executed is stored in pflash blocks 0 and 1 // backup copy is in blocks 2 and 3 // UPON ENTRY // block 0: address = 0x00000 // MFBALR1: 0x0060 MFBAHR1: 0x0000 // block 1: address = 0x08000 // MFBALR17: 0x8060 MFBAHR17: 0x0000 // block 2: address = 0x10000 // MFBALR18: 0x0060 MFBAHR18: 0x1000 // block 3: address = 0x18000 // MFBALR19: 0x0080 MFBAHR19: 0x1000 //------------------------------------------------------------------------------------ // temporarily set size of blocks 0 and 1 to 0kB by setting MFBALRx.BLOCK_SIZE = 0 (x = 1, 17) // setting MFBALRx.BLOCK_SIZE = 0 disables these blocks // this is necessary as you cannot map two blocks to the same address // doing so will result in a data abort exception DecRegs.MFBALR1.all = 0x0000; // block 0, size = 0 KBytes DecRegs.MFBALR17.all = 0x8000; // block 1, size = 0 KBytes DecRegs.MFBAHR18.all = 0x0000; // map block 2 to address 0x00000 (MFBAHL18 = 0x0060) DecRegs.MFBAHR19.all = 0x0000; // map block 3 to address 0x08000 (MFBAHL19 = 0x8060) DecRegs.MFBAHR1.all = 0x0001; // map block 0 to address 0x10000 (MFBAHL1 = 0x0000) DecRegs.MFBAHR17.all = 0x0001; // map block 1 to address 0x18000 (MFBAHL17 = 0x8000) DecRegs.MFBALR1.all = 0x0060; // block 0, size = 32Kbytes DecRegs.MFBALR17.all = 0x8060; // block 1, size = 32Kbytes }