// Calculate and store the CRC of data from 0x00 to 0xFF crcInitial(); // When CAN is not used, the read offset is always 0. When CAN is used, it depends on the number of transmitted bytes. if(CAN_USED == FALSE) { read_offset = 0; } // Unlock device clearLockAll(BROADCAST); // Clear POR, FAULT for device setClr(BROADCAST, CLRFAULT | CLRPOR); // Check if ACKEN is set for(dev_idx = 0; dev_idx < DEVICE_CNT; dev_idx++) { FlexRead(device_address[dev_idx], FLEXWIRE0, DATA_LENGTH__1, TRUE); if(ledRcvBuffer[read_offset] & ACKEN_1) { ackEnabled[device_address[dev_idx]] = TRUE; } else { ackEnabled[device_address[dev_idx]] = FALSE; } } // ***Disable all channels for device - this is reset value of register, but ensure for restart of program disableAllCh(BROADCAST); // Set PWMFREQ = 2000Hz // Can set PWM frequency as broadcast which will overwrite all other settings in same register setPWMfreq(BROADCAST, PWMFREQ__2K0); // Need to set REFRANGE per device to retain existing setting - PWM frequency and REFRANGE are for TPS92912x in the same register // Set REFRANGE = 512 for(dev_idx = 0; dev_idx < DEVICE_CNT; dev_idx++) { setRefRange(device_address[dev_idx], REFRANGE__512); } //***Set DC for all Channels - actually this is the reset value in EEPROM regValue[0] = IOUT__MAX; setIOUTAllCh(BROADCAST, ®Value[0], TRUE); //***Set PWMOUT for all Channels - PWM high is reset value in EEPROM and PWM low is reset from register regValue[0] = PWM__1; setPWMAllCh(BROADCAST, ®Value[0], TRUE); setPWMhighAllCh(BROADCAST, ®Value[0], TRUE); // Set Single-LED-Short threshold and Low Supply Threshold - Settings are for EVMs setSLSth(BROADCAST, SLSTH0__2V50, 0); setSLSth(BROADCAST, SLSTH1__2V50, 1); // Need to set SLSEN and LowSupplyTh per device to retain existing setting - REFRANGE is for TPS929160/240 in the same register for(dev_idx = 0; dev_idx < DEVICE_CNT; dev_idx++) { setLowSupplyTh(device_address[dev_idx], LOWSUPTH__4V); enableSLS(device_address[dev_idx]); } // Clear FAULT for device because low supply threshold was just set setClr(BROADCAST, CLRFAULT); // Enable diagnostics for all channels - actually this is the reset value in EEPROM enableDiagAllCh(BROADCAST); //Assign LED Drivers to the correct LED according to the model and color of the LEDs if(model == MODEL_REAR) { blinker_dev_idx = LED_DRIVER_1_IDX; otherFunc_dev_idx = LED_DRIVER_2_IDX; blinker_limit = BLINKER_NLED_REAR-1; } else //if MODEL_HEAD { blinker_dev_idx = LED_DRIVER_2_IDX; otherFunc_dev_idx = LED_DRIVER_1_IDX; blinker_limit = BLINKER_NLED_HEAD-1; } //Turn off all LEDs enableAllCh(device_address[blinker_dev_idx]); for(ch_idx = 15; ch_idx >= 0; ch_idx--) { regValue[0] = PWM__0; setPWMoneCh(device_address[blinker_dev_idx], regValue, device_LED_idx[ch_idx]); } //Enabling one LED only regValue[0] = PWM__1; setPWMoneCh(device_address[blinker_dev_idx], regValue, 8);