The Register Settings that i have followed for the bellow required conditions; input values to the charger:15V/2.4A; expecting output settings :14.3V/1.5A; battery settings 3S battery/with BQ76920; prochot pin is left unused,this is to charge only battery without system... 1:ChargeOption0() 0x020E; 2:ChargeCurrent() 0x0600; 3:MaxChargeVoltage() 0X3800; 4:ChargeOption1() 0X0210; 5:ChargeOption2() 0X02B7; 6:ChargeOption3() 0X0000; 7:ProchotOption0() 0X4A54; 8:ProchotOption1() 0X8120; 9:ADCOption() 0X00FF; 10:OTGVoltage() 0X0000; 11:OTGCurrent() 0X0000; 12:InputVoltage() 0x3C00; 13:MinSystemVoltage() 0X2400; 14:IIN_HOST() 0X3000;