''' Validation : AFE79xx Library Version v1.67, v1.74 Case RX TX FB CLK Notes ---- ----------------- ----------------- ----------------- ----------- ------------ 1 245.76Msps, 24410 491.52Msps, 44210 491.52Msps, 22210 FADC=2949.12M DAC in interleaved mode SerDes=9830.4Mbps SerDes=9830.4Mbps SerDes=9830.4Mbps FDAC=8847.36M PLL0, NCO=3500M PLL0, NCO=3500M NCO=3500M REF=491.52M 2 245.76Msps, 24410 491.52Msps, 44210 491.52Msps, 22210 FADC=2949.12M DAC in straight mode SerDes=9830.4Mbps SerDes=9830.4Mbps SerDes=9830.4Mbps FDAC=8847.36cM PLL0, NCO=3500M PLL0, NCO=3500M NCO=3500M REF=491.52M ''' setupParams.skipFpga = 1 sysParams = AFE.systemParams setupParams.fpgaRefClk = 184.32 AFE.systemStatus.loadTrims = 1 sysParams.fbEnable = [False]*2 sysParams.FRef = 491.52 sysParams.FadcRx = 2949.12 sysParams.FadcFb = 2949.12 sysParams.Fdac = 2949.12*3 sysParams.enableDacInterleavedMode = False #DAC interleave mode to save power consumption. Fs/2 - Fin spur occurs sysParams.modeTdd = 0 # 0- Single TDD Pin for all Channels # 1- Separate Control for 2T/2R/1F # 2- Separate Control for 1T/1R/1F sysParams.topLevelSystemMode = 'StaticTDDMode' sysParams.RRFMode = 0 #4T4R2F FDD mode sysParams.jesdSystemMode = [3,3] #SystemMode 0: 2R1F-FDD ; rx1-rx2-fb-fb #SystemMode 1: 1R1F-FDD ; rx1-rx1-fb-fb #SystemMode 2: 2R-FDD ; rx1-rx1-rx2-rx2 #SystemMode 3: 1R ; rx1-rx1-rx1-rx1 #SystemMode 4: 1F ; fb-fb-fb-fb #SystemMode 5: 1R1F-TDD ; rx1/fb-rx1/fb-rx1/fb-rx1/fb #SystemMode 8: 1R1F-TDD 1R-FDD (FB-2Lanes)(RX1 RX2 interchanged) ; rx2/fb-rx2/fb-rx1-rx1 sysParams.jesdLoopbackEn = 0 #Make it 1 to Enable the JESDTX to JESDRX internal loopback sysParams.LMFSHdRx =['44210', '44210', '44210', '44210'] # The 2nd and 4th are valid only for jesdSystemMode values in (2,6,7,8). For other modes, select 4 converter modes for 1st and 3rd. sysParams.LMFSHdFb = ["22210","22210"] sysParams.LMFSHdTx = ["44210","44210","44210","44210"] sysParams.jesdTxProtocol = [2,2] #64b/66b sysParams.jesdRxProtocol = [2,2] #64b/66b sysParams.serdesFirmware = True # If you want to lead any firmware, please speify the path here. Otherwise it will not write any firmware sysParams.jesdTxLaneMux = [0,1,2,3,4,5,6,7] # Enter which lanes you want in each location. # Note that across 2T Mux is not possible in 0.5. # For example, if you want to exchange the first two lines of each 2T, this should be [[1,0,2,3],[5,4,6,7]] sysParams.jesdRxLaneMux = [0,1,2,3,4,5,6,7] # Enter which lanes you want in each location. # Note that across 2R Mux is not possible in 0.5. # For example, if you want to exchange the first two lines of each 2R, this should be [[1,0,2,3],[5,4,6,7]] sysParams.jesdRxRbd = [4, 4] # scrambler is disabled sysParams.rxJesdTxScr = [False]*4 sysParams.fbJesdTxScr = [False]*2 sysParams.jesdRxScr = [False]*4 sysParams.rxJesdTxK = [1,1,1,1] sysParams.fbJesdTxK = [1,1] sysParams.jesdRxK = [1,1,1,1] sysParams.ncoFreqMode = "1KHz" sysParams.txNco0 = [[5000,5000], #Band0, Band1 for TxA for NCO0 [6000,6000], #Band0, Band1 for TxB for NCO0 [7000,7000], #Band0, Band1 for TxC for NCO0 [5400,5400]] #Band0, Band1 for TxD for NCO0 sysParams.rxNco0 = [[5000,5000], #Band0, Band1 for RxA for NCO0 [6000,6000], #Band0, Band1 for RxB for NCO0 [7000,7000], #Band0, Band1 for RxC for NCO0 [5400,5400]] #Band0, Band1 for RxD for NCO0 sysParams.fbNco0 = [1500,1800] #FBA, FBC for NCO0 sysParams.numBandsRx = [0]*4 # 0 for single, 1 for dual sysParams.numBandsFb = [0,0] sysParams.numBandsTx = [0,0,0,0] sysParams.ddcFactorRx = [4]*4 # DDC decimation factor for RX A, B, C and D sysParams.ddcFactorFb = [4]*2 sysParams.ducFactorTx = [12]*4 AFE.systemStatus.loadTrims =1 ## The following parameters sets up the LMK04828 clocking schemes lmkParams.pllEn = True#False lmkParams.inputClk = 1474.56#737.28 lmkParams.lmkFrefClk = True ## The following parameters sets up the SYNCIN and SYNCOUT to interface with the TSW14J57 sysParams.jesdABLvdsSync = 1 sysParams.jesdCDLvdsSync = 1 sysParams.rxJesdTxSyncMux = [0,0,0,0] sysParams.fbJesdTxSyncMux = [0,0] sysParams.jesdRxSyncMux = [0,0,0,0] #[0,0,1,1] sysParams.syncLoopBack = True # ## The following parameters sets up the AGC # sysParams.agcParams[0].agcMode = 1 ##internal AGC # sysParams.agcParams[0].gpioRstEnable = 0 ##disable GPIO based reset to AGC detector # sysParams.agcParams[0].atken = [0, 1, 0] ##enable big and small step attack # sysParams.agcParams[0].decayen = [0,1,0] ##enable big and small step decay # sysParams.agcParams[0].atksize = [2,1,0] ## bigs step = 2dB, small step = 1dB # sysParams.agcParams[0].decaysize = [2,1,0] ##big step = 2dB, small step = 1dB # sysParams.agcParams[0].atkthreshold = [-1, -2, -14] ##attack threshold # sysParams.agcParams[0].decaythreshold = [-14, -6, -20] ##decay threshold # sysParams.agcParams[0].atkwinlength = [170, 170] ## detector time constant expressed inn absolute time in ns. # sysParams.agcParams[0].decaywinlength = 87380 ##detector time constant expressed in absolute time in ns. All detectors use the same value for decay time constant # sysParams.agcParams[0].atkNumHitsAbs = [8,8] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock # sysParams.agcParams[0].decayNumHitsAbs = [100,100] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock # sysParams.agcParams[0].minDsaAttn = 0 ##minimum DSA attenuation used by AGC # sysParams.agcParams[0].maxDsaAttn = 22 ##maximum DSA attenuation used by AGC # sysParams.agcParams[0].totalGainRange = 22 ##total gain range used by ALC for gain compensation # sysParams.agcParams[0].minAttnAlc = 0 ##minimum attenuation used by ALC for compensation when useMinAttnAgc = 0 # sysParams.agcParams[0].useMinAttnAgc = 1 ##enable ALC to use minimum attenuation from AGC for which compensation is required. # sysParams.agcParams[0].alcEn = 1 # sysParams.agcParams[0].alcMode = 0 ##floating point DGC # sysParams.agcParams[0].fltPtMode = 0 ##if exponent > 0, dont send MSB # sysParams.agcParams[0].fltPtFmt = 1 ##3 bit exponent ## The following parameters sets up the GPIOs sysParams.gpioMapping={ 'H8': 'ADC_SYNC0', 'H7': 'ADC_SYNC1', 'N8': 'ADC_SYNC2', 'N7': 'ADC_SYNC3', 'H9': 'DAC_SYNC0', 'G9': 'DAC_SYNC1', 'N9': 'DAC_SYNC2', 'P9': 'DAC_SYNC3', 'P14': 'GLOBAL_PDN', 'K14': 'FBABTDD', 'R6': 'FBCDTDD', 'H15': ['TXATDD','TXBTDD'], 'V5': ['TXCTDD','TXDTDD'], 'E7': ['RXATDD','RXBTDD'], 'R15': ['RXCTDD','RXDTDD']} #AFE.systemParams.papParams[0]['enable'] = True #AFE.systemParams.papParams[1]['enable'] = True #AFE.systemParams.papParams[2]['enable'] = True #AFE.systemParams.papParams[3]['enable'] = True lmklogDumpInst=mLogDump.logDump(ASTERIX_DIR+DEVICES_DIR+r"\LMK.txt") lmklogDumpInst.logFormat=0x01 lmk.logClassInst = lmklogDumpInst lmk.rawWriteLogEn=1 #logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"AFE79xxConfig_LMK.txt") #logDumpInst.logFormat = 0x01 lmklogDumpInst.rewriteFile = 1 lmklogDumpInst.ignoreLogComments=1 #lmklogDumpInst.enableReads=False ## SPI reads are not logged #lmklogDumpInst.enableReadCheck=False ## Initiates LMK04828 and AFE79xx Bring-up setupParams.skipLmk = False AFE.initializeConfig() lmkParams.sysrefFreq = AFE.systemStatus.sysrefFreq AFE.LMK.lmkConfig()