root@am57xx-evm:/usr/share/ti/dlp-sdk# ./DLP_LIGHTCRAFTER Connecting to projector... Configuring projector... Connecting to camera... Configuring camera... Texas Instruments DLP Commandline 3D Scanner 0: Exit 1: Generate camera calibration board and enter feature measurements 2: Prepare DLP LightCrafter 4500 (once per projector) 3: Prepare system for calibration and scanning 4: Calibrate camera 5: Calibrate system 6: Perform scan (vertical patterns only) 7: Perform scan (horizontal patterns only) 8: Perform scan (vertical and horizontal patterns) 9: Reconnect camera and projector Select menu item: 4 <<<<<<<<<<<<<<<<<<<<<< Calibrating the Camera >>>>>>>>>>>>>>>>>>>>>> Loading camera calibration settings... Setting up camera calibration Projecting white pattern to illuminate calibration board Calibrating camera... Calibration boards required = 20 Calibration boards captured = 0 Read the following instructions in their entirety! Press ENTER when ready to read the instructions... Camera calibration instructions: 1. After the live view has started, place the calibration board so it is completely visible within the camera frame and is stationary - The board should be placed at the desired scanning distance 2. Adjust the camera's aperture and focus until the image is well illuminated and sharp - Lock the aperture and focus in place if possible - If the camera focus or aperture is adjusted, the calibration must be redone 3. Select the live view window and press the SPACE_BAR key to capture the calibration board's current position 4. Move the calibration board and repeat step 3 until calibration is complete - Capture images with the board at different distances from the camera - Capture images with the board at different positions in the camera frame - The position of the camera can be changed as well rather than moving the board NOTE: Press ESC key to quit the calibration routine Press ENTER after reading the above instructions... [ 736.513810] usb 1-1.4: usbfs: process 1209 (DLP_LIGHTCRAFTE) did not claim interface 0 before use Started camera. No such plugin for spec "Auto" init done Using Wayland-EGL wlpvr: PVR Services Initialised