AM1810 initialization passed! Booting TI User Boot Loader UBL Version: 1.65 UBL Flashtype: SPI Starting SPI Memory Copy... Valid magicnum, 0x55424CBB, found at offset 0x00010000. DONE Jumping to entry point at 0xC1080000. U-Boot 2009.11 (Apr 18 2011 - 14:24:01) I2C: ready DRAM: 64 MB MMC: davinci: 0 *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial ARM Clock : 300000000 Hz DDR Clock : 150000000 Hz Error - unable to probe SPI flash. Net: Ethernet PHY: GENERIC @ 0x00 Hit any key to stop autoboot: 0 reading boot.scr ** Unable to read "boot.scr" from mmc 0:1 ** reading uImage 2109660 bytes read ## Booting kernel from Legacy Image at c0700000 ... Image Name: Arago/2.6.32+2.6.33-rt29-psp03.3 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2109596 Bytes = 2 MB Load Address: c0008000 Entry Point: c0008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Linux version 2.6.33.7-rt29 (schuyler_2@neo) (gcc version 4.3.3 (Sourcery G++ Li te 2009q1-203) ) #1 PREEMPT RT Tue Jan 11 21:00:48 CST 2011 CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177 CPU: VIVT data cache, VIVT instruction cache Machine: DaVinci DA850/OMAP-L138/AM18xx EVM Memory policy: ECC disabled, Data cache writeback DaVinci da850/omap-l138/am18xx variant 0x1 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128 Kernel command line: mem=32M console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw rootw ait ip=off PID hash table entries: 128 (order: -3, 512 bytes) Dentry cache hash table entries: 4096 (order: 2, 16384 bytes) Inode-cache hash table entries: 2048 (order: 1, 8192 bytes) Memory: 32MB = 32MB total Memory: 28068KB available (3892K code, 338K data, 148K init, 0K highmem) Real-Time Preemption Support (C) 2004-2007 Ingo Molnar Experimental preemptable hierarchical RCU implementation. NR_IRQS:245 Console: colour dummy device 80x30 Calibrating delay loop... 149.50 BogoMIPS (lpj=747520) Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok DaVinci: 144 gpio irqs regulator: core version 0.5 NET: Registered protocol family 16 bio: create slab at 0 SCSI subsystem initialized usbcore: registered new interface driver usbfs usbcore: registered new interface driver hub usbcore: registered new device driver usb regulator: VDCDC1: 3200 <--> 3300 mV at 3300 mV regulator: VDCDC2: 1750 <--> 3300 mV at 3300 mV regulator: VDCDC3: 950 <--> 1375 mV at 1200 mV regulator: LDO1: 1800 mV regulator: LDO2: 1150 <--> 1300 mV at 1200 mV pca953x 1-0020: failed reading register i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL) Advanced Linux Sound Architecture Driver Version 1.0.21. Switching to clocksource timer0_1 musb_hdrc: version 6.0, cppi4.1-dma, host, debug=0 Waiting for USB PHY clock good... musb_hdrc: USB Host mode controller at fee00000 using DMA, IRQ 58 musb_hdrc musb_hdrc: MUSB HDRC host driver musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1 hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected NET: Registered protocol family 2 IP route cache hash table entries: 1024 (order: 0, 4096 bytes) TCP established hash table entries: 1024 (order: 1, 8192 bytes) TCP bind hash table entries: 1024 (order: 2, 28672 bytes) TCP: Hash tables configured (established 1024 bind 1024) TCP reno registered UDP hash table entries: 64 (order: 0, 4096 bytes) UDP-Lite hash table entries: 64 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. EMAC: MII PHY configured, RMII PHY will not be functional JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc. msgmni has been set to 54 io scheduler noop registered (default) da8xx_lcdc da8xx_lcdc.0: GLCD: Found Sharp_LK043T1DG01 panel Console: switching to colour frame buffer device 60x34 Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A console [ttyS2] enabled brd: module loaded at24 1-0050: 32768 byte 24c256 EEPROM (writable) Read MAC addr from EEPROM: 00:0e:99:03:70:45 ahci ahci: forcing PORTS_IMPL to 0x1 ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl SATA mode ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc scsi0 : ahci ata1: SATA max UDMA/133 irq 67 spi_davinci spi_davinci.1: DaVinci SPI driver in EDMA mode Using RX channel = 18 , TX channel = 19 and event queue = 1 m25p80 spi1.0: non-JEDEC variant of m25p64 m25p80 spi1.0: m25p64 (8192 Kbytes) Creating 4 MTD partitions on "m25p80": 0x000000000000-0x000000040000 : "U-Boot" 0x000000040000-0x000000050000 : "U-Boot Environment" 0x000000050000-0x0000007f0000 : "Linux" 0x0000007f0000-0x000000800000 : "MAC Address" Read MAC addr from EEPROM: ff:ff:ff:ff:ff:ff spi_davinci spi_davinci.1: Controller at 0xfef0e000 console [netcon0] enabled netconsole: network logging started Initializing USB Mass Storage driver... usbcore: registered new interface driver usb-storage USB Mass Storage support registered. input: TPS6507x Touchscreen as /devices/platform/i2c-gpio.1/i2c-1/1-0048/input/i nput0 omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 omap_rtc: RTC power up reset detected omap_rtc: already running i2c /dev entries driver Linux video capture interface: v2.00 usbcore: registered new interface driver uvcvideo USB Video Class driver (v0.1.0) watchdog watchdog: heartbeat 60 sec cpuidle: using governor ladder cpuidle: using governor menu davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode usbcore: registered new interface driver usbhid usbhid: USB HID core driver usbcore: registered new interface driver snd-usb-audio No device for DAI tlv320aic3x asoc: tlv320aic3x <-> davinci-i2s mapping ok mmc0: new SDHC card at address e624 mmcblk0: mmc0:e624 SD08G 7.40 GiB mmcblk0: ALSA device list: #0: DA850/OMAP-L138 EVM (tlv320aic3x) TCP cubic registered NET: Registered protocol family 17 Clocks: disable unused i2c1 Clocks: disable unused emac Clocks: disable unused aemif Clocks: disable unused spi0 Clocks: disable unused mcbsp0 Clocks: disable unused mcbsp1 Clocks: disable unused vpif Clocks: disable unused ecap0 p1 ata1: SATA link down (SStatus 0 SControl 300) p2 p3 regulator_init_complete: incomplete constraints, leaving LDO2 on regulator_init_complete: incomplete constraints, leaving LDO1 on regulator_init_complete: incomplete constraints, leaving VDCDC3 on regulator_init_complete: incomplete constraints, leaving VDCDC2 on regulator_init_complete: incomplete constraints, leaving VDCDC1 on davinci_emac_probe: using random MAC addr: 46:72:81:13:db:19 emac-mii: probed omap_rtc omap_rtc: setting system clock to 2011-01-25 15:00:19 UTC (1295967619) EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is rec ommended kjournald starting. Commit interval 5 seconds EXT3-fs (mmcblk0p2): using internal journal EXT3-fs (mmcblk0p2): recovery complete EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode VFS: Mounted root (ext3 filesystem) on device 179:2. Freeing init memory: 148K INIT: version 2.86 booting Please wait: booting... Starting udev EXT3-fs (mmcblk0p3): warning: maximal mount count reached, running e2fsck is rec ommended kjournald starting. Commit interval 5 seconds EXT3-fs (mmcblk0p3): using internal journal EXT3-fs (mmcblk0p3): recovery complete EXT3-fs (mmcblk0p3): mounted filesystem with writeback data mode Remounting root file system... Caching udev devnodes Populating dev cache NET: Registered protocol family 10 logger: mount: mount point /proc/bus/usb does not exist ALSA: Restoring mixer settings... No state is present for card EVM Unknown hardware: "tlv320aic3x" "" "" "" "" Hardware is initialized using a guess method No state is present for card EVM Configuring network interfaces... eth0: attached PHY driver [SMSC LAN8710/LAN872 0] (mii_bus:phy_addr=1:00, id=7c0f1) ADDRCONF(NETDEV_UP): eth0: link is not ready udhcpc (v1.13.2) started Sending discover... PHY: 1:00 - Link is Up - 100/Full ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready Sending discover... Sending discover... No lease, forking to background done. Setting up IP spoofing protection: rp_filter. INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Dropbear SSH server: dropbear. Starting telnet daemon. Starting syslogd/klogd: done Starting thttpd. Starting Matrix GUI application.