MMC: davinci: 0 SF: Detected SST25VF080B with page size 4096, total 1 MiB In: serial Out: serial Err: serial ARM Clock : 300000000 Hz DDR Clock : 150000000 Hz Net: Ethernet PHY: GENERIC @ 0x00 DaVinci-EMAC Hit any key to stop autoboot: 0 NAND read: device 0 offset 0x20000, size 0x200000 Bad block table found at page 65472, version 0x01 Bad block table found at page 65408, version 0x01 2097152 bytes read: OK ## Booting kernel from Legacy Image at c0700000 ... Image Name: Linux-2.6.37 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2002280 Bytes = 1.9 MiB Load Address: c0008000 Entry Point: c0008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Linux version 2.6.37 (root@erl) (gcc version 4.5.3 20110311 (prerelease) (GCC) 2 CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177 CPU: VIVT data cache, VIVT instruction cache Machine: DaVinci DA850/OMAP-L138/AM18x EVM Memory policy: ECC disabled, Data cache writeback DaVinci da850/omap-l138/am18x variant 0x1 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 8128 Kernel command line: mem=32M console=ttyS2,115200n8 root=/dev/mtdblock1 rw rootfstype=jffs2 ip=dhcp PID hash table entries: 128 (order: -3, 512 bytes) Dentry cache hash table entries: 4096 (order: 2, 16384 bytes) Inode-cache hash table entries: 2048 (order: 1, 8192 bytes) Memory: 32MB = 32MB total Memory: 28272k/28272k available, 4496k reserved, 0K highmem Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) DMA : 0xff000000 - 0xffe00000 ( 14 MB) vmalloc : 0xc2800000 - 0xfea00000 ( 962 MB) lowmem : 0xc0000000 - 0xc2000000 ( 32 MB) modules : 0xbf000000 - 0xc0000000 ( 16 MB) .init : 0xc0008000 - 0xc002a000 ( 136 kB) .text : 0xc002a000 - 0xc03dc000 (3784 kB) .data : 0xc03dc000 - 0xc03fdea0 ( 136 kB) SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Preemptable hierarchical RCU implementation. RCU-based detection of stalled CPUs is disabled. Verbose stalled-CPUs detection is disabled. NR_IRQS:245 Console: colour dummy device 80x30 Calibrating delay loop... 149.50 BogoMIPS (lpj=747520) pid_max: default: 32768 minimum: 301 Security Framework initialized Mount-cache hash table entries: 512 CPU: Testing write buffer coherency: ok DaVinci: 144 gpio irqs NET: Registered protocol family 16 da850_evm_init: VGA registration Done: 0 bio: create slab at 0 SCSI subsystem initialized i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL) LinuxPPS API ver. 1 registered Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti Switching to clocksource timer0_1 NET: Registered protocol family 2 IP route cache hash table entries: 1024 (order: 0, 4096 bytes) TCP established hash table entries: 1024 (order: 1, 8192 bytes) TCP bind hash table entries: 1024 (order: 0, 4096 bytes) TCP: Hash tables configured (established 1024 bind 1024) TCP reno registered UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. EMAC: RMII PHY configured, MII PHY will not be functional nfs4filelayout_init: NFSv4 File Layout Driver Registering... JFFS2 version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc. msgmni has been set to 55 io scheduler noop registered io scheduler deadline registered io scheduler cfq registered (default) Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a AR7 serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a AR7 serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a AR7 console [ttyS2] enabled nbd: registered device at major 43 Uniform Multi-Platform E-IDE driver ONFI flash detected NAND device: Manufacturer ID: 0xad, Chip ID: 0xf1 (Hynix ����������������������) Creating 2 MTD partitions on "davinci_nand.1": 0x000000020000-0x000000420000 : "kernel" 0x000000420000-0x000008000000 : "filesystem" davinci_nand davinci_nand.1: controller rev. 2.5 spi_davinci spi_davinci.1: DMA: supported spi_davinci spi_davinci.1: DMA: RX channel: 18, TX channel: 19, event queue: 0 spi_davinci spi_davinci.1: Controller at 0xfef0e000 davinci_mdio davinci_mdio.0: davinci mdio revision 1.5 davinci_mdio davinci_mdio.0: detected phy mask fffffffe davinci_mdio.0: probed davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720 PPP generic driver version 2.4.2 NET: Registered protocol family 24 console [netcon0] enabled netconsole: network logging started omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 omap_rtc: RTC power up reset detected omap_rtc: already running i2c /dev entries driver davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode TCP cubic registered NET: Registered protocol family 17 Registering the dns_resolver key type davinci_emac_probe: using random MAC addr: 72:c5:ce:82:44:cf omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) davinci_mdio davinci_mdio.0: resetting idled controller net eth0: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=0:00, id) Sending DHCP requests .. PHY: 0:00 - Link is Up - 100/Full ., OK IP-Config: Got DHCP answer from 10.1.6.5, my address is 10.1.6.81 IP-Config: Complete: device=eth0, addr=10.1.6.81, mask=255.255.255.0, gw=255.255.255.255, host=10.1.6.81, domain=example.org, nis-domain=(none), bootserver=10.1.6.5, rootserver=10.1.6.5, rootpath= VFS: Mounted root (jffs2 filesystem) on device 31:1. Freeing init memory: 136K INIT: version 2.86 booting Please wait: booting... Error opening /dev/fb0: No such device or address Starting udev udevd (477): /proc/477/oom_adj is deprecated, please use /proc/477/oom_score_ad. udev: starting version 141 Remounting root file system... Caching udev devnodes Populating dev cache logger: mount: mount point /proc/bus/usb does not exist Configuring network interfaces... udhcpc (v1.13.2) started Sending discover... Sending select for 10.1.6.81... Lease of 10.1.6.81 obtained, lease time 600 done. Setting up IP spoofing protection: rp_filter. Tue Jan 25 12:30:00 UTC 2011 INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting OpenBSD Secure Shell server: sshd Privilege separation user sshd does not exist Starting syslogd/klogd: done _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am180x-evm ttyS2 Arago 2010.12 am180x-evm ttyS2 am180x-evm login: root root@am180x-evm:~# touch kalai root@am180x-evm:~# ls -l >x root@am180x-evm:~# ls -l >kalai root@am180x-evm:~# cat kalai -rw-r--r-- 1 root root 508590 Jan 25 12:37 D_message.out -rwxr-xr-x 1 root root 5399 Jan 25 2011 char_lcd_drv.ko -rwxr-xr-x 1 root root 284508 Jan 25 2011 dsplink1.ko -rw-r--r-- 1 root root 0 Jan 25 12:31 kalai -rwxr-xr-x 1 root root 459998 Jan 25 2011 message_D -rw-r--r-- 1 root root 396 Jan 25 12:30 x root@am180x-evm:~#