//------------------------------------------------------------------------------
// \file    test_audio.c
// \brief   implementation of OMAP-L138 audio test.
//
//-----------------------------------------------------------------------------

#include "stdio.h"
#include "types.h"
#include "evmomapl138.h"
#include "evmomapl138_mcasp.h"
#include "evmomapl138_aic3106.h"
#include "test_audio.h"

//-----------------------------------------------------------------------------
// Private Defines and Macros
//-----------------------------------------------------------------------------

//-----------------------------------------------------------------------------
// Static Variable Declarations
//-----------------------------------------------------------------------------

static int16_t sinetable[48] = {
    0x0000, 0x10b4, 0x2120, 0x30fb, 0x3fff, 0x4dea, 0x5a81, 0x658b,
    0x6ed8, 0x763f, 0x7ba1, 0x7ee5, 0x7ffd, 0x7ee5, 0x7ba1, 0x76ef,
    0x6ed8, 0x658b, 0x5a81, 0x4dea, 0x3fff, 0x30fb, 0x2120, 0x10b4,
    0x0000, 0xef4c, 0xdee0, 0xcf06, 0xc002, 0xb216, 0xa57f, 0x9a75,
    0x9128, 0x89c1, 0x845f, 0x811b, 0x8002, 0x811b, 0x845f, 0x89c1,
    0x9128, 0x9a76, 0xa57f, 0xb216, 0xc002, 0xcf06, 0xdee0, 0xef4c
};

//-----------------------------------------------------------------------------
// Private Function Prototypes
//-----------------------------------------------------------------------------
static uint32_t testAudioLineOut(void);
static uint32_t testAudioLineIn(void);
static void shutdownAudio(void);

//-----------------------------------------------------------------------------
// Public Function Definitions
//-----------------------------------------------------------------------------

//-----------------------------------------------------------------------------
// \brief   tests the AIC3106 CODEC
//
// \param   none.
//
// \return  uint32_t
//-----------------------------------------------------------------------------
uint32_t TEST_audio(void)
{
	uint32_t rtn = ERR_NO_ERROR;

   printf("--------------------------------------------------------------------\r\n");
   printf("                     Audio CODEC test\r\n\r\n");
   
   printf("Additional Equipment\r\n");
   printf("--------------------\r\n");
   printf("- 3.5mm pass through cable\r\n\r\n");
   printf("- 3.5mm headphones\r\n\r\n");
   
   printf("Test Description\r\n");
   printf("----------------\r\n");
   printf("The test will begin by playing a 5 second tone though the line\r\n");
   printf("out port. The 3.5mm pass through cable will not be needed for\r\n");
   printf("this portion of the test. After playing the tone, audio from the\n\r");
   printf("line in port will be played through the line out port for 15 seconds.\r\n");
   printf("--------------------------------------------------------------------\r\n\r\n");

	//------------------------------------
	// initialize the required bsl modules
	//------------------------------------
   printf("Initialize the Required BSL Modules\r\n");
   printf("-----------------------------------\r\n\r\n");
   
	rtn = MCASP_init();
	if (rtn != ERR_NO_ERROR)
	{
		printf("error initializing mcasp!\r\n");
		return (rtn);
	}

	rtn = AIC3106_init();
	if (rtn != ERR_NO_ERROR)
	{
		printf("error initializing aic3106!\r\n");
		return (rtn);
	}


	//-----------------------
	// execute line out test.
	//-----------------------
   printf("\r\nExecute Test\r\n");
   printf("------------\r\n\r\n");
	
	printf("--- test audio line out (put on your headphones...) ---\r\n");
	rtn = testAudioLineOut();
   if (rtn != ERR_NO_ERROR)
   {
      printf("\tline out test failed\r\n\r\n");
      return (rtn);
   }
   else
   {
      printf("\tline out test passed\r\n\r\n");
   }

#if 0
	//------------------------------------
	// initialize the required bsl modules
	//------------------------------------
	rtn = MCASP_init();
	if (rtn != ERR_NO_ERROR)
	{
		printf("error initializing mcasp!\r\n");
		return (rtn);
	}

	rtn = AIC3106_init();
	if (rtn != ERR_NO_ERROR)
	{
		printf("error initializing aic3106!\r\n");
		return (rtn);
	}

	//-----------------------
	// execute line in test.
	//-----------------------
	printf("--- test audio line in (put on your headphones and plug in source to line in...) ---\r\n");

	rtn = testAudioLineIn();
   if (rtn != ERR_NO_ERROR)
   {
      printf("\tline in test failed\r\n\r\n");
      return (rtn);
   }
   else
   {
      printf("\tline in test passed\r\n\r\n");
   }

	// kill codec and mcasp.
   shutdownAudio();

#endif 

	return (rtn);
}

//-----------------------------------------------------------------------------
// Private Function Definitions
//-----------------------------------------------------------------------------

uint32_t testAudioLineOut(void)
{
   uint32_t rtn = ERR_NO_ERROR;
   int16_t msec, sec;
   int16_t sample;

   // enable the audio clocks, verifying each bit is properly set.
   SETBIT(MCASP->XGBLCTL, XHCLKRST);
   while (!CHKBIT(MCASP->XGBLCTL, XHCLKRST)) {}
   SETBIT(MCASP->RGBLCTL, RHCLKRST);
   while (!CHKBIT(MCASP->RGBLCTL, RHCLKRST)) {}

   SETBIT(MCASP->XGBLCTL, XCLKRST);
   while (!CHKBIT(MCASP->XGBLCTL, XCLKRST)) {}
   SETBIT(MCASP->RGBLCTL, RCLKRST);
   while (!CHKBIT(MCASP->RGBLCTL, RCLKRST)) {}

   SETBIT(MCASP->XGBLCTL, XSRCLR);
   while (!CHKBIT(MCASP->XGBLCTL, XSRCLR)) {}
   SETBIT(MCASP->RGBLCTL, RSRCLR);
   while (!CHKBIT(MCASP->RGBLCTL, RSRCLR)) {}

   /* Write a 0, so that no underrun occurs after releasing the state machine */
   MCASP->XBUF11 = 0;
   //MCASP->RBUF12 = 0;

   SETBIT(MCASP->XGBLCTL, XSMRST);
   while (!CHKBIT(MCASP->XGBLCTL, XSMRST)) {}
   SETBIT(MCASP->RGBLCTL, RSMRST);
   while (!CHKBIT(MCASP->RGBLCTL, RSMRST)) {}

   SETBIT(MCASP->XGBLCTL, XFRST);
   while (!CHKBIT(MCASP->XGBLCTL, XFRST)) {}
   SETBIT(MCASP->RGBLCTL, RFRST);
   while (!CHKBIT(MCASP->RGBLCTL, RFRST)) {}

   // wait for transmit ready and send a dummy byte.
   while(!CHKBIT(MCASP->SRCTL11, XRDY)) {}
   MCASP->XBUF11 = 0;

   // transmit beep.
   for (sec = 0; sec < 5; sec++)
   {
      for (msec = 0; msec < 1000; msec++)
      {
         for (sample = 0; sample < 48; sample++)
         {
            // wait for xmit ready and send a sample to the left channel.
            while (!CHKBIT(MCASP->SRCTL11, XRDY)) {}
            MCASP->XBUF11 = (sinetable[sample] << 15) | 0x00000000;

            // wait for xmit ready and send a sample to the left channel.
            while (!CHKBIT(MCASP->SRCTL11, XRDY)) {}
            MCASP->XBUF11 = (sinetable[sample] << 15) | 0x00000000;
         }
      }
   }
   return (rtn);
}

uint32_t testAudioLineIn(void)
{
   uint32_t rtn = ERR_NO_ERROR;
   int16_t msec, sec, sample;
   int32_t dat;

   // enable the audio clocks, verifying each bit is properly set.
   SETBIT(MCASP->XGBLCTL, XHCLKRST);
   while (!CHKBIT(MCASP->XGBLCTL, XHCLKRST)) {}
   SETBIT(MCASP->RGBLCTL, RHCLKRST);
   while (!CHKBIT(MCASP->RGBLCTL, RHCLKRST)) {}

   SETBIT(MCASP->XGBLCTL, XCLKRST);
   while (!CHKBIT(MCASP->XGBLCTL, XCLKRST)) {}
   SETBIT(MCASP->RGBLCTL, RCLKRST);
   while (!CHKBIT(MCASP->RGBLCTL, RCLKRST)) {}

   SETBIT(MCASP->XGBLCTL, XSRCLR);
   while (!CHKBIT(MCASP->XGBLCTL, XSRCLR)) {}
   SETBIT(MCASP->RGBLCTL, RSRCLR);
   while (!CHKBIT(MCASP->RGBLCTL, RSRCLR)) {}

   /* Write a 0, so that no underrun occurs after releasing the state machine */
   MCASP->XBUF11 = 0;

   SETBIT(MCASP->XGBLCTL, XSMRST);
   while (!CHKBIT(MCASP->XGBLCTL, XSMRST)) {}
   SETBIT(MCASP->RGBLCTL, RSMRST);
   while (!CHKBIT(MCASP->RGBLCTL, RSMRST)) {}

   SETBIT(MCASP->XGBLCTL, XFRST);
   while (!CHKBIT(MCASP->XGBLCTL, XFRST)) {}
   SETBIT(MCASP->RGBLCTL, RFRST);
   while (!CHKBIT(MCASP->RGBLCTL, RFRST)) {}

   // wait for transmit ready and send a dummy byte.
   while(!CHKBIT(MCASP->SRCTL11, XRDY)) {}
   MCASP->XBUF11 = 0;

   // loop audio
   for (sec = 0; sec < 15; sec++)
   {
      for (msec = 0; msec < 1000; msec++)
      {
         for (sample = 0; sample < 48; sample++)
         {
            // wait for recv ready and send a sample to the left channel.
            while (!CHKBIT(MCASP->SRCTL11, XRDY)) {}
   			MCASP->XBUF11 = dat;
            dat = MCASP->XBUF12;

            // wait for recv ready and send a sample to the right channel.
            while (!CHKBIT(MCASP->SRCTL11, XRDY)) {}
   			MCASP->XBUF11 = dat;
            dat = MCASP->XBUF12;
         }
      }
   }
   return (rtn);
}

void shutdownAudio(void)
{
   // close codec.
   AIC3106_writeRegister(AIC3106_REG_PAGESELECT, 0);
   AIC3106_writeRegister(AIC3106_REG_RESET, 0x80);

   // close mcasp.
   MCASP->SRCTL0 = 0;
   MCASP->SRCTL1 = 0;
   MCASP->SRCTL2 = 0;
   MCASP->SRCTL3 = 0;
   MCASP->SRCTL5 = 0;
   MCASP->SRCTL11 = 0;
   MCASP->SRCTL12 = 0;
   MCASP->GBLCTL = 0;
}