U-Boot 2014.10 (Sep 01 2015 - 11:52:28) Watchdog enabled I2C: ready DRAM: 512 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Using default environment Board name=NTXLF101 Board rev=revA Net: not set. Validating first E-fuse MAC cpsw, usb_ether Hit any key to stop autoboot: 0 gpio: pin 53 (gpio 53) value is 1 switch to partitions #0, OK mmc0 is current device gpio: pin 54 (gpio 54) value is 1 Checking for: /uEnv.txt ... Checking for: /boot.scr ... Checking for: /boot/boot.scr ... Checking for: /boot/uEnv.txt ... gpio: pin 55 (gpio 55) value is 1 39 bytes read in 40 ms (0 Bytes/s) Loaded environment from /boot/uEnv.txt Checking if uname_r is set in /boot/uEnv.txt... gpio: pin 56 (gpio 56) value is 1 Running uname_boot ... loading /boot/vmlinuz-3.14.26-gb9df364-dirty ... 4391432 bytes read in 280 ms (15 MiB/s) loading /boot/dtbs/3.14.26-gb9df364-dirty/ntx-lf101.dtb ... 33329 bytes read in 86 ms (377.9 KiB/s) debug: [console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait fixrtc] ... debug: [bootz 0x82000000 - 0x88000000] ... Kernel image @ 0x82000000 [ 0x000000 - 0x430208 ] ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8fff4000, end 8ffff230 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 3.14.26-gb9df364-dirty (patrick@vb) (gcc version 4.8.3 20140401 (prerelease) (crosstool-NG linaro-1.13.1-4.8-2014.04 - Linaro GCC 4.8-2014.04) ) #16 SMP Thu Sep 3 11:18:27 EDT 2015 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine model: TI AM335x BeagleBone [ 0.000000] cma: CMA: reserved 16 MiB at 9e800000 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (neon ) [ 0.000000] PERCPU: Embedded 9 pages/cpu @df9d3000 s14720 r8192 d13952 u36864 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129536 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait fixrtc [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 486592K/522240K available (5703K kernel code, 700K rwdata, 2212K rodata, 402K init, 5521K bss, 35648K reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc07c3128 (7917 kB) [ 0.000000] .init : 0xc07c4000 - 0xc0828980 ( 403 kB) [ 0.000000] .data : 0xc082a000 - 0xc08d9198 ( 701 kB) [ 0.000000] .bss : 0xc08d9198 - 0xc0e3d5c0 (5522 kB) [ 0.000000] Hierarchical RCU implementation. [ 0.000000] RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1 [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: timer2 at 26000000 Hz [ 0.000012] sched_clock: 32 bits at 26MHz, resolution 38ns, wraps every 165191049177ns [ 0.000050] OMAP clocksource: timer1 at 26000000 Hz [ 0.000747] Console: colour dummy device 80x30 [ 0.000793] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar [ 0.000801] ... MAX_LOCKDEP_SUBCLASSES: 8 [ 0.000808] ... MAX_LOCK_DEPTH: 48 [ 0.000815] ... MAX_LOCKDEP_KEYS: 8191 [ 0.000821] ... CLASSHASH_SIZE: 4096 [ 0.000828] ... MAX_LOCKDEP_ENTRIES: 16384 [ 0.000834] ... MAX_LOCKDEP_CHAINS: 32768 [ 0.000840] ... CHAINHASH_SIZE: 16384 [ 0.000847] memory used by lock dependency info: 3695 kB [ 0.000854] per task-struct memory footprint: 1152 bytes [ 0.000895] Calibrating delay loop... 1076.42 BogoMIPS (lpj=5382144) [ 0.079208] pid_max: default: 32768 minimum: 301 [ 0.079529] Security Framework initialized [ 0.079635] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.079647] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.097568] CPU: Testing write buffer coherency: ok [ 0.098714] CPU0: thread -1, cpu 0, socket -1, mpidr 0 [ 0.098777] Setting up static identity map for 0x8056bbf0 - 0x8056bc60 [ 0.101570] Brought up 1 CPUs [ 0.101586] SMP: Total of 1 processors activated. [ 0.101595] CPU: All CPU(s) started in SVC mode. [ 0.104061] devtmpfs: initialized [ 0.111791] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.143991] omap_hwmod: tptc0 using broken dt data from edma [ 0.144322] omap_hwmod: tptc1 using broken dt data from edma [ 0.144637] omap_hwmod: tptc2 using broken dt data from edma [ 0.151976] omap_hwmod: debugss: _wait_target_disable failed [ 0.209815] pinctrl core: initialized pinctrl subsystem [ 0.213846] regulator-dummy: no parameters [ 0.216797] NET: Registered protocol family 16 [ 0.221586] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.226729] cpuidle: using governor ladder [ 0.226754] cpuidle: using governor menu [ 0.235690] syscon 44e10000.control_module: regmap [mem 0x44e10000-0x44e107fb] registered [ 0.239148] platform 49000000.edma: alias fck already exists [ 0.239270] platform 49000000.edma: alias fck already exists [ 0.239291] platform 49000000.edma: alias fck already exists [ 0.243113] OMAP GPIO hardware version 0.1 [ 0.275936] No ATAGs? [ 0.275960] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.332221] bio: create slab at 0 [ 0.367019] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver [ 0.369170] vbat: 5000 mV [ 0.371234] vmmcsd_fixed: 3300 mV [ 0.372445] wlan-en-regulator: 1800 mV [ 0.377481] i2c-core: driver [palmas] using legacy suspend method [ 0.377499] i2c-core: driver [palmas] using legacy resume method [ 0.378855] SCSI subsystem initialized [ 0.381126] usbcore: registered new interface driver usbfs [ 0.381521] usbcore: registered new interface driver hub [ 0.382188] usbcore: registered new device driver usb [ 0.384313] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c0_pins, deferring probe [ 0.384353] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral [ 0.390448] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.395063] Switched to clocksource timer1 [ 0.532198] NET: Registered protocol family 2 [ 0.533887] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.534055] TCP bind hash table entries: 4096 (order: 5, 147456 bytes) [ 0.535418] TCP: Hash tables configured (established 4096 bind 4096) [ 0.535604] TCP: reno registered [ 0.535630] UDP hash table entries: 256 (order: 2, 20480 bytes) [ 0.535803] UDP-Lite hash table entries: 256 (order: 2, 20480 bytes) [ 0.536752] NET: Registered protocol family 1 [ 0.538013] RPC: Registered named UNIX socket transport module. [ 0.538032] RPC: Registered udp transport module. [ 0.538041] RPC: Registered tcp transport module. [ 0.538049] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.539125] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available [ 0.547067] futex hash table entries: 256 (order: 2, 16384 bytes) [ 0.679188] VFS: Disk quotas dquot_6.5.2 [ 0.679383] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.681135] NFS: Registering the id_resolver key type [ 0.681468] Key type id_resolver registered [ 0.681484] Key type id_legacy registered [ 0.681591] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 0.681959] msgmni has been set to 982 [ 0.684645] io scheduler noop registered [ 0.684666] io scheduler deadline registered [ 0.684731] io scheduler cfq registered (default) [ 0.688077] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.693477] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.700593] omap_uart 44e09000.serial: no wakeirq for uart0 [ 0.701173] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a OMAP UART0 [ 1.357407] console [ttyO0] enabled [ 1.362973] omap_uart 481a8000.serial: no wakeirq for uart0 [ 1.368711] 481a8000.serial: ttyO4 at MMIO 0x481a8000 (irq = 61, base_baud = 3000000) is a OMAP UART4 [ 1.381694] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20 [ 1.416692] brd: module loaded [ 1.436046] loop: module loaded [ 1.439578] (stk) :sysfs entries created [ 1.443503] (stk) : debugfs entries created [ 1.448553] (hci_tty): inside hci_tty_init [ 1.453877] (hci_tty): allocated 251, 0 [ 1.463340] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.486767] usbcore: registered new interface driver asix [ 1.492401] usbcore: registered new interface driver ax88179_178a [ 1.499383] usbcore: registered new interface driver cdc_ether [ 1.505595] usbcore: registered new interface driver smsc95xx [ 1.511543] usbcore: registered new interface driver net1080 [ 1.517689] usbcore: registered new interface driver cdc_subset [ 1.523782] usbcore: registered new interface driver zaurus [ 1.529728] usbcore: registered new interface driver cdc_ncm [ 1.537274] usbcore: registered new interface driver cdc_wdm [ 1.543224] usbcore: registered new interface driver usb-storage [ 1.549638] usbcore: registered new interface driver usbtest [ 1.558333] mousedev: PS/2 mouse device common for all mice [ 1.568680] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0 [ 1.577005] i2c /dev entries driver [ 1.580741] Driver for 1-wire Dallas network protocol. [ 1.590654] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.712809] mmc0: host does not support reading read-only switch. assuming write-enable. [ 1.722945] mmc0: new high speed SDHC card at address aaaa [ 1.730807] mmcblk0: mmc0:aaaa SU32G 29.7 GiB [ 1.740219] mmcblk0: p1 p2 [ 1.789412] mmc1: BKOPS_EN bit is not set [ 1.800707] mmc1: new high speed MMC card at address 0001 [ 1.808442] ledtrig-cpu: registered to indicate activity on CPUs [ 1.814539] mmcblk1: mmc1:0001 MMC04G 3.65 GiB [ 1.820113] mmcblk1boot0: mmc1:0001 MMC04G partition 1 1.00 MiB [ 1.827086] usbcore: registered new interface driver usbhid [ 1.832494] usbhid: USB HID core driver [ 1.837010] mmcblk1boot1: mmc1:0001 MMC04G partition 2 1.00 MiB [ 1.844950] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral [ 1.852962] mmcblk1: p1 [ 1.861787] oprofile: using arm/armv7 [ 1.866148] TCP: cubic registered [ 1.869374] Initializing XFRM netlink socket [ 1.873601] NET: Registered protocol family 17 [ 1.878198] NET: Registered protocol family 15 [ 1.882802] Key type dns_resolver registered [ 1.887857] mmcblk1boot1: unknown partition table [ 1.896106] PM: bootloader does not support rtc-only! [ 1.901029] ThumbEE CPU extension supported. [ 1.905383] Registering SWP/SWPB emulation handler [ 1.910034] SmartReflex Class3 initialized [ 1.917048] mmcblk1boot0: unknown partition table [ 1.925966] vbat: disabling [ 1.928696] regulator-dummy: disabling [ 1.938803] omap_hsmmc 47810000.mmc: card claims to support voltages below defined range [ 1.955104] DCDC1: at 1350 mV [ 1.960711] vdd_mpu: 925 <--> 1375 mV at 1325 mV [ 1.967688] vdd_core: 925 <--> 1150 mV at 1125 mV [ 1.974453] LDO1: at 1800 mV [ 1.979966] LDO2: at 3300 mV [ 1.984825] mmc2: queuing unknown CIS tuple 0x91 (3 bytes) [ 1.992582] LDO3: 1800 mV [ 1.996877] mmc2: new high speed SDIO card at address 0001 [ 2.008025] LDO4: at 3300 mV [ 2.013296] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 2.018720] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 2.025429] remoteproc0: wkup_m3 is available [ 2.029750] remoteproc0: Note: remoteproc is still under development and considered experimental. [ 2.038483] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed. [ 2.049991] remoteproc0: Direct firmware load failed with error -2 [ 2.056160] remoteproc0: Falling back to user helper [ 2.125061] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6 [ 2.130990] davinci_mdio 4a101000.mdio: detected phy mask fffffffc [ 2.140325] libphy: 4a101000.mdio: probed [ 2.144235] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver unknown [ 2.152092] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver unknown [ 2.161416] cpsw 4a100000.ethernet: Detected MACID = 7c:66:9d:1d:af:c6 [ 2.172577] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801) [ 2.181118] sr_init: No PMIC hook to init smartreflex [ 2.187049] sr_init: platform driver register failed for SR [ 2.216242] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem [ 2.223350] EXT4-fs (mmcblk0p2): write access will be enabled during recovery [ 2.964339] EXT4-fs (mmcblk0p2): recovery complete [ 2.974414] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 2.982498] VFS: Mounted root (ext4 filesystem) readonly on device 179:2. [ 2.991503] devtmpfs: mounted [ 2.994945] Freeing unused kernel memory: 400K (c07c4000 - c0828000) Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory [ 3.337311] random: init urandom read with 73 bits of entropy available [ 3.621113] init: plymouth-upstart-bridge main process (715) terminated with status 1 [ 3.639479] init: plymouth-upstart-bridge main process ended, respawning [ 3.774471] init: plymouth-upstart-bridge main process (725) terminated with status 1 [ 3.782418] init: plymouth-upstart-bridge main process ended, respawning [ 3.793074] init: ureadahead main process (718) terminated with status 5 [ 3.896118] init: plymouth-upstart-bridge main process (728) terminated with status 1 [ 3.903819] init: plymouth-upstart-bridge main process ended, respawning [ 6.817791] remoteproc0: failed to load am335x-pm-firmware.elf [ 6.871239] remoteproc0: request_firmware failed: -2 [ 6.876339] wkup_m3 44d00000.wkup_m3: rproc_boot failed [ 8.165474] (stk) :ldisc installation timeout[ 9.165197] (stk) : timed out waiting for ldisc to be un-installed [ 10.275290] (stk) :ldisc installation timeout [ 11.275227] (stk) : timed out waiting for ldisc to be un-installed * Stopping Send an event to indicate plymouth is up [ OK ] * Starting Mount filesystems on boot [ OK ] * Starting Fix-up /sys/kernel/debug filesystem [ OK ] * Stopping Fix-up /sys/kernel/debug filesystem [ OK ] * Starting Populate and link to /run filesystem [ OK ] * Stopping Populate and link to /run filesystem [ OK ] * Stopping Track if upstart is running in a container [ OK ] * Starting Initialize or finalize resolvconf [ OK ] * Starting set console keymap [ OK ] * Starting Signal sysvinit that virtual filesystems are mounted [ OK ] * Starting Signal sysvinit that virtual filesystems are mounted [ OK ] * Stopping set console keymap [ OK ] * Starting Signal sysvinit that remote filesystems are mounted [ OK ] * Starting Bridge udev events into upstart [ OK ] * Starting device node and kernel event manager [ OK ] * Starting load modules from /etc/modules [ OK ] * Starting cold plug devices [ OK ] * Starting log initial device creation [ OK ] * Stopping load modules from /etc/modules [ OK ] * Starting configure network device security [ OK ] * Starting Signal sysvinit that the rootfs is mounted [ OK ] * Stopping cold plug devices [ OK ] * Stopping log initial device creation [ OK ] * Starting configure network device security [ OK ] * Starting set console font [ OK ] * Stopping set console font [ OK ] * Starting userspace bootsplash [ OK ] * Stopping userspace bootsplash [ OK ] * Starting Mount network filesystems [ OK ] * Starting Send an event to indicate plymouth is up [ OK ] (stk) :ldisc installation timeout * Starting Clean /tmp directory [ OK ] * Stopping Clean /tmp directory [ OK ] * Stopping Send an event to indicate plymouth is up [ OK ] * Stopping Mount network filesystems [ OK ] [ 13.385384] (stk) : timed out waiting for ldisc to be un-installed Waiting for network configuration... Waiting up to 60 more seconds for network configuration... Booting system without full network configuration... * Starting Signal sysvinit that local filesystems are mounted [ OK ] * Starting configure network device security [ OK ] * Stopping Mount filesystems on boot [ OK ] * Starting Failsafe Boot Delay [ OK ] * Starting flush early job output to logs [ OK ] * Starting configure network device [ OK ] (stk) :ldisc installation timeout * Starting D-Bus system message bus [ OK ] * Stopping flush early job output to logs [ OK ] * Stopping Failsafe Boot Delay [ OK ] * Starting system logging daemon [ OK ] (stk) : timed out waiting for ldisc to be un-installed * Starting System V initialisation compatibility [ OK ] * Starting configure virtual network devices [ OK ] * Starting mDNS/DNS-SD daemon [ OK ] * Starting Reload cups, upon starting avahi-daemon to make sure remote q[ OK ]are populated * Stopping System V initialisation compatibility [ OK ] (stk) :ldisc installation timeout * Starting Reload cups, upon starting avahi-daemon to make sure remote q[fail]are populated [ 17.605157] (stk) : timed out waiting for ldisc to be un-installed * Starting System V runlevel compatibility [ OK ] * Starting save kernel messages [ OK ] * Starting OpenSSH server [ OK ] * Starting ACPI daemon [ OK ] * Starting regular background program processing daemon [ OK ] * Stopping save kernel messages [ OK ] * Loading cpufreq kernel modules... (stk) :ldisc installation timeout [ OK ] * disabled, governor not available... * Starting Bridge file events into upstart [ OK ] * CPUFreq Utilities: Setting ondemand CPUFreq governor... * Starting Bridge socket events into upstart [ OK ] (stk) : timed out waiting for ldisc to be un-installed [ 19.721750] Bluetooth: st_register failed -22 [ OK ] udhcpd: Disabled. Edit /etc/default/udhcpd to enable it. AH00558: apache2: Could not reliably determine the server's fully qualified domain name, using 127.0.1.1. Set the 'ServerName' directive globally to suppress this message * * Stopping System V runlevel compatibility [ OK ] Ubuntu 14.04.1 LTS arm ttyO0 default username:password is [ubuntu:temppwd] arm login: ubuntu Password: Welcome to Ubuntu 14.04.1 LTS (GNU/Linux 3.14.26-gb9df364-dirty armv7l) * Documentation: https://help.ubuntu.com/ The programs included with the Ubuntu system are free software; the exact distribution terms for each program are described in the individual files in /usr/share/doc/*/copyright. Ubuntu comes with ABSOLUTELY NO WARRANTY, to the extent permitted by applicable law. To run a command as administrator (user "root"), use "sudo ". See "man sudo_root" for details. ubuntu@arm:~$ lsmod Module Size Used by wl18xx 80483 0 wlcore 176264 2 wl18xx mac80211 454728 2 wl18xx,wlcore cfg80211 414003 3 mac80211,wl18xx,wlcore wlcore_sdio 4139 0 btwilink 3883 0 bluetooth 262665 2 btwilink 6lowpan_iphc 6286 1 bluetooth ubuntu@arm:~$ ifconfig eth0 Link encap:Ethernet HWaddr 7c:66:9d:1d:af:c6 UP BROADCAST MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) Interrupt:56 lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) ubuntu@arm:~$