[Start: Texas Instruments XDS110 USB Debug Probe] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\************~1.SCP\AppData\Local\TEXASI~1\ CCS\ccs1271\0\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 100/110/510 class product. This utility will load the adapter 'jioxds110.dll'. The library build date was 'Apr 19 2024'. The library build time was '14:04:01'. The library package version is '12.7.0.00130'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. The controller has a version number of '5' (0x00000005). The controller has an insertion length of '0' (0x00000000). This utility will attempt to reset the controller to enter SWD mode. -----[Print the reset-command hardware log-file]----------------------------- This emulator does not create a reset log-file. -----[Perform the SWD Mode Integrity test]----------------------------------- This test will read the IDCODE register 1 time. The IDCODE register value is 0x6ba02477. The SWD Mode Integrity test has succeeded. [End: Texas Instruments XDS110 USB Debug Probe]