#!/bin/bash # Environment setup to be done if using MSYS Bash shell for build # Specify the base directory of the c6000 compiler with UNIX style path separator export C6X_BASE_DIR='"C:/ti/ccsv5/tools/compiler/c6000_7.4.2"' # Specify the base directory of the c6000 compiler in format understandable by the MSYS Bash shell export C6X_BASE_DIR_MSYS=/c/ti/ccsv5/tools/compiler/c6000_7\.4\.2 # Don't modify the below variables. They are derived from the above definitions export PATH=$PATH:$C6X_BASE_DIR_MSYS/bin export TOOLSC6X=$C6X_BASE_DIR export TOOLSC6XDOS=$C6X_BASE_DIR