/** * @file multicoreLoopback.c * * @brief * This is an example application which showcases how the SRIO Driver * API can be used in a multiple core environment. * * The test suite sends/receives data as follows:- * * CORE 1 --> CORE 2 --> CORE 3 --> CORE 0 --> CORE 1 * * At each step the received data is validated (Payload and Received * Identifiers). * * The goal of the test suite is to showcase that the SRIO Driver API * are multi-core safe. * * \par * NOTE: * (C) Copyright 2009 Texas Instruments, Inc. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * * \par */ #include #include #include #include #include #include #include #include #include #include #include #include /* IPC includes */ #include #include #include #include #include #include /* SRIO Driver Include File. */ #include /* CPPI/QMSS Include Files. */ #include #include #include /* CSL Include Files */ #include #include #include #include #include /* PDK module Headers */ #include /********************************************************************** ************************** LOCAL Definitions ************************* **********************************************************************/ #define NUM_HOST_DESC 32 #define SIZE_HOST_DESC 48 #define SRIO_MAX_MTU 256 /* Defines the core number responsible for system initialization. */ #define CORE_SYS_INIT 1 /* Number of cores for which the test is being executed. */ #define NUM_CORES 4 /* SRIO Application Hardware Semaphore. */ #define SRIO_APP_HW_SEM 5 /********************************************************************** ************************** Global Variables ************************** **********************************************************************/ /* Memory used for the descriptors. */ #pragma DATA_ALIGN (host_region, 16) Uint8 host_region[NUM_HOST_DESC * SIZE_HOST_DESC]; Qmss_InitCfg qmssInitConfig; /* Global Varialble which keeps track of the core number executing the * application. */ UInt32 coreNum = 0xFFFF; /* from producer_srio.c * #pragma DATA_SECTION (isSRIOInitialized, ".srioSharedMem"); * volatile Uint32 isSRIOInitialized = 0; */ #pragma DATA_ALIGN (isSRIOInitialized, 128) #pragma DATA_SECTION (isSRIOInitialized, ".srioSharedMem"); volatile Uint32 isSRIOInitialized = 0; #pragma DATA_ALIGN (isSRIOSocketsCreated, 128) #pragma DATA_SECTION (isSRIOSocketsCreated, ".srioSharedMem"); volatile Uint32 isSRIOSocketsCreated = 0; #pragma DATA_ALIGN (firstToRun, 128) #pragma DATA_SECTION (firstToRun, ".srioSharedMem"); volatile Uint32 firstToRun = 0; /* Memory used for the accumulator list. */ #pragma DATA_ALIGN (gHiPriAccumList, 16) UInt32 gHiPriAccumList[32]; /* These are the device identifiers used used in the TEST Application */ const uint32_t DEVICE_ID1_16BIT = 0xBEEF; const uint32_t DEVICE_ID1_8BIT = 0xAB; const uint32_t DEVICE_ID2_16BIT = 0x4560; const uint32_t DEVICE_ID2_8BIT = 0xCD; const uint32_t DEVICE_ID3_16BIT = 0x1234; const uint32_t DEVICE_ID3_8BIT = 0x12; const uint32_t DEVICE_ID4_16BIT = 0x5678; const uint32_t DEVICE_ID4_8BIT = 0x56; /********************************************************************** ************************* Extern Definitions ************************* **********************************************************************/ extern UInt32 malloc_counter; extern UInt32 free_counter; extern int32_t SrioDevice_init (void); extern Void* Osal_srioDataBufferMalloc(UInt32 numBytes); /* QMSS device specific configuration */ extern Qmss_GlobalConfigParams qmssGblCfgParams; /* CPPI device specific configuration */ extern Cppi_GlobalConfigParams cppiGblCfgParams; /* OSAL Data Buffer Memory Initialization. */ extern int32_t Osal_dataBufferInitMemory(uint32_t dataBufferSize); /********************************************************************** ************************ SRIO TEST FUNCTIONS ************************* **********************************************************************/ /** * @b Description * @n * Utility function which converts a local address to global. * * @param[in] addr * Local address to be converted * * @retval * Global Address */ static UInt32 l2_global_address (Uint32 addr) { UInt32 corenum; /* Get the core number. */ corenum = CSL_chipReadReg(CSL_CHIP_DNUM); /* Compute the global address. */ return (addr + (0x10000000 + (corenum*0x1000000))); } /** * @b Description * @n * Utility function that is required by the IPC module to set the proc Id. * The proc Id is set via this function instead of hard coding it in the .cfg file * * @retval * Not Applicable. */ Void myStartupFxn (Void) { MultiProc_setLocalId (CSL_chipReadReg (CSL_CHIP_DNUM)); } /** * @b Description * @n * This function enables the power/clock domains for SRIO. * * @retval * Not Applicable. */ static Int32 enable_srio (void) { #ifndef SIMULATOR_SUPPORT /* SRIO power domain is turned OFF by default. It needs to be turned on before doing any * SRIO device register access. This not required for the simulator. */ /* Set SRIO Power domain to ON */ CSL_PSC_enablePowerDomain (CSL_PSC_PD_SRIO); /* Enable the clocks too for SRIO */ CSL_PSC_setModuleNextState (CSL_PSC_LPSC_SRIO, PSC_MODSTATE_ENABLE); /* Start the state transition */ CSL_PSC_startStateTransition (CSL_PSC_PD_SRIO); /* Wait until the state transition process is completed. */ while (!CSL_PSC_isStateTransitionDone (CSL_PSC_PD_SRIO)); /* Return SRIO PSC status */ if ((CSL_PSC_getPowerDomainState(CSL_PSC_PD_SRIO) == PSC_PDSTATE_ON) && (CSL_PSC_getModuleState (CSL_PSC_LPSC_SRIO) == PSC_MODSTATE_ENABLE)) { /* SRIO ON. Ready for use */ return 0; } else { /* SRIO Power on failed. Return error */ return -1; } #else /* PSC is not supported on simulator. Return success always */ return 0; #endif } /** * @b Description * @n * System Initialization Code. This is added here only for illustrative * purposes and needs to be invoked once during initialization at * system startup. * * @retval * Success - 0 * @retval * Error - <0 */ static Int32 system_init (Void) { Int32 result; Qmss_MemRegInfo memRegInfo; /* Initialize the QMSS Configuration block. */ memset (&qmssInitConfig, 0, sizeof (Qmss_InitCfg)); /* Set up the linking RAM. Use the internal Linking RAM. * LLD will configure the internal linking RAM address and maximum internal linking RAM size if * a value of zero is specified. Linking RAM1 is not used */ qmssInitConfig.linkingRAM0Base = 0; qmssInitConfig.linkingRAM0Size = 0; qmssInitConfig.linkingRAM1Base = 0; qmssInitConfig.maxDescNum = NUM_HOST_DESC; #ifdef xdc_target__bigEndian System_printf("Using Big Endian QMSS\n"); qmssInitConfig.pdspFirmware[0].pdspId = Qmss_PdspId_PDSP1; qmssInitConfig.pdspFirmware[0].firmware = &acc48_be; qmssInitConfig.pdspFirmware[0].size = sizeof (acc48_be); #else System_printf("Using Little Endian QMSS\n"); qmssInitConfig.pdspFirmware[0].pdspId = Qmss_PdspId_PDSP1; qmssInitConfig.pdspFirmware[0].firmware = &acc48_le; qmssInitConfig.pdspFirmware[0].size = sizeof (acc48_le); #endif /* Initialize Queue Manager Sub System */ result = Qmss_init (&qmssInitConfig, &qmssGblCfgParams); if (result != QMSS_SOK) { System_printf ("Error initializing Queue Manager SubSystem error code : %d\n", result); return -1; } /* Start the QMSS. */ if (Qmss_start() != QMSS_SOK) { System_printf ("Error: Unable to start the QMSS\n"); return -1; } /* Memory Region 0 Configuration */ memRegInfo.descBase = (UInt32 *)l2_global_address((UInt32)host_region); memRegInfo.descSize = SIZE_HOST_DESC; memRegInfo.descNum = NUM_HOST_DESC; memRegInfo.manageDescFlag = Qmss_ManageDesc_MANAGE_DESCRIPTOR; memRegInfo.memRegion = Qmss_MemRegion_MEMORY_REGION_NOT_SPECIFIED; /* Initialize and inset the memory region. */ result = Qmss_insertMemoryRegion (&memRegInfo); if (result < QMSS_SOK) { System_printf ("Error inserting memory region: %d\n", result); return -1; } /* Initialize CPPI CPDMA */ result = Cppi_init (&cppiGblCfgParams); if (result != CPPI_SOK) { System_printf ("Error initializing Queue Manager SubSystem error code : %d\n", result); return -1; } /* CPPI and Queue Manager are initialized. */ System_printf ("Debug: Queue Manager and CPPI are initialized.\n"); System_printf ("Debug: Host Region 0x%x\n", host_region); return 0; } /** * @b Description * @n * The function tests multicore * * @param[in] hSrioDrv * Handle to the SRIO driver * * @retval * Success - 0 * @retval * Error - <0 */ static Int32 test_multicore (Srio_DrvHandle hSrioDrv) { Srio_SockHandle srioSocket; Srio_SockBindAddrInfo bindInfo; UInt8* txData; Srio_SockAddrInfo to; Srio_SockAddrInfo from; UInt16 idx; Int32 num_bytes; UInt8* ptr_rxDataPayload; Int32 sendToCore; Int32 recvFromCore; Srio_DrvBuffer hDrvBuffer; UInt32 allocatedLen; UInt16 coreDeviceID[NUM_CORES]; UInt8 errCnt =0; System_printf ("**********************************************\n"); System_printf ("******** Multicore Testing (Core %d) *********\n", coreNum); System_printf ("**********************************************\n"); /* Open SRIO Socket in Blocking Mode * Open a socket with the driver handle. Get a socket handle. * Now you can transmit and rx*/ srioSocket = Srio_sockOpen (hSrioDrv, Srio_SocketType_TYPE11, TRUE); if (srioSocket == NULL) { System_printf ("Error: Unable to open socket1\n"); return -1; } /* Initialize the core Device IDs: Each core has a seperate device ID. */ coreDeviceID[0] = DEVICE_ID1_16BIT; coreDeviceID[1] = DEVICE_ID2_16BIT; coreDeviceID[2] = DEVICE_ID3_16BIT; coreDeviceID[3] = DEVICE_ID4_16BIT; /* Initialize the core bindings; we use the same mailbox & letter identifiers. */ bindInfo.type11.tt = TRUE; bindInfo.type11.id = coreDeviceID[coreNum]; bindInfo.type11.letter = 2; bindInfo.type11.mbox = 3; bindInfo.type11.segMap = 0x0; /* Bind the SRIO socket * Bind to a queue in the srio hardware*/ if (Srio_sockBind (srioSocket, &bindInfo) < 0) { System_printf ("Error: socket1 bind failed\n"); return -1; } /* Get a transmit buffer from the SRIO Driver. */ hDrvBuffer = Srio_allocTransmitBuffer(hSrioDrv, &txData, &allocatedLen); if (hDrvBuffer == NULL) { System_printf ("Error: Producer Memory Allocation failed.\n"); return -1; } System_printf("Debug(Core %i): received a tx buff %p with length %i.\n", coreNum, txData, allocatedLen); /* Create the transmit data payload. */ for (idx = 0; idx < 100; idx++) txData[idx] = 0x00 | coreNum; System_printf("Debug(Core %i): txData 0x%x 0x%x 0x%x...\n",coreNum, txData[0],txData[50], txData[99]); /* The global variable is a shared resource which is being accessed from multiple cores. * So here we need to protect it and ensure that there is only 1 core which is accessing * it at a time. We use a Hardware Semaphore to protect this. */ while ((CSL_semAcquireDirect (SRIO_APP_HW_SEM)) == 0); /* Invalidate the cache and make sure you get the latest from the memory. */ CACHE_invL1d ((void *) &isSRIOSocketsCreated, 128, CACHE_WAIT); /* The core has created the sockets:*/ isSRIOSocketsCreated++; /* The SRIO Socket has been created. Writeback the contents to the cache. */ CACHE_wbL1d ((void *) &isSRIOSocketsCreated, 128, CACHE_WAIT); /* Release the hardware semaphore. */ CSL_semReleaseSemaphore (SRIO_APP_HW_SEM); /* We can proceed with the data transmission & reception tests only after all the * cores have created and bound their SRIO sockets. This is a simple counter running * in shared memory which allows us to SYNC up the socket creation. Wait till all the * cores have created the sockets */ while (isSRIOSocketsCreated != NUM_CORES) CACHE_invL1d ((void *) &isSRIOSocketsCreated, 128, CACHE_WAIT); System_printf ("Core %i is ready to start RR-------------------------------------------\n", coreNum); /* Is this the starting core? */ // while ((CSL_semAcquireDirect (SRIO_APP_HW_SEM)) == 0) // { // //System_printf("Debug(Core %i): Waiting for sem.\n",coreNum); // }; // System_printf("Debug(Core %i): Got sem\n",coreNum); // CACHE_invL1d ((void *) &firstToRun, 128, CACHE_WAIT); if (coreNum == 1) { // firstToRun = 2; // CACHE_wbL1d ((void *) &firstToRun, 128, CACHE_WAIT); // Cache_wb ((void *) &firstToRun, 4, Cache_Type_L1D, TRUE); System_printf ("Debug(Core %i) is first.\n", coreNum); /* Starting Core: This is a special case because unlike the other cores; this initiates * the whole test cycle by sending the first packet. */ sendToCore = (coreNum + 1) % NUM_CORES; recvFromCore = coreNum - 1; if (recvFromCore < 0) recvFromCore = NUM_CORES-1; /* Send the data out. */ to.type11.tt = TRUE; to.type11.id = 0xbeef;//coreDeviceID[sendToCore]; to.type11.letter = 2; to.type11.mbox = 3; /* Send the data out from the producer core to the consumer core. */ if (Srio_sockSend (srioSocket, hDrvBuffer, 100, &to) < 0) { System_printf ("Error: SRIO Socket send failed\n"); return -1; } /* Debug Message */ System_printf ("Debug(Core %d): Successfully sent data to ID:0x%x\n", coreNum, to.type11.id); // /* CORE0: Wait for data to arrive from NUM_CORES-1 */ // System_printf ("Debug(Core %d): Waiting for data to arrive. myID: 0x%x\n", coreNum, bindInfo.type11.id); // // /* Receive the data. */ // num_bytes = Srio_sockRecv (srioSocket, (Srio_DrvBuffer*)&ptr_rxDataPayload, &from); // if (num_bytes > 0) // { // /* Make sure that the data was received from the producer core */ // if (from.type11.id != coreDeviceID[recvFromCore]) // { // System_printf ("Error: Invalid source id 0x%x Expected 0x%x\n", from.type11.id, coreDeviceID[recvFromCore]); // return -1; // } // // /* Received and Transmitted packet length match. Payload verification */ // for (idx = 0; idx < 100; idx++) // { // if (ptr_rxDataPayload[idx] != (0xA0 | recvFromCore)) // { // System_printf ("Error: Receive Data Payload verification failed @ index %d value = %d\n", idx, ptr_rxDataPayload[idx]); // // return -1; // } // } // System_printf ("Debug(Core %d): Successfully received %d bytes\n", coreNum, num_bytes); // System_printf("Debug(Core %i): rxData 0x%x 0%x 0x%x...\n", coreNum, ptr_rxDataPayload[0],ptr_rxDataPayload[50], ptr_rxDataPayload[99]); // // // /* Cleanup the received data payload. */ // Srio_freeRxDrvBuffer(srioSocket, (Srio_DrvBuffer)ptr_rxDataPayload); // } // else // { // /* Error: In receiving data */ // System_printf ("Error: Unable to receive data error code: %d\n", num_bytes); // return -1; // } } CSL_semReleaseSemaphore (SRIO_APP_HW_SEM); Uint8 i; for( i = 0; i < 16; i++) { /* Any other core besides the starting core will initally wait for data to arrive */ sendToCore = (coreNum + 1) % NUM_CORES; recvFromCore = coreNum - 1; if (recvFromCore < 0) recvFromCore = NUM_CORES-1; System_printf ("Debug(Core %d): Waiting for data to arrive. myId: 0x%x\n", coreNum, bindInfo.type11.id); /* Receive the data. */ num_bytes = Srio_sockRecv (srioSocket, (Srio_DrvBuffer*)&ptr_rxDataPayload, &from); if (num_bytes > 0) { /* Make sure that the data was received from the producer core */ if (from.type11.id != coreDeviceID[recvFromCore]) { System_printf ("Error: Invalid source id 0x%x Expected 0x%x\n", from.type11.id, coreDeviceID[recvFromCore]); errCnt++; //return -1; } /* Received and Transmitted packet length match. Payload verification */ for (idx = 0; idx < 100; idx++) { { if (ptr_rxDataPayload[idx] != ((0x00 + ((i)<<4)) | recvFromCore)) { System_printf ("Error: Receive Data Payload verification failed @ index %d value = 0x%x expected 0x%x\n", idx, ptr_rxDataPayload[idx], ((0x00 + (i<<4)) | recvFromCore)); idx = 100; errCnt++; // return -1; } } } System_printf ("Debug(Core %d): Successfully received %d bytes. rxData 0x%x 0x%x 0x%x...\n", coreNum, num_bytes,ptr_rxDataPayload[0],ptr_rxDataPayload[50], ptr_rxDataPayload[99]); //System_printf("Debug(Core %i): rxData 0x%x 0%x 0x%x...\n", coreNum, ptr_rxDataPayload[0],ptr_rxDataPayload[50], ptr_rxDataPayload[99]); /* Cleanup the received data payload. */ Srio_freeRxDrvBuffer(srioSocket, (Srio_DrvBuffer)ptr_rxDataPayload); } else { /* Error: In receiving data */ System_printf ("Error: Unable to receive data error code: %d\n", num_bytes); errCnt++; // return -1; } /* CoreX: Sends outs the packet to CoreX+1. */ to.type11.tt = TRUE; to.type11.id = coreDeviceID[sendToCore]; to.type11.letter = 2; to.type11.mbox = 3; if(coreNum == 1) //increment i early because it initially transmitted. { for (idx = 0; idx < 100; idx++) txData[idx] = (0x00+((i+1)<<4)) | coreNum; } else { for (idx = 0; idx < 100; idx++) txData[idx] = (0x00+((i)<<4)) | coreNum; } /* Send the data out from the producer core to the consumer core. */ if (Srio_sockSend (srioSocket, hDrvBuffer, 100, &to) < 0) { System_printf ("Error: SRIO Socket send failed\n"); errCnt++; //return -1; } System_printf ("Debug(Core %d): Successfully sent data to ID:0x%x\n", coreNum, coreDeviceID[sendToCore]); } /* Close the sockets */ Srio_sockClose (srioSocket); /* We are done with the test. */ if(errCnt > 0) { System_printf("Debug(Core %i): Completed with errors %i.\n",coreNum,errCnt); return -1; } System_printf ("Debug(Core %d): Multicore Test Passed\n", coreNum); return 0; } /** * @b Description * @n * This is the Multicore Test task * * @retval * Not Applicable. */ static Void multicoreTestTask(UArg arg0, UArg arg1) { Srio_DrvConfig cfg; Srio_DrvHandle hSrioDriver; UInt8 isAllocated; /* Initialize the OSAL Data Buffer */ if (Osal_dataBufferInitMemory(SRIO_MAX_MTU) < 0) return; /* Initialize the SRIO Driver Configuration. */ memset ((Void *)&cfg, 0, sizeof(Srio_DrvConfig)); /* Setup the SRIO Driver Managed Configuration. */ cfg.bAppManagedConfig = FALSE; /* Driver Managed: Receive Configuration */ cfg.u.drvManagedCfg.bIsRxCfgValid = 1; cfg.u.drvManagedCfg.rxCfg.rxMemRegion = Qmss_MemRegion_MEMORY_REGION0; cfg.u.drvManagedCfg.rxCfg.numRxBuffers = 4; cfg.u.drvManagedCfg.rxCfg.rxMTU = SRIO_MAX_MTU; /* Accumulator Configuration. */ { int32_t coreToQueueSelector[4]; /* This is the table which maps the core to a specific receive queue. */ coreToQueueSelector[0] = 704; coreToQueueSelector[1] = 705; coreToQueueSelector[2] = 706; coreToQueueSelector[3] = 707; /* Since we are programming the accumulator we want this queue to be a HIGH PRIORITY Queue */ cfg.u.drvManagedCfg.rxCfg.rxCompletionQueue = Qmss_queueOpen (Qmss_QueueType_HIGH_PRIORITY_QUEUE, coreToQueueSelector[coreNum], &isAllocated); if (cfg.u.drvManagedCfg.rxCfg.rxCompletionQueue < 0) { System_printf ("Error: Unable to open the SRIO Receive Completion Queue\n"); return; } /* Accumulator Configuration is VALID. */ cfg.u.drvManagedCfg.rxCfg.bIsAccumlatorCfgValid = 1; /* Accumulator Configuration. */ cfg.u.drvManagedCfg.rxCfg.accCfg.channel = coreNum; cfg.u.drvManagedCfg.rxCfg.accCfg.command = Qmss_AccCmd_ENABLE_CHANNEL; cfg.u.drvManagedCfg.rxCfg.accCfg.queueEnMask = 0; cfg.u.drvManagedCfg.rxCfg.accCfg.queMgrIndex = coreToQueueSelector[coreNum]; cfg.u.drvManagedCfg.rxCfg.accCfg.maxPageEntries = 2; cfg.u.drvManagedCfg.rxCfg.accCfg.timerLoadCount = 0; cfg.u.drvManagedCfg.rxCfg.accCfg.interruptPacingMode = Qmss_AccPacingMode_LAST_INTERRUPT; cfg.u.drvManagedCfg.rxCfg.accCfg.listEntrySize = Qmss_AccEntrySize_REG_D; cfg.u.drvManagedCfg.rxCfg.accCfg.listCountMode = Qmss_AccCountMode_ENTRY_COUNT; cfg.u.drvManagedCfg.rxCfg.accCfg.multiQueueMode = Qmss_AccQueueMode_SINGLE_QUEUE; /* Initialize the accumulator list memory */ memset ((Void *)&gHiPriAccumList[0], 0, sizeof(gHiPriAccumList)); cfg.u.drvManagedCfg.rxCfg.accCfg.listAddress = l2_global_address((UInt32)&gHiPriAccumList[0]); System_printf("Debug(Core %i): list address 0x%x\n", coreNum, cfg.u.drvManagedCfg.rxCfg.accCfg.listAddress); } /* Driver Managed: Transmit Configuration */ cfg.u.drvManagedCfg.bIsTxCfgValid = 1; cfg.u.drvManagedCfg.txCfg.txMemRegion = Qmss_MemRegion_MEMORY_REGION0; cfg.u.drvManagedCfg.txCfg.numTxBuffers = 4; cfg.u.drvManagedCfg.txCfg.txMTU = SRIO_MAX_MTU; /* Start the SRIO Driver * Called by each core to get handle of active driver. */ hSrioDriver = Srio_start(&cfg); if (hSrioDriver == NULL) { System_printf ("Error: SRIO Driver Start Failed\n"); return; } /* SRIO Driver is operational at this time. */ System_printf ("Debug: SRIO Driver has been started Instance Handle 0x%p\n", hSrioDriver); /* Hook up the SRIO interrupts with the core. */ EventCombiner_dispatchPlug (48, (EventCombiner_FuncPtr)Srio_rxCompletionIsr, (UArg)hSrioDriver, TRUE); EventCombiner_enableEvent(48); /* Map the event id to hardware interrupt 8. */ Hwi_eventMap(8, 48); /* Enable interrupt 8. */ Hwi_enableInterrupt(8); /* SRIO Driver is operational at this time. */ System_printf ("Debug: SRIO Driver ISR has been registered\n"); /* Run the Multicore Test */ if (test_multicore (hSrioDriver) < 0) { System_printf ("Error: Multicore Tests failed\n"); return; } /* Print out the Malloc & Free Counter */ System_printf ("Debug(Core %d): Allocation Counter : %d\n", coreNum, malloc_counter); System_printf ("Debug(Core %d): Free Counter : %d\n", coreNum, free_counter); /* Check if there is a memory leak? Since we dont implement the DEINIT API * there are 'cfg.numRxDesc' and 'cfg.numTxDesc' buffers always allocated for * the SRIO Driver. 1 allocation is there for the Driver Instance * Take this into account while we check for leaks? */ if ((cfg.u.drvManagedCfg.rxCfg.numRxBuffers + cfg.u.drvManagedCfg.txCfg.numTxBuffers + free_counter + 1 ) != malloc_counter) { System_printf ("Error: Memory Leak Detected\n"); Task_exit(); } /* Control comes here implies that all testing passed. */ System_printf ("Debug(Core %d): Multicore Example successful.\n", coreNum); return; } /** * @b Description * @n * Entry point for the example * * @retval * Not Applicable. */ Void main(Void) { Task_Params taskParams; /* Get the core number. */ coreNum = CSL_chipReadReg (CSL_CHIP_DNUM); while ((CSL_semAcquireDirect (SRIO_APP_HW_SEM)) == 0); CACHE_invL1d ((void *) &firstToRun, 128, CACHE_WAIT); if(firstToRun == 0) { System_printf("\n\n\n\n******** Welcome to the Multicore Loopback Left Side Test ********* \n"); firstToRun = 1; CACHE_wbL1d ((void *) &firstToRun, 128, CACHE_WAIT); System_printf("Debug(Core %i) firstToRun %i\n",coreNum,firstToRun); } CSL_semReleaseSemaphore (SRIO_APP_HW_SEM); System_printf ("****************************************************\n"); System_printf ("****** Multicore Loopback Testing (Core %d) *******\n", coreNum); System_printf ("****************************************************\n"); /* Initialize the heap in shared memory. Using IPC module to do that */ Ipc_start(); /* Initialize the system only if the core was configured to do so. */ if (coreNum == CORE_SYS_INIT) { System_printf ("Debug(Core %d): System Initialization for CPPI & QMSS\n", coreNum); /* System Initialization */ if (system_init() < 0) return; /* Power on SRIO peripheral before using it */ if (enable_srio () < 0) { System_printf ("Error: SRIO PSC Initialization Failed\n"); return; } /* Device Specific SRIO Initializations: This should always be called before * initializing the SRIO Driver. */ if (SrioDevice_init() < 0) { System_printf ("Error: SRIO Hardware Initialization Failed\n"); return; } /* Initialize the SRIO Driver * Called only by one core. */ if (Srio_init () < 0) { System_printf ("Error: SRIO Driver Initialization Failed\n"); return; } /* SRIO Driver is operational at this time. */ System_printf ("Debug(Core %d): SRIO Driver has been initialized\n", coreNum); /* Write to the SHARED memory location at this point in time. The other cores cannot execute * till the SRIO Driver is up and running. */ isSRIOInitialized = 1; /* The SRIO IP block has been initialized. We need to writeback the cache here because it will * ensure that the rest of the cores which are waiting for SRIO to be initialized would now be * woken up. */ // CACHE_wbL1d ((void *) &isSRIOInitialized, 128, CACHE_WAIT); Cache_wb ((void *) &isSRIOInitialized, 4, Cache_Type_L1D, TRUE); } else { /* TODO: Testing this.... */ System_printf ("Debug(Core %d): Waiting for SRIO to be initialized.\n", coreNum); /* All other cores loop around forever till the SRIO is up and running. * We need to invalidate the cache so that we always read this from the memory. */ // while (isSRIOInitialized == 0) // CACHE_invL1d ((void *) &isSRIOInitialized, 128, CACHE_WAIT); while (isSRIOInitialized == 0) { Cache_inv ((void *) &isSRIOInitialized, 4, Cache_Type_L1D, TRUE); } System_printf("Debug(Core %d): SRIO Initialized.\n",coreNum); /* Start the QMSS. */ if (Qmss_start() != QMSS_SOK) { System_printf ("Error: Unable to start the QMSS\n"); return; } System_printf ("Debug(Core %d): SRIO can now be used.\n", coreNum); } /* Create the Multicore Test Task. */ Task_Params_init(&taskParams); Task_create(multicoreTestTask, &taskParams, NULL); /* Start the BIOS */ BIOS_start(); }