|
Radio Control Layer (RCL)
|
A PRX device normally acts as the main receiver in an NESB network. Depending on user configuration, the handler acts similarly to the Generic Rx Command handler, or it can add automatic acknowledgement and address filtering.
The following sections describe how the command can be configured and used, its life cycle, and how it fits into the RCL architecture.
In order to submit a PRX command, the following steps must have taken place:
Once these steps have been completed, RCL_Command_submit and RCL_Command_pend are called to effectively send a packet and then wait for the command to conclude.
As with any command handler, the application must built packets so that they are compatible with the internal packet format used in the LRF. Having said this, NESB packets also have a specific packet format that needs to be considered at the application level.
This can be accomplished by using a struct to define the various fields that need to be considered when building or checking the content of the packet.
Taking this into consideration, packet generation needs to consider how the 11-bit header is placed in the LRF FIFO. the following function shows one way to accomplish this:
Command configuration and submitting is similar to generic command handlers, but depending on the desired auto acknowledgment behavior, it might be necessary to also configure the sycnword specific behavior.
The NESB Prx command handler has a life cycle that depends on several things. If configuration is such that an acknowledgement is expected, the device will automatically switch from Rx mode to Tx mode to send an acknowledge to the specific PTX device that started the packet transaction. Furthermore, the PRX device performs address filtering so that it can ignore packets coming from PTX devices not associated with the network. If a valid packet from a valid address is received, the command can either continue listening for additional packets until a graceful or hard stop ends the operation. Once this has happened, the callback and the command status can be used for error checking and the application can proceed according to its specification.
| RCL Event (In) | Description |
|---|---|
| setup | Setup has been performed |
| timerStart | Timer-based start signalled |
| rxBufferUpdate | RX buffer has been updated |
| RCL Event (Out) | Description |
|---|---|
| lastCmdDone | The RCL is finished with the command |
| cmdStarted | Command handler has accepted and started executing |
| rxBufferFinished | An RX multi-buffer is finished |
| rxEntryAvail | An RX entry has been made available |
| LRF Event | Description |
|---|---|
| opDone | The PBE operation has finished |
| opError | Something went wrong. Cause located in the PBE ENDCAUSE register |
| rxOk | Packet received with CRC OK and not to be ignored by the MCU |
| rxNok | Packet received with CRC error |