Texas Instruments SmartRF Flash Programmer v1.13.7-no-mfc --------------------------------------------------------- SmartRFProgConsole [Target][Actions][File][Interface Slow][Change / IEEE address][Flash lock][Bootloader ID] The order of the parameters is irrelevant. Target: [S][AU][AS][B] S System-on-Chip (programmed via USB) Type S(n), where n is the board ID number, to select a specific EB. Otherwise, if there are multiple boards, the one to be programmed will be selected at random. AU EB application (programmed via USB) Type AU(n), where n is the board ID number, to select a specific EB. Otherwise, if there are multiple boards, the one to be programmed will be selected at random. AS(n) EB application (programmed via the EC2 adapter on serial port COMn). (only SmartRF04EB) B(n) EB bootloader (programmed via the EC2 adapter on serial port COMn). (only SmartRF04EB) Actions to perform: [P][EP][EPV][EPVC][PV][PVC][V][R][RP][EP][WP][CE] P Program (all targets) EP Erase and program (all targets) EPV Erase, program and verify (all targets) EPVC Erase, program and verify (CRC each page=>faster) (only target S) PV Program (append) and verify (only target S) PVC Program and verify (CRC each page=>faster) (only target S) V Verify against hex or hem file (targets S, AS, B) VC Verify against hex or hem file (CRC each page=>faster) (targets S, AS, B) R Read into hex file (only target S) RP= Read flash page into binary file (only target S) EP= Erase flash page (only target S) WP= Write flash page from binary file (only target S) EWP= Erase and Write flash page from binary file (only target S) CE Full chip erase (only target S) File: F="f" "f" Flash image file name (intel hex file (*.hex), or hex merge file (*.hem)) A merge file can contain one or more file/change specifications. See "example.hem" for how to create one. Interface Slow(Target = S): [IS] IS Program SoC (System on chip) with reduced speed on the debug interface. Change hex file before programming (e.g. for serial number): [A=a,D=d][EKF="f"] A=a,D=d Change one or more bytes in the hex file before downloading it. a Hexadecimal address (e.g. 2C03, 01BC25) d One or more bytes to be changed, in hexadecimal format, separated with dots (e.g. 4B, 1.2.3.A.B.C, 12.34.56.AB.CD.EF or 12.3.AB) EKF Patch hex file with Encryption Key data. "f" Certificate file from Certicom with encryption key data. IEEE MAC address related options [KI(F=f)] [RI(F=f,[PRI][SEC])] [WI(F=f,I=i)] (only CC243x, CC253x and CC254x) KI(F=f) Keep the IEEE MAC address currently on the chip when programming it RI(F=f,[PRI][SEC]) Read out the IEEE MAC address currently on the chip For devices with both a primary and a secondary address, the option "PRI" or "SEC" can be used to specify which to read. "PRI" is default. WI(F=f,I=i) Write the given IEEE MAC address to the chip when programming it f The chip's flash size in kB (only used for CC243x) CC243x: 32, 64, or 128 (determines the location of the IEEE address) CC253x, CC254x: set to 0 (not used) i IEEE MAC address to write in hexadecimal format, separated with dots (e.g. 00.12.4B.00.00.00.00.01). 8 bytes for CC243x and CC253x, and 6 bytes for CC254x. Flash lock (Target = S): [L(c)][LB(c)][LD(c)][LA(c)][LP(x-y)][LD][LPD(x-y)] "L(c), LB(c), LD(c), LA(c)" only CC243x, cc111x and CC251x. "LP(x-y), LD, LPD(x-y)" only CC253x and CC254x c Code for write protection of the upper section of the flash: CC111x, CC251x: 0=All, 1=24 kB, 16 kB, 8 kB, 4 kB, 2 kB, 1 kB, 7=None CC2430, CC2431: 0=All, 1=64 kB, 32 kB, 16 kB, 8 kB, 4 kB, 2 kB, 7=None L(c) Write protect section only (L(7) is equal to omitting this parameter) LB(c) Write protect section + boot block LD(c) Write protect section, and block debug commands LA(c) Write protect section + boot block, and block debug commands LP(x-y) Write protect flash pages from page x to page y. Several ranges can be given separated with a comma: E.g. LP(0-26,48-126), LP(0,1,2,8-10). LD Block debug commands LPD(x-y) Write protect flash pages and block debug commands. Bootloader ID (Target = B): I=i i Becomes the EB ID number when programming new bootloader. Use 1-4 digits (e.g. 0123, 3, or 45). Important: EBs that are used on the same computer must have unique ID numbers! Read/Erase/Write Flash page options: RP=n, EWP=n, WP=n, EP=n n The Page number Examples: SmartRFProgConsole S EPV F=C:\test.hex A=135,D="1 23 45" SmartRFProgConsole S P F="C:\test.hex" SmartRFProgConsole EPV AU(0123) F=D:\Test.hex SmartRFProgConsole B(1) EPV "F=C:\Filename with spaces.hex" I=1234 SmartRFProgConsole S EP F="C:\Test flash lock.hex" LB(3) SmartRFProgConsole S EP F="C:\Test flash lock.hex" LD SmartRFProgConsole S EP F="C:\Test flash lock.hex" LP(0-126) SmartRFProgConsole S EP F="C:\Test flash lock.hex" LPD(0-126) SmartRFProgConsole S EPV F="C:\test.hex" WI(F=0,I=00.12.4B.00.00.00.00.01) SmartRFProgConsole S EPV F="C:\test.hex" KI(F=1) SmartRFProgConsole S EPV F="C:\test.hex" EKF=certificate_example.txt SmartRFProgConsole S PVC F="C:\test.hex" SmartRFProgConsole S RP=1 F="C:\test.bin" SmartRFProgConsole S EP=1 SmartRFProgConsole S WP=1 F="C:\test.bin" SmartRFProgConsole S EWP=1 F="C:\test.bin" To list all connected EBs/programmers (max 64): SmartRFProgConsole X Status messages are printed to stdout, error messages to stderr. Return Codes: 0 = Success 1 = System error 2 = Parameter error 3 = Illegal parameter combinations 4 = Missing parameters 5 = Missing image file or communication error