-su-4.1# ./configure with_x=no --with-kerneldir=/home/shuwen/RDK3/RDK3.0/linux-04.04.00.01 --with-driver=userspace --host=arm-arago-linux-gnueabi --build=x86-linux --target=arm && make ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi- && make install ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi- >/tmp/log checking for a BSD-compatible install... /usr/bin/install -c checking whether build environment is sane... yes checking for arm-arago-linux-gnueabi-strip... no checking for strip... strip configure: WARNING: using cross tools not prefixed with host triplet checking for a thread-safe mkdir -p... /bin/mkdir -p checking for gawk... gawk checking whether make sets $(MAKE)... yes checking for arm-arago-linux-gnueabi-gcc... no checking for gcc... gcc checking for C compiler default output file name... a.out checking whether the C compiler works... yes checking whether we are cross compiling... yes checking for suffix of executables... checking for suffix of object files... o checking whether we are using the GNU C compiler... yes checking whether gcc accepts -g... yes checking for gcc option to accept ISO C89... none needed checking for style of include used by make... GNU checking dependency style of gcc... gcc3 checking whether gcc and cc understand -c and -o together... yes checking for a BSD-compatible install... /usr/bin/install -c checking whether make sets $(MAKE)... (cached) yes checking for mknod... /bin/mknod checking for mkfifo... /usr/bin/mkfifo checking for depmod... /sbin/depmod checking for libusb-config... no checking whether ln -s works... yes checking build system type... x86-unknown-linux-gnu checking host system type... arm-arago-linux-gnueabi checking for a sed that does not truncate output... /bin/sed checking for grep that handles long lines and -e... /bin/grep checking for egrep... /bin/grep -E checking for fgrep... /bin/grep -F checking for ld used by gcc... /usr/bin/ld checking if the linker (/usr/bin/ld) is GNU ld... yes checking for BSD- or MS-compatible name lister (nm)... no checking for arm-arago-linux-gnueabi-dumpbin... no checking for arm-arago-linux-gnueabi-link... no checking for dumpbin... no checking for link... link -dump -symbols checking the name lister (link -dump -symbols) interface... BSD nm checking the maximum length of command line arguments... 1572864 checking whether the shell understands some XSI constructs... yes checking whether the shell understands "+="... yes checking for /usr/bin/ld option to reload object files... -r checking for arm-arago-linux-gnueabi-objdump... no checking for objdump... objdump checking how to recognize dependent libraries... pass_all checking for arm-arago-linux-gnueabi-ar... no checking for ar... ar checking for arm-arago-linux-gnueabi-strip... strip checking for arm-arago-linux-gnueabi-ranlib... no checking for ranlib... ranlib checking command to parse link -dump -symbols output from gcc object... failed checking how to run the C preprocessor... gcc -E checking for ANSI C header files... yes checking for sys/types.h... yes checking for sys/stat.h... yes checking for stdlib.h... yes checking for string.h... yes checking for memory.h... yes checking for strings.h... yes checking for inttypes.h... yes checking for stdint.h... yes checking for unistd.h... yes checking for dlfcn.h... yes checking for objdir... .libs checking if gcc supports -fno-rtti -fno-exceptions... no checking for gcc option to produce PIC... -fPIC -DPIC checking if gcc PIC flag -fPIC -DPIC works... yes checking if gcc static flag -static works... yes checking if gcc supports -c -o file.o... yes checking if gcc supports -c -o file.o... (cached) yes checking whether the gcc linker (/usr/bin/ld) supports shared libraries... yes checking whether -lc should be explicitly linked in... no checking dynamic linker characteristics... GNU/Linux ld.so checking how to hardcode library paths into programs... immediate checking whether stripping libraries is possible... yes checking if libtool supports shared libraries... yes checking whether to build shared libraries... yes checking whether to build static libraries... yes checking for python... /usr/bin/python checking for python version... 2.6 checking for python platform... linux2 checking for python script directory... ${prefix}/lib/python2.6/dist-packages checking for python extension module directory... ${exec_prefix}/lib/python2.6/dist-packages checking for ANSI C header files... (cached) yes checking whether time.h and sys/time.h may both be included... yes checking fcntl.h usability... yes checking fcntl.h presence... yes checking for fcntl.h... yes checking limits.h usability... yes checking limits.h presence... yes checking for limits.h... yes checking sys/ioctl.h usability... yes checking sys/ioctl.h presence... yes checking for sys/ioctl.h... yes checking sys/time.h usability... yes checking sys/time.h presence... yes checking for sys/time.h... yes checking syslog.h usability... yes checking syslog.h presence... yes checking for syslog.h... yes checking for unistd.h... (cached) yes checking for an ANSI C-conforming const... yes checking for inline... inline checking for off_t... yes checking for pid_t... yes checking for size_t... yes checking whether struct tm is in sys/time.h or time.h... time.h checking return type of signal handlers... void checking for vprintf... yes checking for _doprnt... no checking for gethostname... yes checking for gettimeofday... yes checking for mkfifo... yes checking for select... yes checking for socket... yes checking for strdup... yes checking for strerror... yes checking for strtoul... yes checking for snprintf... yes checking for strsep... yes checking for vsyslog... yes checking for forkpty... no checking for forkpty in -lutil... yes checking vga.h usability... no checking vga.h presence... no checking for vga.h... no checking for X... disabled checking for getopt_long... yes checking for mktemp... yes checking for Linux kernel sources... /home/shuwen/RDK3/RDK3.0/linux-04.04.00.01/ checking for which drivers can be installed on this system... checking for caraca_init in -lcaraca_client... no checking ftdi.h usability... no checking ftdi.h presence... no checking for ftdi.h... no checking iguanaIR.h usability... no checking iguanaIR.h presence... no checking for iguanaIR.h... no checking for ir_strerror in -lirman... no checking for ir_strerror in -lirman_sw... no checking portaudio.h usability... no checking portaudio.h presence... no checking for portaudio.h... no checking alsa/asoundlib.h usability... no checking alsa/asoundlib.h presence... no checking for alsa/asoundlib.h... no checking scsi/sg.h usability... yes checking scsi/sg.h presence... yes checking for scsi/sg.h... yes checking linux/input.h usability... yes checking linux/input.h presence... yes checking for linux/input.h... yes checking linux/types.h usability... yes checking linux/types.h presence... yes checking for linux/types.h... yes checking for linux/hiddev.h... yes checking for HIDDEV_FLAG_UREF support... yes checking sys/soundcard.h usability... yes checking sys/soundcard.h presence... yes checking for sys/soundcard.h... yes checking linux/i2c-dev.h usability... yes checking linux/i2c-dev.h presence... yes checking for linux/i2c-dev.h... yes checking for daemon... yes configure: creating ./config.status config.status: creating Makefile config.status: creating drivers/Makefile config.status: creating drivers/lirc_atiusb/Makefile config.status: creating drivers/lirc_bt829/Makefile config.status: creating drivers/lirc_dev/Makefile config.status: creating drivers/lirc_gpio/Makefile config.status: creating drivers/lirc_i2c/Makefile config.status: creating drivers/lirc_igorplugusb/Makefile config.status: creating drivers/lirc_ttusbir/Makefile config.status: creating drivers/lirc_imon/Makefile config.status: creating drivers/lirc_parallel/Makefile config.status: creating drivers/lirc_sasem/Makefile config.status: creating drivers/lirc_serial/Makefile config.status: creating drivers/lirc_sir/Makefile config.status: creating drivers/lirc_wpc8769l/Makefile config.status: creating daemons/Makefile config.status: creating tools/Makefile config.status: creating doc/Makefile config.status: creating doc/man/Makefile config.status: creating config.h config.status: config.h is unchanged config.status: executing depfiles commands config.status: executing libtool commands Your hardware does not require a special LIRC kernel module. Now enter 'make' and 'make install' to compile and install the package. make all-recursive make[1]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0' Making all in drivers make[2]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/drivers' make[3]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/drivers' make[3]: Nothing to be done for `all-am'. make[3]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/drivers' make[2]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/drivers' Making all in daemons make[2]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/daemons' make all-am make[3]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/daemons' make[3]: Nothing to be done for `all-am'. make[3]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/daemons' make[2]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/daemons' Making all in tools make[2]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/tools' make[2]: Nothing to be done for `all'. make[2]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/tools' Making all in doc make[2]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/doc' Making all in man make[3]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/doc/man' make[3]: Nothing to be done for `all'. make[3]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/doc/man' make[3]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/doc' make[3]: Nothing to be done for `all-am'. make[3]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/doc' make[2]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0/doc' make[2]: Entering directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0' make[2]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0' make[1]: Leaving directory `/home/shuwen/RDK3/RDK3.0/lirc-0.9.0'