root@dm816x-evm:/media/mmcblk0p3/progs# . ./skript -sh: ./skript: /usr/local/share/ti/ti-media-controller-utils/load-hd-firmware.sh: not found Starting PVR insmod: error inserting '/lib/modules/2.6.37/kernel/drivers/gpu/pvr/pvrsrvkm.ko': -1 File exists /dev/mem opened. Memory mapped at address 0x402da000. Read at address 0x48180F04 (0x402daf04): 0x00000000 Write at address 0x48180F04 (0x402daf04): 0x00000000, readback 0x00000000 /dev/mem opened. Memory mapped at address 0x4011a000. Read at address 0x48180900 (0x4011a900): 0x00000102 Write at address 0x48180900 (0x4011a900): 0x00000002, readback 0x00000002 /dev/mem opened. Memory mapped at address 0x402e0000. Read at address 0x48180920 (0x402e0920): 0x00000002 Write at address 0x48180920 (0x402e0920): 0x00000002, readback 0x00000002 Module drm failed to load. Retrying. Running /sbin/depmod X.Org X Server 1.7.5 Release Date: 2010-02-16 X Protocol Version 11, Revision 0 Build Operating System: Linux 2.6.35-30-generic-pae i686 Current Operating System: Linux dm816x-evm 2.6.37 #1 Wed Jun 1 12:18:59 IST 2011 armv7l Kernel command line: console=ttyO2,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=256M earlyprink vram=50M ti816xfb.vram=0:16M,1:16M,2:6M ip=off noinitrd Build Date: 28 September 2011 11:37:44PM Current version of pixman: 0.16.4 .Before reporting problems, check http://wiki.x.org .to make sure that you have the latest version. Markers: (--) probed, (**) from config file, (==) default setting, .(++) from command line, (!!) notice, (II) informational, .(WW) warning, (EE) error, (NI) not implemented, (??) unknown. (==) Log file: "/usr/local/XSGX/var/log/Xorg.0.log", Time: Wed Jun 1 17:19:29 2011 Continuing to load PowerVR services (++) Using config file: "/usr/local/XSGX/etc/xorg.conf" (==) No Layout section. Using the first Screen section. (**) |-->Screen "Screen" (0) (**) | |-->Monitor "" (**) | |-->Device "Video Device" (==) No monitor specified for screen "Screen". .Using a default monitor configuration. (==) Not automatically adding devices (==) Not automatically enabling devices (WW) The directory "/usr/local/XSGX/share/fonts/X11/TTF/" does not exist. .Entry deleted from font path. (WW) The directory "/usr/local/XSGX/share/fonts/X11/OTF" does not exist. .Entry deleted from font path. (==) FontPath set to: ./usr/local/XSGX/share/fonts/X11/misc/, ./usr/local/XSGX/share/fonts/X11/Type1/, ./usr/local/XSGX/share/fonts/X11/100dpi/, ./usr/local/XSGX/share/fonts/X11/75dpi/ (==) ModulePath set to "/usr/local/XSGX/lib/xorg/modules" (==) |-->Input Device "Main Touch Screen" (==) |-->Input Device "Keyboard" (==) No Layout section. Using the first core pointer device. (==) No Layout section. Using the first core keyboard device. (--) using VT number 2