/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "spi.h" #include "usart.h" #include "gpio.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include #include "ads1256.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ ADS125X_t ads1256; float volt[8] = {0.0f, 0.0f, 0.0f, 0.0f, 0.0f, 0.0f, 0.0f, 0.0f}; /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ // HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ // SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ // MX_GPIO_Init(); // MX_USART1_UART_Init(); // MX_SPI2_Init(); /* USER CODE BEGIN 2 */ ads1256.csPort = SPI2_CS_GPIO_Port; ads1256.csPin = SPI2_CS_Pin; ads1256.drdyPort = ADS1256_READY_GPIO_Port; ads1256.drdyPin = ADS1256_READY_Pin; ads1256.vref = 2.5f; ads1256.oscFreq = ADS125X_OSC_FREQ; ADS125X_Init(&ads1256, &hspi2, ADS125X_DRATE_10SPS, ADS125X_GAIN_1, 0); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ rt_kprintf("Hello Quectel\r\n"); rt_thread_mdelay(1000); ADS125X_ChannelDiff_Set(&ads1256, ADS125X_MUXP_AIN0, ADS125X_MUXN_AIN1); volt[0] = ADS125X_ADC_ReadVolt(&ads1256); rt_kprintf("volt0 = %f\n", volt[0]); ADS125X_ChannelDiff_Set(&ads1256, ADS125X_MUXP_AIN1, ADS125X_MUXN_AIN2); volt[1] = ADS125X_ADC_ReadVolt(&ads1256); rt_kprintf("volt1 = %f\n", volt[1]); ADS125X_ChannelDiff_Set(&ads1256, ADS125X_MUXP_AIN2, ADS125X_MUXN_AIN3); // ADS125X_CMD_Send(&ads1256, ADS125X_CMD_SYNC); volt[2] = ADS125X_ADC_ReadVolt(&ads1256); rt_kprintf("volt2 = %f\n", volt[2]); ADS125X_ChannelDiff_Set(&ads1256, ADS125X_MUXP_AIN3, ADS125X_MUXN_AIN4); volt[3] = ADS125X_ADC_ReadVolt(&ads1256); rt_kprintf("volt3 = %f\n", volt[3]); ADS125X_ChannelDiff_Set(&ads1256, ADS125X_MUXP_AIN4, ADS125X_MUXN_AIN5); volt[4] = ADS125X_ADC_ReadVolt(&ads1256); rt_kprintf("volt4 = %f\n", volt[4]); ADS125X_ChannelDiff_Set(&ads1256, ADS125X_MUXP_AIN5, ADS125X_MUXN_AIN6); volt[5] = ADS125X_ADC_ReadVolt(&ads1256); rt_kprintf("volt5 = %f\n", volt[5]); ADS125X_ChannelDiff_Set(&ads1256, ADS125X_MUXP_AIN6, ADS125X_MUXN_AIN7); volt[6] = ADS125X_ADC_ReadVolt(&ads1256); rt_kprintf("volt6 = %f\n", volt[6]); /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) { Error_Handler(); } } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief Period elapsed callback in non blocking mode * @note This function is called when TIM1 interrupt took place, inside * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment * a global variable "uwTick" used as application time base. * @param htim : TIM handle * @retval None */ void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { /* USER CODE BEGIN Callback 0 */ /* USER CODE END Callback 0 */ if (htim->Instance == TIM1) { HAL_IncTick(); } /* USER CODE BEGIN Callback 1 */ /* USER CODE END Callback 1 */ } /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */